Balluff - BVS CA-GT Technical Documentation
Loading...
Searching...
No Matches
Related Pages
Here is a list of all related documentation pages:
 Order Code Nomenclature
 What's inside and accessories
 Technical Data
 Sensor Overview
 Summary of CMOS sensors
 Filters
 APIs And Tools
 GenICam™ GenTL Software Stack
 The Impact Acquire Software Stack
 Developing Applications Using The Impact Acquire SDK
 GUI Tools
 Relationship Between Framework, Firmware And SDK
 GenICam™ And Advanced Features
 About Settings
 DirectShow Interface
 Troubleshooting
 Error Code List
 Accessing log files
 General Issues
 I can see the camera in IPConfigure, but I cannot access the camera
 Image Data Is Lost (Incomplete Frames)
 The error counter increases
 I get an exception when setting OffsetX or OffsetY
 I get an oscillating frame rate
 Why does updating the device list take so long
 Windows®
 The 'LostImagesCount' increases
 VLC Media Player Issues
 Linux
 No GenICam™ devices are detected on a Linux system
 No GigE Vision™ devices are detected on a Linux system
 Glossary
 Related Manuals
 Use Cases
 Introducing acquisition / recording possibilities
 Acquiring a number of images
 Recording sequences with pre-trigger
 Generating very long exposure times
 Working with multiple AOIs (mv Multi Area Mode)
 Using the mvMultiExposureCount feature
 Working with burst mode buffer
 Working with Event Control
 Using Video Stream Recording
 Introducing multicasting
 Using the Particle Image Velocimetry (PIV) shutter feature
 Working with the dual exposure feature ("mvMultiZone")
 Improving the acquisition / image quality
 Correcting image errors of a sensor
 Optimizing the color/luminance fidelity of the camera
 Reducing noise by frame averaging
 Setting a flicker-free auto expose and auto gain
 Working with binning / decimation
 Working with the Dual ADC feature of Sony Gen4 sensors
 Improving the communication
 Optimizing the bandwidth
 Discovering Devices In Different Subnets
 Working with triggers
 Processing triggers from an incremental encoder
 Generating a pulse width modulation (PWM)
 Outputting a pulse at every other external trigger
 Creating different exposure times for consecutive images
 Detecting overtriggering
 Triggering of an indefinite sequence with precise starting time
 Low latency triggering
 Working with I/Os
 Controlling strobe or flash at the outputs
 Creating a debouncing filter at the inputs
 Mapping UserOutputs to Physical Outputs in the Sequencer
 Saving data on the device
 Creating user data entries
 Creating user set entries
 Working with device features
 Working with the temperature sensors
 Disabling the heartbeat
 Reset timestamp by hardware
 Synchronizing camera timestamps
 Working With The Serial Interface (mv Serial Interface Control)
 Working with several cameras simultaneously
 Using Action Commands
 Creating synchronized acquisitions
 Using the primary application switchover functionality
 Working with 3rd party tools
 Using VLC Media Player
 Working with ROS (Robot Operating System)
 Working with GStreamer - The Impact Acquire GenICam GStreamer Plugin
 Appendix A. Specific Camera / Sensor Data
 A.1 Pregius S CMOS (Mono)
 BVS CA-GT1-0051BG (5.1 Mpix [2464 x 2064])
 Device Feature And Property List
 BVS CA-GT1-0081UG (8.1 Mpix [2848 x 2848])
 Device Feature And Property List
 BVS CA-GT1-0081ZG (8.1 Mpix [2848 x 2848])
 Device Feature And Property List
 BVS CA-GT1-0124BG (12.4 Mpix [4128 x 3008])
 Device Feature And Property List
 BVS CA-GT1-0162ZG (16.2 Mpix [5328 x 3040])
 Device Feature And Property List
 BVS CA-GT1-0204ZG (20.4 Mpix [4512 x 4512])
 Device Feature And Property List
 BVS CA-GT1-0246ZG (24.6 Mpix [5328 x 4608])
 Device Feature And Property List
 A.2 Pregius S CMOS (Color)
 BVS CA-GT1-0051BC (5.1 Mpix [2464 x 2064])
 Device Feature And Property List
 BVS CA-GT1-0081ZC (8.1 Mpix [2848 x 2848])
 Device Feature And Property List
 BVS CA-GT1-0124BC (12.4 Mpix [4128 x 3008])
 Device Feature And Property List
 BVS CA-GT1-0162ZC (16.2 Mpix [5328 x 3040])
 Device Feature And Property List
 BVS CA-GT1-0204ZC (20.4 Mpix [4512 x 4512])
 Device Feature And Property List
 BVS CA-GT1-0246ZC (24.6 Mpix [5328 x 4608])
 Device Feature And Property List
 Appendix B. Product Comparison
 Appendix C. Tested ARM platforms
 C.1 ARM64 based devices
 NVIDIA Jetson™ AGX Orin