|
Impact Acquire SDK Java
|
| CAutoCloseable | |
| CDeviceManager | Grants access to devices that can be operated by this software interface |
| CImageDisplayWindow | A class that can be used to display images in a window |
| CRuntimeException | |
| CImpactAcquireException | A base class for exceptions generated by Impact Acquire |
| CEDeviceManager | A base class for device manager related exceptions |
| CEPropertyHandling | A base class for exceptions related to the property module |
| CECantAllocateNewList | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_CANT_ALLOCATE_LIST error |
| CECantSerializeData | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_CANT_SERIALIZE_DATA error |
| CEComponent | A base class for mvIMPACT.acquire.Component object related exceptions from the property module |
| CEIncompatibleComponents | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INCOMPATIBLE_COMPONENTS error |
| CEMethod | A base class for mvIMPACT.acquire.Method object related exceptions from the property module |
| CEInvalidParameterList | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_METHOD_INVALID_PARAM_LIST error |
| CEMethodPtrInvalid | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_METHOD_PTR_INVALID error |
| CENoModifySizeRights | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NO_MODIFY_SIZE_RIGHTS error |
| CENoReadRights | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NO_READ_RIGHTS error |
| CENoWriteRights | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NO_WRITE_RIGHTS error |
| CENotAList | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NOT_A_LIST error |
| CENotAMethod | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NOT_A_METHOD error |
| CENotAProperty | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NOT_A_PROPERTY error |
| CEProperty | A base class for mvIMPACT.acquire.Property related exceptions from the property module |
| CEInvalidValue | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_PROP_VALUE error |
| CEInvalidValueType | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_PROP_VALUE_TYPE error |
| CETranslationTableCorrupted | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_TRANSLATION_TABLE_CORRUPTED error |
| CETranslationTableNotDefined | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_TRANSLATION_TABLE_NOT_DEFINED error |
| CEValIDOutOfBounds | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VAL_ID_OUT_OF_BOUNDS error |
| CEValTooLarge | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VAL_TOO_LARGE error |
| CEValTooSmall | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VAL_TOO_SMALL error |
| CEValidationFailed | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VALIDATION_FAILED error |
| CEPropertyList | A base class for component list related exceptions from the property module |
| CECantAccessData | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_LIST_CANT_ACCESS_DATA error |
| CECantRegisterComponent | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_CANT_REGISTER_COMPONENT error |
| CEComponentIDInvalid | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_COMPONENT_ID_INVALID error |
| CEComponentNotFound | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_COMPONENT_NOT_FOUND error |
| CEInvalidListID | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_LIST_ID_INVALID error |
| CEListEntryOccupied | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_LIST_ENTRY_OCCUPIED error |
| CEImplementationMissing | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_IMPLEMENTATION_MISSING error |
| CEInputBufferTooSmall | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INPUT_BUFFER_TOO_SMALL error |
| CEInvalidFileContent | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_FILE_CONTENT error |
| CEInvalidInputParameter | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_INPUT_PARAMETER error |
| CESizeMismatch | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_SIZE_MISMATCH error |
| CEUnsupportedOperation | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_UNSUPPORTED_OPERATION error |
| CEUnsupportedParameter | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_UNSUPPORTED_PARAMETER error |
| CEWrongParamCount | An exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_WRONG_PARAM_COUNT error |
| CAbstractList | |
| CComponentVector | |
| CDoubleVector | |
| CGenTLProducerConfigurationVector | |
| CInt64Vector | |
| CIntVector | |
| CStringDoubleVector | |
| CStringInt64Vector | |
| CStringIntVector | |
| CStringVector | |
| CAbstractMap | |
| CStringPropertyIMap | |
| CRandomAccess | |
| CComponentVector | |
| CDoubleVector | |
| CGenTLProducerConfigurationVector | |
| CInt64Vector | |
| CIntVector | |
| CStringDoubleVector | |
| CStringInt64Vector | |
| CStringIntVector | |
| CStringVector | |
| CacquireConstants | |
| Cacquire | |
| CAcquisitionControl | Category for the acquisition and trigger control features |
| CActionControl | Category that contains the Action control features |
| CAnalogControl | Category that contains the Analog control features |
| CCameraDescriptionManager | Grants access to camera description objects(Device specific interface layout only) (deprecated) |
| CChannelData | A structure for image buffer channel specific data |
| CChunkDataControl | Category that contains the Chunk Data control features |
| CColorTransformationControl | Category that contains the Color Transformation control features |
| CComponentAccess | A base class to implement access to internal driver objects |
| CComponent | A base class to implement access to internal driver components |
| CComponentList | A class to provide access to component lists |
| CMethod | A class to call arbitrary driver functions |
| CProperty | A base class for properties |
| CPropertyF | A template class to represent float properties and enumerated float properties |
| CPropertyI | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyI64 | A template class to represent 64 bit integer properties and enumerated 64 bit integer properties |
| CPropertyPtr | A class to represent pointer properties |
| CPropertyS | A class to represent string properties |
| CComponentLocatorBase | A base class to locate components within the driver |
| CComponentLocator | A class to locate components within the driver |
| CDeviceComponentLocator | A class to locate components within the driver |
| CComponentCallback | A simple helper class to wrap the creation of a callback object |
| CComponentCollection | A base class for sets of properties that can be modified by the user |
| CAutoControlParameters | A class to control the automatic control parameters of a device(Device specific interface layout only) |
| CBasicDeviceSettings | A base class for essential device related settings |
| CBasicDeviceSettingsWithAOI | A base class for camera related settings(Device specific interface layout only) |
| CCameraSettingsBase | A base class for camera related settings(Device specific interface layout only) |
| CCameraSettingsBlueDevice | A base class for camera related settings belonging to the mvBlueXXX-series (Device specific interface layout only) |
| CCameraSettingsBlueCOUGAR | mvBlueCOUGAR related camera settings (Device specific interface layout only) |
| CCameraSettingsBlueFOX | mvBlueFOX related camera settings(Device specific interface layout only) |
| CCameraSettingsFrameGrabber | A class to access frame grabber related camera settings(Device specific interface layout only) (deprecated) |
| CCameraSettingsVirtualDevice | mvVirtualDevice related camera settings(Device specific interface layout only) |
| CCameraSettingsV4L2Device | mvV4L2 related camera settings(Device specific interface layout only) |
| CBufferPart | Contains information about a specific part of a captured buffer |
| CCameraDescriptionBase | A base class to describe a camera (Device specific interface layout only) connected to a frame grabber (deprecated) |
| CCameraDescriptionDigitalBase | A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated) |
| CCameraDescriptionDigitalBase2 | A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated) |
| CCameraDescriptionCameraLink | A class to describe a CameraLink® compliant camera(Device specific interface layout only) (deprecated) |
| CCameraDescriptionDigital | A class to describe a non-standard digital video signal(Device specific interface layout only) (deprecated) |
| CCameraDescriptionSDI | A base class to describe an SDI(Serial Digital Interface) camera signal (Device specific interface layout only) (deprecated) |
| CCameraDescriptionStandardBase | An internal base class to describe standard analogue video cameras(Device specific interface layout only) (deprecated) |
| CCameraDescriptionNonStandard | A class describing non-standard video cameras(Device specific interface layout only) (deprecated) |
| CCameraDescriptionStandard | A class describing analogue standard compliant video cameras(Device specific interface layout only) (deprecated) |
| CConnector | A class describing how a video signal source(e.g |
| CDataStreamModule | Category that contains items that belong to the data stream module of the transport layer |
| CDepthControl | Adjustment and triggering of the depth image for 3D control |
| CDeviceModule | Category contains items that belong to the device module of the transport layer |
| CDigitalIOMeasurementControl | Properties for configuring settings belonging to the digital I/O measurement(Device specific interface layout only) |
| CGainOffsetKneeChannelParameters | Properties for configuring settings belonging to a certain channel of the GainOffsetKnee filter |
| CGenTLDriverConfigurator | A class that contains items to configure the behaviour of the GenICam GenTL driver stack |
| CGenTLProducerConfiguration | A class that contains items to configure the behaviour of the GenICam GenTL driver stack |
| CHDRControl | A class to control the HDR (High Dynamic Range) parameters of a device (Device specific interface layout only) |
| CHDRKneePoint | A class to configure a HDR (High Dynamic Range) knee point (Device specific interface layout only) |
| CI2CControl | Properties for accessing features belonging to the I2C control(Device specific interface layout only) |
| CImageDestination | Properties to define the format of resulting images |
| CImageMemoryManager | An interface class to access DMA memory related properties(Device specific interface layout only) (deprecated) |
| CImageProcessing | Base class for image processing related properties |
| CImageRequestControl | A helper class to control the way an image request will be processed |
| CInfo | A base class to access various general information about the device and its driver |
| CInfoBlueDevice | A more specific class to query information about a mvBlueDevice device and its driver(Device specific interface layout only) |
| CInfoBlueCOUGAR | A more specific class to query information about a mvBlueCOUGAR devices and its driver(Device specific interface layout only) |
| CInfoBlueFOX | A more specific class to query information about a mvBlueFOX device and its driver(Device specific interface layout only) |
| CInterfaceModule | Category that contains items that belong to the interface module of the transport layer |
| CLUTParameters | Properties for configuring settings belonging to a certain LUT (Look Up Table) to be applied to a captured image |
| CMirrorParameters | Properties for configuring settings belonging to the mirror filter that processes a certain channel of a captured image |
| CMotorFocusControl | Properties for configuring settings belonging to the motor focus control (Device specific interface layout only) |
| CPulseStartConfiguration | A class to configure the creation of digital signals passed to one or more of the digital outputs of a device(Device specific interface layout only) |
| CRTCtrProgram | A class to represent real time control programs(Device specific interface layout only) |
| CRTCtrProgramStep | A class to represent one step of a real time control(RTCtr) program (Device specific interface layout only) |
| CRequestInfoConfiguration | Properties to configure which information shall be attached to the resulting images |
| CStatistics | Contains basic statistical information |
| CSyncOutput | A class to represent a sync |
| CSystemModule | Category that contains items that belong to the system module of the transport layer |
| CSystemSettings | A base class for accessing settings that control the overall behaviour of a device driver |
| CSystemBlueFOX | A class containing mvBlueFOX specific settings to control the overall behaviour of the driver(Device specific interface layout only) |
| CSystemV4L2 | A class containing mvV4L2 specific settings to control the overall behaviour of the driver(Device specific interface layout only) |
| CTriggerControl | A class to configure the behaviour of trigger signals |
| CWhiteBalanceSettings | Properties for adjusting the colors during a Bayer conversion |
| CmvAutoFeatureControl | Contains features to control the image controllers |
| CmvCurrentControl | Category that contains features to control the devices Current Control parameters |
| CmvDefectivePixelCorrectionControl | Contains features to control the device's defective pixel correction parameters |
| CmvFFCControl | Contains features to control the devices Flat Field Correction parameters |
| CmvFrameAverageControl | Category that contains features to control the frame averaging engine |
| CmvHDRControl | Category that contains features to control the devices High Dynamic Range parameters |
| CmvLensControl | Contains features to control motorized lenses |
| CmvLogicGateControl | Category that contains features to control the devices Logic Gate Control parameters |
| CmvPoDLDeviceControl | Category for device information and control |
| CmvPoDLPortControl | Category for status and control features for the camera ports |
| CmvSerialInterfaceControl | Contains features to control the serial interface |
| CCounterAndTimerControl | Category that contains the Counter and Timer control features |
| CCustomCommandGenerator | Contains convenience functions to control features understood by a devices custom command interpreter |
| CDevice | This class and its functions represent an actual device detected by this interface in the current system |
| CDeviceControl | Classes and functions that will be available if the device is used |
| CDigitalInput | A class to represent a digital input pin(Device specific interface layout only) |
| CDigitalIOControl | Category that contains the digital input and output control features |
| CDigitalOutput | A class to represent a digital output pin(Device specific interface layout only) |
| CEncoderControl | Category that contains the quadrature Encoder Control features |
| CEventControl | Category that contains Event control features |
| CDeviceAccess | |
| CFeatureAccess | |
| CExceptionFactory | A factory class to raise Impact Acquire related exceptions |
| CFileAccessControl | Category that contains the File Access control features |
| CFirmwareUpdater | A class to perform a firmware update of a specific device |
| CFullSettingsBase | A base class that provides access to the most common settings for a device |
| CSettingsBlueFOX | This class provides access to general settings as well as to settings which are unique for the mvBlueFOX(Device specific interface layout only) |
| CFunctionInterface | The function interface to devices supported by this interface |
| CImageBuffer | Fully describes a captured image |
| CImageBufferDesc | A wrapper class to handle mvIMPACT.acquire.ImageBuffer structures |
| CImageDisplay | A class that can be used for displaying images within existing windows or GUI elements that can provide a window handle |
| CImageFormatControl | Category for Image Format Control features |
| CIOSubSystem | A base class to handle digital inputs and outputs(Device specific interface layout only) |
| CIOSubSystemBlueFOX | A class to handle the digital inputs and outputs for mvBlueFOX USB cameras(Device specific interface layout only) |
| CIOSubSystemCommon | A base class to handle the digital inputs and outputs for devices (Device specific interface layout only) |
| CIOSubSystemFrameGrabber | A class to handle the digital inputs and outputs for frame grabber devices(Device specific interface layout only) (deprecated) |
| CLensControlBase | Contains convenience functions to control features understood by generic lens adapters |
| CLensControlBirger | Contains convenience functions to control features understood by Birger Engineering, Inc |
| CLightControl | Category containing the Lighting control features |
| CLogicBlockControl | Category that contains the Logic Block control features |
| CLUTControl | Category that includes the LUT control features |
| CmvCameraIOPortControl | Category for Camera I/O Port Control features |
| CmvI2cInterfaceControl | Contains features to control the I2C interface |
| CmvIODeviceControl | Category for system wide I/O Control features |
| CmvSupplyVoltageControl | Category for controlling the supply voltages |
| CmvTriggerGeneratorControl | Category for controlling the trigger generator |
| COpticControl | Category for optical control features |
| COutputSignalGeneratorBlueDevice | A class to create complex digital output signals(Device specific interface layout only) |
| COutputSignalGeneratorFrameGrabber | A class to create complex digital output signals(Device specific interface layout only) (deprecated) |
| CRequest | Contains information about a captured buffer |
| CRequestFactory | A default request factory |
| CScan3dControl | Category for control of 3D camera specific features |
| CSequencerControl | Category for the Sequencer Control features |
| CSoftwareSignalControl | Category that contains the Software Signal Control features |
| CSourceControl | Category that contains the source control features |
| CStringDoublePair | |
| CStringInt64Pair | |
| CStringIntPair | |
| CStringPropertyIMap.Iterator | |
| CTAcquisitionField | Defines which field triggers the start of the acquisition (deprecated) |
| CTAcquisitionMode | Defines valid acquisition modes |
| CTAcquisitionStartStopBehaviour | Defines valid modes for acquisition start/stop behaviour |
| CTAoiMode | Defines valid Area Of Interest modes |
| CTAutoControlMode | Defines valid auto control modes |
| CTAutoControlSpeed | Defines valid auto-control speed modes |
| CTAutoExposureControl | Defines valid AEC( Automatic Exposure Control ) modes |
| CTAutoGainControl | Defines valid AGC( Automatic Gain Control ) modes |
| CTAutoOffsetCalibration | Defines valid offset calibration modes |
| CTBayerConversionMode | Defines the Bayer conversion algorithm to use |
| CTBayerMosaicParity | Defines valid Bayer formats |
| CTBayerWhiteBalanceResult | Defines valid results of a white balance calibration |
| CTBlueFOXDigitalInputThreshold | Defines valid thresholds( in Volt ) for the digital inputs of the |
| CTBlueFOXFooterMode | Defines the footer mode of the mvBlueFOX |
| CTBlueFOXInfoSensorCapabilities | Defines valid image sensor capabilities |
| CTBlueFOXOffsetAutoBlackSpeed | Defines Offset Auto Calibration Controller Speed |
| CTBlueFOXSensorTiming | Sensor timing options |
| CTBlueFOXTransferSize | Defines the block size used for the USB transfer of the mvBlueFOX |
| CTBoolean | Defines a Boolean value type |
| CTBufferPartDataType | Defines buffer part data types |
| CTCallbackType | Defines the type of callback to register |
| CTCameraAoiMode | Defines the camera Aoi modes |
| CTCameraBinningMode | Defines valid binning modes for the camera |
| CTCameraDataFormat | Defines the data format the camera is sending (deprecated) |
| CTCameraExposeMode | Defines recognized camera sensor expose modes |
| CTCameraExternalSyncEdge | Some grabbers are able to get the video signal and sync signals ( HD-IN, VD-IN ) on separate lines |
| CTCameraExternalSyncOutput | Some grabbers are able to get the video signal and the sync signal on different input pins |
| CTCameraFlashMode | Defines valid camera flash modes |
| CTCameraFlashType | Defines valid camera flash control types |
| CTCameraHDRMode | Defines valid camera High Dynamic Range modes |
| CTCameraInterlacedType | Defines how the camera transmits its video signal (deprecated) |
| CTCameraLinkDataValidMode | Defines how the camera transmits the DVAL signal defined in the CameraLink® standard (deprecated) |
| CTCameraOutput | Defines valid ways a camera can offer image data to a capture device (deprecated) |
| CTCameraPixelClock | Defines valid camera pixel frequencies |
| CTCameraScanMode | Defines valid scan modes for the a camera |
| CTCameraSerialPortBaudRate | Defines valid baud rates for serial port communication between frame grabber and camera (deprecated) |
| CTCameraShutterMode | Defines recognized camera sensor shutter modes |
| CTCameraTapsXGeometry | Multitap cameras can transmit data in different ways |
| CTCameraTapsYGeometry | Multi-tap cameras can transmit data in different ways |
| CTCameraTestMode | Defines valid transmission modes for the camera |
| CTCameraTriggerMode | Defines valid camera sensor trigger modes |
| CTCameraTriggerSource | Defined valid camera sensor trigger source values |
| CTChannelSplitMode | Defines valid modes for channel split filters |
| CTClampMode | Clamp signal means, that an AC coupled video signal is clamped on the porch to get a signal transfer with less noise and independent from the d.c |
| CTColorProcessingMode | Defines the color processing mode |
| CTColorTwistInputCorrectionMatrixMode | Defines valid values for input color correction matrices |
| CTColorTwistOutputCorrectionMatrixMode | Defines valid values for output color correction matrices |
| CTComponentFlag | Flags defining access rights and other component properties |
| CTComponentRepresentation | Defines valid recommended representations for features |
| CTComponentType | Allowed components handled by this module |
| CTComponentVisibility | Defines valid recommended visibilities for features |
| CTDarkCurrentFilterMode | Defines valid modes for the dark current filter |
| CTDefectivePixelsFilterMode | Defines valid modes for defective pixels filter |
| CTDeviceAccessMode | Defines valid device access modes |
| CTDeviceAdvancedOptions | Defines valid advanced options |
| CTDeviceAutoNegotiatePacketSizeMode | Defines the way the packet size auto negotiation is handled for GigE Vision™ devices |
| CTDeviceCapability | Defines valid device capabilities |
| CTDeviceClass | Defines valid generic device classes |
| CTDeviceDigitalOutputMode | Defines grabber specific digital output modes |
| CTDeviceImageTrigger | Defines acquisition start event if using pulse sequences (deprecated) |
| CTDeviceInterfaceLayout | Defines valid interface layouts for the device |
| CTDeviceListType | Defines valid interface list types, which can be located using an instance of mvIMPACT.acquire.DeviceComponentLocator |
| CTDeviceLoadSettings | Defines valid modes for the loading of settings during initialization |
| CTDevicePowerMode | Defines the power mode for this device |
| CTDeviceScanRateMode | Defines valid device scan rate mode (deprecated) |
| CTDeviceSignalOutputStartEvent | Defines valid moments to start the signal generation on the digital outputs (deprecated) |
| CTDeviceState | Defines valid Device states |
| CTDeviceSyncOutMode | Valid sync |
| CTDeviceTriggerInterface | Defines which trigger interface is currently active for the device |
| CTDeviceTriggerMode | Valid trigger modes for frame grabber boards (deprecated) |
| CTDeviceTriggerOverlap | Specifies the type trigger overlap permitted with the previous frame (deprecated) |
| CTDigIOState | Defines valid digital I/O states |
| CTDigitalIOMeasurementMode | Defines valid IO Measurement Modes |
| CTDigitalIOMeasurementSource | Defines valid IO Measurement Sources |
| CTDigitalOutputControlMode | Defines valid ways to create signals on a digital output (deprecated) |
| CTDigitalSignal | Defines valid digital source signal constants that can be used to configure a devices behaviour in certain digital I/O related modes (deprecated) |
| CTDisplayMode | Defines valid display modes |
| CTDMR_ERROR | Errors reported by the device manager |
| CTestControl | Category for Test Control features |
| CTFieldGateMode | The field gate is used to detect the field ( odd or even ) for interlaced video signals (deprecated) |
| CTFirmwareUpdateAction | Defines valid steps for the actual firmware update process |
| CTFirmwareUpdateStep | Defines valid steps for the actual firmware update process |
| CTFlatFieldFilterCorrectionMode | Defines valid modes for the flat field correction |
| CTFlatFieldFilterMode | Defines valid modes for the flat field filter |
| CTFormatFlags | Defines valid display pixel formats |
| CTHWUpdateResult | Defines valid Device HW update results |
| CTI2COperationMode | Valid I2C operation modes |
| CTI2COperationStatus | Valid I2C operation status values |
| CTImageBufferFormatReinterpreterMode | Valid image buffer format reinterpreter modes |
| CTImageBufferPixelFormat | Valid image buffer pixel formats |
| CTImageDestinationPixelFormat | Defines the pixel format of the result image |
| CTImageDisplayError | Defines valid error values for this module |
| CTImageFileFormat | Defines valid image file formats |
| CTImageProcessingFilter | Defines valid filters which can be applied to the captured image before it is transferred to the user |
| CTImageProcessingMode | Defines valid modes the internal image processing pipeline can be operated in |
| CTImageProcessingOptimization | Defines valid modes the internal image processing algorithms can be operated in |
| CTImageProcessingResult | Defines valid values for the result of a certain image processing algorithm applied to a request |
| CTImageRequestControlMode | Defines the behaviour of an mvIMPACT.acquire.ImageRequestControl |
| CTImageRequestParam | Defines valid image request parameters |
| CTImpactBufferFlag | Flags to define the way an mvIMPACT buffer is created and handled |
| CTInfoSensorColorMode | Defines the type of camera sensor |
| CTInfoSensorColorPattern | Defines the bayer pattern of the sensor |
| CTInfoSensorType | Defines the type of camera sensor |
| CTInterfaceEnumerationBehaviour | Defines the enumeration behaviour of a certain interface of a third-party GenTL producer |
| CTInterlacedMode | Defines how to handle interlaced image data (deprecated) |
| CTInterpolationMode | Defines valid scaler interpolation modes |
| CTLibraryQuery | Defines valid libraries to query information from |
| CTLineCounter | Currently available for mvTITAN/mvGAMMA-CL (deprecated) |
| CTLUTGammaMode | Defines valid LUT(LookUp Table) gamma modes |
| CTLUTImplementation | Defines valid LUT(LookUp Table) implementations |
| CTLUTInterpolationMode | Defines valid LUT(LookUp Table) interpolation modes |
| CTLUTMapping | Defines valid LUT(LookUp Table) mapping modes |
| CTLUTMode | Defines valid LUT(LookUp Table) modes |
| CTMemoryManagerMode | Defines valid modes to operate the memory manager in |
| CTMemoryManagerPoolMode | Defines the pool mode of memory manager |
| CTMirrorMode | Defines valid mirror modes |
| CTMirrorOperationMode | Defines valid mirror operation modes |
| CTOnBoardMemoryMode | Defines valid modes for the handling of the device' on board memory (if available) (deprecated) |
| CTPayloadType | Defines supported payload types |
| CTPolarizedDataExtractionInterpolationMode | Defines valid modes for the interpolation mode of polarization data extraction filters |
| CTPolarizedDataExtractionMode | Defines valid modes for polarization data extraction filters |
| CTPropertyLimits | Defines valid limits which can be queried for a mvIMPACT.acquire.Property object |
| CTPROPHANDLING_ERROR | Error codes of the module handling everything related to properties |
| CTPulseStartTrigger | Defines valid pulse start trigger values |
| CTransferControl | Category for the data Transfer Control features |
| CTransportLayerControl | Category that contains the transport Layer control features |
| CTRequestImageMemoryMode | Defines valid image modes for request objects |
| CTRequestResult | Defines valid result of an image request |
| CTRequestState | Defines the current state of this mvIMPACT.acquire.Request |
| CTRequestTransmissionMode | Defines valid request transmission modes |
| CTRTCtrlModes | Defines valid RTCtrl Modes |
| CTRTProgOpCodes | Defines valid RTProg OpCodes |
| CTScalerInterpolationMode | Defines valid scaler interpolation modes |
| CTScalerMode | Defines valid scaler modes |
| CTScanClock | Analogue grabbers generate its scan clock on different ways (deprecated) |
| CTScanStandard | Defines valid scan modes for standard cameras (deprecated) |
| CTScope | Defines the scope for data import/export operations |
| CTSequencerSetParameter | Defines valid parameters that can be modified within a sequencer set at runtime |
| CTStorageFlag | Defines the way component lists are imported and exported |
| CTStorageLocation | Defines valid storage locations for component list import, export and delete operations |
| CTTriggerMoment | Defines a trigger moment for a digital signal |
| CTUserDataAccessRight | Defines valid flags for controlling the user access rights to the user data that can be stored in the devices non-volatile memory |
| CTUserDataReconnectBehaviour | Defined valid values for the behaviour of the user data when a device has been disconnected and reconnected within a running process |
| CTValueType | Allowed values types for property objects |
| CTVideoCodec | Defines valid video codecs that might be supported by the underlying video compression engine |
| CTVideoStandard | Defines valid video standards that might be supported by a video capture device |
| CTVirtualDeviceImageType | Defines valid image types used when capturing data from a certain directory |
| CTVirtualDeviceTestMode | Defines valid test modes for virtual devices |
| CTWhiteBalanceCalibrationMode | Defines valid white balance calibration modes |
| CTWhiteBalanceParameter | Defines valid parameter sets selectable via the WhiteBalance property |
| CUserData | A helper class to work with the device specific non-volatile memory(if available) |
| CUserDataEntry | A helper class that represents one entry in the devices non-volatile memory (if available) |
| CUserSetControl | Category that contains the User Set control features |
| CVideoStream | A class to create compressed video stream from images captured or loaded using the Impact Acquire API |
| CVideoStreamPauseScope | A smaller helper class for pausing a video stream for a defined time |
| CWhiteBalancer | Convenience class to provide an easy way for a more precise white balance calibration |