Impact Acquire SDK Java
Loading...
Searching...
No Matches
Class List
Here are the classes, structs, unions and interfaces with brief descriptions:
 PmvIMPACT
 Pacquire
 Pexamples
 Phelper
 CDeviceAccess
 CFeatureAccess
 Cacquire
 CacquireConstants
 CAcquisitionControlCategory for the acquisition and trigger control features
 CActionControlCategory that contains the Action control features
 CAnalogControlCategory that contains the Analog control features
 CAutoControlParametersA class to control the automatic control parameters of a device(Device specific interface layout only)
 CBasicDeviceSettingsA base class for essential device related settings
 CBasicDeviceSettingsWithAOIA base class for camera related settings(Device specific interface layout only)
 CBufferPartContains information about a specific part of a captured buffer
 CCameraDescriptionBaseA base class to describe a camera (Device specific interface layout only) connected to a frame grabber (deprecated)
 CCameraDescriptionCameraLinkA class to describe a CameraLink® compliant camera(Device specific interface layout only) (deprecated)
 CCameraDescriptionDigitalA class to describe a non-standard digital video signal(Device specific interface layout only) (deprecated)
 CCameraDescriptionDigitalBaseA base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated)
 CCameraDescriptionDigitalBase2A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated)
 CCameraDescriptionManagerGrants access to camera description objects(Device specific interface layout only) (deprecated)
 CCameraDescriptionNonStandardA class describing non-standard video cameras(Device specific interface layout only) (deprecated)
 CCameraDescriptionSDIA base class to describe an SDI(Serial Digital Interface) camera signal (Device specific interface layout only) (deprecated)
 CCameraDescriptionStandardA class describing analogue standard compliant video cameras(Device specific interface layout only) (deprecated)
 CCameraDescriptionStandardBaseAn internal base class to describe standard analogue video cameras(Device specific interface layout only) (deprecated)
 CCameraSettingsBaseA base class for camera related settings(Device specific interface layout only)
 CCameraSettingsBlueCOUGARmvBlueCOUGAR related camera settings (Device specific interface layout only)
 CCameraSettingsBlueDeviceA base class for camera related settings belonging to the mvBlueXXX-series (Device specific interface layout only)
 CCameraSettingsBlueFOXmvBlueFOX related camera settings(Device specific interface layout only)
 CCameraSettingsFrameGrabberA class to access frame grabber related camera settings(Device specific interface layout only) (deprecated)
 CCameraSettingsV4L2DevicemvV4L2 related camera settings(Device specific interface layout only)
 CCameraSettingsVirtualDevicemvVirtualDevice related camera settings(Device specific interface layout only)
 CChannelDataA structure for image buffer channel specific data
 CChunkDataControlCategory that contains the Chunk Data control features
 CColorTransformationControlCategory that contains the Color Transformation control features
 CComponentA base class to implement access to internal driver components
 CComponentAccessA base class to implement access to internal driver objects
 CComponentCallbackA simple helper class to wrap the creation of a callback object
 CComponentCollectionA base class for sets of properties that can be modified by the user
 CComponentListA class to provide access to component lists
 CComponentLocatorA class to locate components within the driver
 CComponentLocatorBaseA base class to locate components within the driver
 CComponentVector
 CConnectorA class describing how a video signal source(e.g
 CCounterAndTimerControlCategory that contains the Counter and Timer control features
 CCustomCommandGeneratorContains convenience functions to control features understood by a devices custom command interpreter
 CDataStreamModuleCategory that contains items that belong to the data stream module of the transport layer
 CDepthControlAdjustment and triggering of the depth image for 3D control
 CDeviceThis class and its functions represent an actual device detected by this interface in the current system
 CDeviceComponentLocatorA class to locate components within the driver
 CDeviceControlClasses and functions that will be available if the device is used
 CDeviceManagerGrants access to devices that can be operated by this software interface
 CDeviceModuleCategory contains items that belong to the device module of the transport layer
 CDigitalInputA class to represent a digital input pin(Device specific interface layout only)
 CDigitalIOControlCategory that contains the digital input and output control features
 CDigitalIOMeasurementControlProperties for configuring settings belonging to the digital I/O measurement(Device specific interface layout only)
 CDigitalOutputA class to represent a digital output pin(Device specific interface layout only)
 CDoubleVector
 CECantAccessDataAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_LIST_CANT_ACCESS_DATA error
 CECantAllocateNewListAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_CANT_ALLOCATE_LIST error
 CECantRegisterComponentAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_CANT_REGISTER_COMPONENT error
 CECantSerializeDataAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_CANT_SERIALIZE_DATA error
 CEComponentA base class for mvIMPACT.acquire.Component object related exceptions from the property module
 CEComponentIDInvalidAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_COMPONENT_ID_INVALID error
 CEComponentNotFoundAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_COMPONENT_NOT_FOUND error
 CEDeviceManagerA base class for device manager related exceptions
 CEImplementationMissingAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_IMPLEMENTATION_MISSING error
 CEIncompatibleComponentsAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INCOMPATIBLE_COMPONENTS error
 CEInputBufferTooSmallAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INPUT_BUFFER_TOO_SMALL error
 CEInvalidFileContentAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_FILE_CONTENT error
 CEInvalidInputParameterAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_INPUT_PARAMETER error
 CEInvalidListIDAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_LIST_ID_INVALID error
 CEInvalidParameterListAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_METHOD_INVALID_PARAM_LIST error
 CEInvalidValueAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_PROP_VALUE error
 CEInvalidValueTypeAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_PROP_VALUE_TYPE error
 CEListEntryOccupiedAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_LIST_ENTRY_OCCUPIED error
 CEMethodA base class for mvIMPACT.acquire.Method object related exceptions from the property module
 CEMethodPtrInvalidAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_METHOD_PTR_INVALID error
 CEncoderControlCategory that contains the quadrature Encoder Control features
 CENoModifySizeRightsAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NO_MODIFY_SIZE_RIGHTS error
 CENoReadRightsAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NO_READ_RIGHTS error
 CENotAListAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NOT_A_LIST error
 CENotAMethodAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NOT_A_METHOD error
 CENotAPropertyAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NOT_A_PROPERTY error
 CENoWriteRightsAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NO_WRITE_RIGHTS error
 CEPropertyA base class for mvIMPACT.acquire.Property related exceptions from the property module
 CEPropertyHandlingA base class for exceptions related to the property module
 CEPropertyListA base class for component list related exceptions from the property module
 CESizeMismatchAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_SIZE_MISMATCH error
 CETranslationTableCorruptedAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_TRANSLATION_TABLE_CORRUPTED error
 CETranslationTableNotDefinedAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_TRANSLATION_TABLE_NOT_DEFINED error
 CEUnsupportedOperationAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_UNSUPPORTED_OPERATION error
 CEUnsupportedParameterAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_UNSUPPORTED_PARAMETER error
 CEValidationFailedAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VALIDATION_FAILED error
 CEValIDOutOfBoundsAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VAL_ID_OUT_OF_BOUNDS error
 CEValTooLargeAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VAL_TOO_LARGE error
 CEValTooSmallAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VAL_TOO_SMALL error
 CEventControlCategory that contains Event control features
 CEWrongParamCountAn exception thrown in case of a mvIMPACT.acquire.TPROPHANDLING_ERROR.PROPHANDLING_WRONG_PARAM_COUNT error
 CExceptionFactoryA factory class to raise Impact Acquire related exceptions
 CFileAccessControlCategory that contains the File Access control features
 CFirmwareUpdaterA class to perform a firmware update of a specific device
 CFullSettingsBaseA base class that provides access to the most common settings for a device
 CFunctionInterfaceThe function interface to devices supported by this interface
 CGainOffsetKneeChannelParametersProperties for configuring settings belonging to a certain channel of the GainOffsetKnee filter
 CGenTLDriverConfiguratorA class that contains items to configure the behaviour of the GenICam GenTL driver stack
 CGenTLProducerConfigurationA class that contains items to configure the behaviour of the GenICam GenTL driver stack
 CGenTLProducerConfigurationVector
 CHDRControlA class to control the HDR (High Dynamic Range) parameters of a device (Device specific interface layout only)
 CHDRKneePointA class to configure a HDR (High Dynamic Range) knee point (Device specific interface layout only)
 CI2CControlProperties for accessing features belonging to the I2C control(Device specific interface layout only)
 CImageBufferFully describes a captured image
 CImageBufferDescA wrapper class to handle mvIMPACT.acquire.ImageBuffer structures
 CImageDestinationProperties to define the format of resulting images
 CImageDisplayA class that can be used for displaying images within existing windows or GUI elements that can provide a window handle
 CImageDisplayWindowA class that can be used to display images in a window
 CImageFormatControlCategory for Image Format Control features
 CImageMemoryManagerAn interface class to access DMA memory related properties(Device specific interface layout only) (deprecated)
 CImageProcessingBase class for image processing related properties
 CImageRequestControlA helper class to control the way an image request will be processed
 CImpactAcquireExceptionA base class for exceptions generated by Impact Acquire
 CInfoA base class to access various general information about the device and its driver
 CInfoBlueCOUGARA more specific class to query information about a mvBlueCOUGAR devices and its driver(Device specific interface layout only)
 CInfoBlueDeviceA more specific class to query information about a mvBlueDevice device and its driver(Device specific interface layout only)
 CInfoBlueFOXA more specific class to query information about a mvBlueFOX device and its driver(Device specific interface layout only)
 CInt64Vector
 CInterfaceModuleCategory that contains items that belong to the interface module of the transport layer
 CIntVector
 CIOSubSystemA base class to handle digital inputs and outputs(Device specific interface layout only)
 CIOSubSystemBlueFOXA class to handle the digital inputs and outputs for mvBlueFOX USB cameras(Device specific interface layout only)
 CIOSubSystemCommonA base class to handle the digital inputs and outputs for devices (Device specific interface layout only)
 CIOSubSystemFrameGrabberA class to handle the digital inputs and outputs for frame grabber devices(Device specific interface layout only) (deprecated)
 CLensControlBaseContains convenience functions to control features understood by generic lens adapters
 CLensControlBirgerContains convenience functions to control features understood by Birger Engineering, Inc
 CLightControlCategory containing the Lighting control features
 CLogicBlockControlCategory that contains the Logic Block control features
 CLUTControlCategory that includes the LUT control features
 CLUTParametersProperties for configuring settings belonging to a certain LUT (Look Up Table) to be applied to a captured image
 CMethodA class to call arbitrary driver functions
 CMirrorParametersProperties for configuring settings belonging to the mirror filter that processes a certain channel of a captured image
 CMotorFocusControlProperties for configuring settings belonging to the motor focus control (Device specific interface layout only)
 CmvAutoFeatureControlContains features to control the image controllers
 CmvCameraIOPortControlCategory for Camera I/O Port Control features
 CmvCurrentControlCategory that contains features to control the devices Current Control parameters
 CmvDefectivePixelCorrectionControlContains features to control the device's defective pixel correction parameters
 CmvFFCControlContains features to control the devices Flat Field Correction parameters
 CmvFrameAverageControlCategory that contains features to control the frame averaging engine
 CmvHDRControlCategory that contains features to control the devices High Dynamic Range parameters
 CmvI2cInterfaceControlContains features to control the I2C interface
 CmvIODeviceControlCategory for system wide I/O Control features
 CmvLensControlContains features to control motorized lenses
 CmvLogicGateControlCategory that contains features to control the devices Logic Gate Control parameters
 CmvPoDLDeviceControlCategory for device information and control
 CmvPoDLPortControlCategory for status and control features for the camera ports
 CmvSerialInterfaceControlContains features to control the serial interface
 CmvSupplyVoltageControlCategory for controlling the supply voltages
 CmvTriggerGeneratorControlCategory for controlling the trigger generator
 COpticControlCategory for optical control features
 COutputSignalGeneratorBlueDeviceA class to create complex digital output signals(Device specific interface layout only)
 COutputSignalGeneratorFrameGrabberA class to create complex digital output signals(Device specific interface layout only) (deprecated)
 CPropertyA base class for properties
 CPropertyFA template class to represent float properties and enumerated float properties
 CPropertyIA template class to represent 32 bit integer properties and 32 bit enumerated integer properties
 CPropertyI64A template class to represent 64 bit integer properties and enumerated 64 bit integer properties
 CPropertyPtrA class to represent pointer properties
 CPropertySA class to represent string properties
 CPulseStartConfigurationA class to configure the creation of digital signals passed to one or more of the digital outputs of a device(Device specific interface layout only)
 CRequestContains information about a captured buffer
 CRequestFactoryA default request factory
 CRequestInfoConfigurationProperties to configure which information shall be attached to the resulting images
 CRTCtrProgramA class to represent real time control programs(Device specific interface layout only)
 CRTCtrProgramStepA class to represent one step of a real time control(RTCtr) program (Device specific interface layout only)
 CScan3dControlCategory for control of 3D camera specific features
 CSequencerControlCategory for the Sequencer Control features
 CSettingsBlueFOXThis class provides access to general settings as well as to settings which are unique for the mvBlueFOX(Device specific interface layout only)
 CSoftwareSignalControlCategory that contains the Software Signal Control features
 CSourceControlCategory that contains the source control features
 CStatisticsContains basic statistical information
 CStringDoublePair
 CStringDoubleVector
 CStringInt64Pair
 CStringInt64Vector
 CStringIntPair
 CStringIntVector
 CStringPropertyIMap
 CIterator
 CStringVector
 CSyncOutputA class to represent a sync
 CSystemBlueFOXA class containing mvBlueFOX specific settings to control the overall behaviour of the driver(Device specific interface layout only)
 CSystemModuleCategory that contains items that belong to the system module of the transport layer
 CSystemSettingsA base class for accessing settings that control the overall behaviour of a device driver
 CSystemV4L2A class containing mvV4L2 specific settings to control the overall behaviour of the driver(Device specific interface layout only)
 CTAcquisitionFieldDefines which field triggers the start of the acquisition (deprecated)
 CTAcquisitionModeDefines valid acquisition modes
 CTAcquisitionStartStopBehaviourDefines valid modes for acquisition start/stop behaviour
 CTAoiModeDefines valid Area Of Interest modes
 CTAutoControlModeDefines valid auto control modes
 CTAutoControlSpeedDefines valid auto-control speed modes
 CTAutoExposureControlDefines valid AEC( Automatic Exposure Control ) modes
 CTAutoGainControlDefines valid AGC( Automatic Gain Control ) modes
 CTAutoOffsetCalibrationDefines valid offset calibration modes
 CTBayerConversionModeDefines the Bayer conversion algorithm to use
 CTBayerMosaicParityDefines valid Bayer formats
 CTBayerWhiteBalanceResultDefines valid results of a white balance calibration
 CTBlueFOXDigitalInputThresholdDefines valid thresholds( in Volt ) for the digital inputs of the
 CTBlueFOXFooterModeDefines the footer mode of the mvBlueFOX
 CTBlueFOXInfoSensorCapabilitiesDefines valid image sensor capabilities
 CTBlueFOXOffsetAutoBlackSpeedDefines Offset Auto Calibration Controller Speed
 CTBlueFOXSensorTimingSensor timing options
 CTBlueFOXTransferSizeDefines the block size used for the USB transfer of the mvBlueFOX
 CTBooleanDefines a Boolean value type
 CTBufferPartDataTypeDefines buffer part data types
 CTCallbackTypeDefines the type of callback to register
 CTCameraAoiModeDefines the camera Aoi modes
 CTCameraBinningModeDefines valid binning modes for the camera
 CTCameraDataFormatDefines the data format the camera is sending (deprecated)
 CTCameraExposeModeDefines recognized camera sensor expose modes
 CTCameraExternalSyncEdgeSome grabbers are able to get the video signal and sync signals ( HD-IN, VD-IN ) on separate lines
 CTCameraExternalSyncOutputSome grabbers are able to get the video signal and the sync signal on different input pins
 CTCameraFlashModeDefines valid camera flash modes
 CTCameraFlashTypeDefines valid camera flash control types
 CTCameraHDRModeDefines valid camera High Dynamic Range modes
 CTCameraInterlacedTypeDefines how the camera transmits its video signal (deprecated)
 CTCameraLinkDataValidModeDefines how the camera transmits the DVAL signal defined in the CameraLink® standard (deprecated)
 CTCameraOutputDefines valid ways a camera can offer image data to a capture device (deprecated)
 CTCameraPixelClockDefines valid camera pixel frequencies
 CTCameraScanModeDefines valid scan modes for the a camera
 CTCameraSerialPortBaudRateDefines valid baud rates for serial port communication between frame grabber and camera (deprecated)
 CTCameraShutterModeDefines recognized camera sensor shutter modes
 CTCameraTapsXGeometryMultitap cameras can transmit data in different ways
 CTCameraTapsYGeometryMulti-tap cameras can transmit data in different ways
 CTCameraTestModeDefines valid transmission modes for the camera
 CTCameraTriggerModeDefines valid camera sensor trigger modes
 CTCameraTriggerSourceDefined valid camera sensor trigger source values
 CTChannelSplitModeDefines valid modes for channel split filters
 CTClampModeClamp signal means, that an AC coupled video signal is clamped on the porch to get a signal transfer with less noise and independent from the d.c
 CTColorProcessingModeDefines the color processing mode
 CTColorTwistInputCorrectionMatrixModeDefines valid values for input color correction matrices
 CTColorTwistOutputCorrectionMatrixModeDefines valid values for output color correction matrices
 CTComponentFlagFlags defining access rights and other component properties
 CTComponentRepresentationDefines valid recommended representations for features
 CTComponentTypeAllowed components handled by this module
 CTComponentVisibilityDefines valid recommended visibilities for features
 CTDarkCurrentFilterModeDefines valid modes for the dark current filter
 CTDefectivePixelsFilterModeDefines valid modes for defective pixels filter
 CTDeviceAccessModeDefines valid device access modes
 CTDeviceAdvancedOptionsDefines valid advanced options
 CTDeviceAutoNegotiatePacketSizeModeDefines the way the packet size auto negotiation is handled for GigE Vision™ devices
 CTDeviceCapabilityDefines valid device capabilities
 CTDeviceClassDefines valid generic device classes
 CTDeviceDigitalOutputModeDefines grabber specific digital output modes
 CTDeviceImageTriggerDefines acquisition start event if using pulse sequences (deprecated)
 CTDeviceInterfaceLayoutDefines valid interface layouts for the device
 CTDeviceListTypeDefines valid interface list types, which can be located using an instance of mvIMPACT.acquire.DeviceComponentLocator
 CTDeviceLoadSettingsDefines valid modes for the loading of settings during initialization
 CTDevicePowerModeDefines the power mode for this device
 CTDeviceScanRateModeDefines valid device scan rate mode (deprecated)
 CTDeviceSignalOutputStartEventDefines valid moments to start the signal generation on the digital outputs (deprecated)
 CTDeviceStateDefines valid Device states
 CTDeviceSyncOutModeValid sync
 CTDeviceTriggerInterfaceDefines which trigger interface is currently active for the device
 CTDeviceTriggerModeValid trigger modes for frame grabber boards (deprecated)
 CTDeviceTriggerOverlapSpecifies the type trigger overlap permitted with the previous frame (deprecated)
 CTDigIOStateDefines valid digital I/O states
 CTDigitalIOMeasurementModeDefines valid IO Measurement Modes
 CTDigitalIOMeasurementSourceDefines valid IO Measurement Sources
 CTDigitalOutputControlModeDefines valid ways to create signals on a digital output (deprecated)
 CTDigitalSignalDefines valid digital source signal constants that can be used to configure a devices behaviour in certain digital I/O related modes (deprecated)
 CTDisplayModeDefines valid display modes
 CTDMR_ERRORErrors reported by the device manager
 CTestControlCategory for Test Control features
 CTFieldGateModeThe field gate is used to detect the field ( odd or even ) for interlaced video signals (deprecated)
 CTFirmwareUpdateActionDefines valid steps for the actual firmware update process
 CTFirmwareUpdateStepDefines valid steps for the actual firmware update process
 CTFlatFieldFilterCorrectionModeDefines valid modes for the flat field correction
 CTFlatFieldFilterModeDefines valid modes for the flat field filter
 CTFormatFlagsDefines valid display pixel formats
 CTHWUpdateResultDefines valid Device HW update results
 CTI2COperationModeValid I2C operation modes
 CTI2COperationStatusValid I2C operation status values
 CTImageBufferFormatReinterpreterModeValid image buffer format reinterpreter modes
 CTImageBufferPixelFormatValid image buffer pixel formats
 CTImageDestinationPixelFormatDefines the pixel format of the result image
 CTImageDisplayErrorDefines valid error values for this module
 CTImageFileFormatDefines valid image file formats
 CTImageProcessingFilterDefines valid filters which can be applied to the captured image before it is transferred to the user
 CTImageProcessingModeDefines valid modes the internal image processing pipeline can be operated in
 CTImageProcessingOptimizationDefines valid modes the internal image processing algorithms can be operated in
 CTImageProcessingResultDefines valid values for the result of a certain image processing algorithm applied to a request
 CTImageRequestControlModeDefines the behaviour of an mvIMPACT.acquire.ImageRequestControl
 CTImageRequestParamDefines valid image request parameters
 CTImpactBufferFlagFlags to define the way an mvIMPACT buffer is created and handled
 CTInfoSensorColorModeDefines the type of camera sensor
 CTInfoSensorColorPatternDefines the bayer pattern of the sensor
 CTInfoSensorTypeDefines the type of camera sensor
 CTInterfaceEnumerationBehaviourDefines the enumeration behaviour of a certain interface of a third-party GenTL producer
 CTInterlacedModeDefines how to handle interlaced image data (deprecated)
 CTInterpolationModeDefines valid scaler interpolation modes
 CTLibraryQueryDefines valid libraries to query information from
 CTLineCounterCurrently available for mvTITAN/mvGAMMA-CL (deprecated)
 CTLUTGammaModeDefines valid LUT(LookUp Table) gamma modes
 CTLUTImplementationDefines valid LUT(LookUp Table) implementations
 CTLUTInterpolationModeDefines valid LUT(LookUp Table) interpolation modes
 CTLUTMappingDefines valid LUT(LookUp Table) mapping modes
 CTLUTModeDefines valid LUT(LookUp Table) modes
 CTMemoryManagerModeDefines valid modes to operate the memory manager in
 CTMemoryManagerPoolModeDefines the pool mode of memory manager
 CTMirrorModeDefines valid mirror modes
 CTMirrorOperationModeDefines valid mirror operation modes
 CTOnBoardMemoryModeDefines valid modes for the handling of the device' on board memory (if available) (deprecated)
 CTPayloadTypeDefines supported payload types
 CTPolarizedDataExtractionInterpolationModeDefines valid modes for the interpolation mode of polarization data extraction filters
 CTPolarizedDataExtractionModeDefines valid modes for polarization data extraction filters
 CTPropertyLimitsDefines valid limits which can be queried for a mvIMPACT.acquire.Property object
 CTPROPHANDLING_ERRORError codes of the module handling everything related to properties
 CTPulseStartTriggerDefines valid pulse start trigger values
 CTransferControlCategory for the data Transfer Control features
 CTransportLayerControlCategory that contains the transport Layer control features
 CTRequestImageMemoryModeDefines valid image modes for request objects
 CTRequestResultDefines valid result of an image request
 CTRequestStateDefines the current state of this mvIMPACT.acquire.Request
 CTRequestTransmissionModeDefines valid request transmission modes
 CTriggerControlA class to configure the behaviour of trigger signals
 CTRTCtrlModesDefines valid RTCtrl Modes
 CTRTProgOpCodesDefines valid RTProg OpCodes
 CTScalerInterpolationModeDefines valid scaler interpolation modes
 CTScalerModeDefines valid scaler modes
 CTScanClockAnalogue grabbers generate its scan clock on different ways (deprecated)
 CTScanStandardDefines valid scan modes for standard cameras (deprecated)
 CTScopeDefines the scope for data import/export operations
 CTSequencerSetParameterDefines valid parameters that can be modified within a sequencer set at runtime
 CTStorageFlagDefines the way component lists are imported and exported
 CTStorageLocationDefines valid storage locations for component list import, export and delete operations
 CTTriggerMomentDefines a trigger moment for a digital signal
 CTUserDataAccessRightDefines valid flags for controlling the user access rights to the user data that can be stored in the devices non-volatile memory
 CTUserDataReconnectBehaviourDefined valid values for the behaviour of the user data when a device has been disconnected and reconnected within a running process
 CTValueTypeAllowed values types for property objects
 CTVideoCodecDefines valid video codecs that might be supported by the underlying video compression engine
 CTVideoStandardDefines valid video standards that might be supported by a video capture device
 CTVirtualDeviceImageTypeDefines valid image types used when capturing data from a certain directory
 CTVirtualDeviceTestModeDefines valid test modes for virtual devices
 CTWhiteBalanceCalibrationModeDefines valid white balance calibration modes
 CTWhiteBalanceParameterDefines valid parameter sets selectable via the WhiteBalance property
 CUserDataA helper class to work with the device specific non-volatile memory(if available)
 CUserDataEntryA helper class that represents one entry in the devices non-volatile memory (if available)
 CUserSetControlCategory that contains the User Set control features
 CVideoStreamA class to create compressed video stream from images captured or loaded using the Impact Acquire API
 CVideoStreamPauseScopeA smaller helper class for pausing a video stream for a defined time
 CWhiteBalancerConvenience class to provide an easy way for a more precise white balance calibration
 CWhiteBalanceSettingsProperties for adjusting the colors during a Bayer conversion