|
Impact Acquire SDK C++
|
| NmvIMPACT | |
| Nacquire | This namespace contains classes and functions belonging to the image acquisition module of this SDK |
| Ndisplay | This namespace contains classes and functions that can be used to display images |
| CImageDisplay | A class that can be used for displaying images within existing windows or GUI elements that can provide a window handle |
| CImageDisplayWindow | A class that can be used to display images in a window |
| NGenICam | This namespace contains classes and functions belonging to the GenICam specific part of the image acquisition module of this SDK |
| Nlabs | This namespace contains classes and functions belonging to the GenICam specific part of the image acquisition module of this SDK that are not yet final and might change in the future without further notice. Yet still we think code within this namespace might prove useful thus we encourage you to use it if beneficial for your application. However be prepared to apply changes when needed. Feedback that helps to improve or finalize code from this namespace will be highly appreciated! A migration guide will be provided and we will perform changes only if they make sense and improve the code |
| CLensControlBase | Contains convenience functions to control features understood by generic lens adapters |
| CLensControlBirger | Contains convenience functions to control features understood by Birger Engineering, Inc. lens adapters |
| CAcquisitionControl | Category for the acquisition and trigger control features |
| CActionControl | Category that contains the Action control features |
| CAnalogControl | Category that contains the Analog control features |
| CChunkDataControl | Category that contains the Chunk Data control features |
| CColorTransformationControl | Category that contains the Color Transformation control features |
| CCounterAndTimerControl | Category that contains the Counter and Timer control features |
| CCustomCommandGenerator | Contains convenience functions to control features understood by a devices custom command interpreter |
| CDataStreamModule | Category that contains items that belong to the data stream module of the transport layer |
| CDepthControl | Adjustment and triggering of the depth image for 3D control |
| CDeviceControl | Category for device information and control |
| CDeviceModule | Category contains items that belong to the device module of the transport layer |
| CDigitalIOControl | Category that contains the digital input and output control features |
| CEncoderControl | Category that contains the quadrature Encoder Control features |
| CEventControl | Category that contains Event control features |
| CFileAccessControl | Category that contains the File Access control features |
| CFileProtocolAdapter | Adapter between the std::iostreambuf and the SFNC Features representing the device file system |
| CGenTLDriverConfigurator | A class that contains items to configure the behaviour of the GenICam GenTL driver stack |
| CGenTLProducerConfiguration | A class that contains items to configure the behaviour of the GenICam GenTL driver stack |
| CIDevFileStreamBase | An output stream buffer derived from std::basic_istream used to read from a file on a device |
| CIDevFileStreamBuf | An input stream buffer derived from std::basic_streambuf used to read from a file of a device |
| CImageFormatControl | Category for Image Format Control features |
| CInterfaceModule | Category that contains items that belong to the interface module of the transport layer |
| CLightControl | Category containing the Lighting control features |
| CLogicBlockControl | Category that contains the Logic Block control features |
| CLUTControl | Category that includes the LUT control features |
| CmvAutoFeatureControl | Contains features to control the image controllers. The properties are applied to Auto Gain Control(AGC) and Auto Exposure Control(AEC) controller. To take effect at least AEC or AGC must be enabled |
| CmvCurrentControl | Category that contains features to control the devices Current Control parameters |
| CmvDefectivePixelCorrectionControl | Contains features to control the device's defective pixel correction parameters |
| CmvFFCControl | Contains features to control the devices Flat Field Correction parameters |
| CmvFrameAverageControl | Category that contains features to control the frame averaging engine |
| CmvHDRControl | Category that contains features to control the devices High Dynamic Range parameters |
| CmvI2cInterfaceControl | Contains features to control the I2C interface |
| CmvLensControl | Contains features to control motorized lenses |
| CmvLogicGateControl | Category that contains features to control the devices Logic Gate Control parameters |
| CmvSerialInterfaceControl | Contains features to control the serial interface |
| CODevFileStreamBase | An output stream buffer derived from std::basic_ostream used to write to a file on a device |
| CODevFileStreamBuf | An output stream buffer derived from std::basic_streambuf used to write to a file on a device |
| COpticControl | Category for optical control features |
| CScan3dControl | Category for control of 3D camera specific features |
| CSequencerControl | Category for the Sequencer Control features |
| CSoftwareSignalControl | Category that contains the Software Signal Control features |
| CSourceControl | Category that contains the source control features |
| CSystemModule | Category that contains items that belong to the system module of the transport layer |
| CTestControl | Category for Test Control features |
| CTransferControl | Category for the data Transfer Control features |
| CTransportLayerControl | Category that contains the transport Layer control features |
| CUserSetControl | Category that contains the User Set control features |
| Nhelper | This namespace contains classes and functions providing convenience access to some or the otherwise more complicated API features. A C++11 or higher compliant compiler is required to use them! |
| CRequestProvider | A helper class that can be used to implement a simple continuous acquisition from a device |
| CThreadSafeQueue | A thread-safe queue |
| Nlabs | This namespace contains classes and functions belonging to the general part of this SDK that are not yet final and might change in the future without further notice. Yet still we think code within this namespace might prove useful thus we encourage you to use it if beneficial for your application. However be prepared to apply changes when needed. Feedback that helps to improve or finalize code from this namespace will be highly appreciated! A migration guide will be provided and we will perform changes only if they make sense and improve the code |
| CVideoStream | A class to create compressed video stream from images captured or loaded using the Impact Acquire API |
| CVideoStreamPauseScope | A smaller helper class for pausing a video stream for a defined time |
| CAutoControlParameters | A class to control the automatic control parameters of a device(Device specific interface layout only) |
| CBasicDeviceSettings | A base class for essential device related settings |
| CBasicDeviceSettingsWithAOI | A base class for camera related settings(Device specific interface layout only) |
| CBufferPart | Contains information about a specific part of a captured buffer |
| CCameraDescriptionBase | A base class to describe a camera (Device specific interface layout only) connected to a frame grabber (deprecated) |
| CCameraDescriptionCameraLink | A class to describe a CameraLink® compliant camera(Device specific interface layout only) (deprecated) |
| CCameraDescriptionDigital | A class to describe a non-standard digital video signal(Device specific interface layout only) (deprecated) |
| CCameraDescriptionDigitalBase | A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated) |
| CCameraDescriptionDigitalBase2 | A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated) |
| CCameraDescriptionManager | Grants access to camera description objects(Device specific interface layout only) (deprecated) |
| CCameraDescriptionNonStandard | A class describing non-standard video cameras(Device specific interface layout only) (deprecated) |
| CCameraDescriptionSDI | A base class to describe an SDI(Serial Digital Interface) camera signal (Device specific interface layout only) (deprecated) |
| CCameraDescriptionStandard | A class describing analogue standard compliant video cameras(Device specific interface layout only) (deprecated) |
| CCameraDescriptionStandardBase | An internal base class to describe standard analogue video cameras(Device specific interface layout only) (deprecated) |
| CCameraSettingsBase | A base class for camera related settings(Device specific interface layout only) |
| CCameraSettingsBlueCOUGAR | mvBlueCOUGAR related camera settings (Device specific interface layout only) |
| CCameraSettingsBlueDevice | A base class for camera related settings belonging to the mvBlueXXX-series (Device specific interface layout only) |
| CCameraSettingsBlueFOX | mvBlueFOX related camera settings(Device specific interface layout only) |
| CCameraSettingsFrameGrabber | A class to access frame grabber related camera settings(Device specific interface layout only) (deprecated) |
| CCameraSettingsV4L2Device | mvV4L2 related camera settings(Device specific interface layout only) |
| CCameraSettingsVirtualDevice | mvVirtualDevice related camera settings(Device specific interface layout only) |
| CChannelData | A structure for image buffer channel specific data |
| CComponent | A base class to implement access to internal driver components |
| CComponentAccess | A base class to implement access to internal driver objects |
| CComponentCallback | A simple helper class to wrap the creation of a callback object |
| CComponentCollection | A base class for sets of properties that can be modified by the user |
| CComponentList | A class to provide access to component lists |
| CComponentLocator | A class to locate components within the driver |
| CComponentLocatorBase | A base class to locate components within the driver |
| CConnector | A class describing how a video signal source(e.g. a camera or image sensor) is connected to a video signal sink(e.g. a frame grabber)(Device specific interface layout only) |
| CDevice | This class and its functions represent an actual device detected by this interface in the current system |
| CDeviceComponentLocator | A class to locate components within the driver |
| CDeviceManager | Grants access to devices that can be operated by this software interface |
| CDigitalInput | A class to represent a digital input pin(Device specific interface layout only) |
| CDigitalIOMeasurementControl | Properties for configuring settings belonging to the digital I/O measurement(Device specific interface layout only) |
| CDigitalOutput | A class to represent a digital output pin(Device specific interface layout only) |
| CECantAccessData | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_LIST_CANT_ACCESS_DATA error |
| CECantAllocateNewList | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_CANT_ALLOCATE_LIST error |
| CECantRegisterComponent | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_CANT_REGISTER_COMPONENT error |
| CECantSerializeData | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_CANT_SERIALIZE_DATA error |
| CEComponent | A base class for mvIMPACT::acquire::Component object related exceptions from the property module |
| CEComponentIDInvalid | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_COMPONENT_ID_INVALID error |
| CEComponentNotFound | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_COMPONENT_NOT_FOUND error |
| CEDeviceManager | A base class for device manager related exceptions |
| CEImplementationMissing | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_IMPLEMENTATION_MISSING error |
| CEIncompatibleComponents | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_INCOMPATIBLE_COMPONENTS error |
| CEInputBufferTooSmall | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_INPUT_BUFFER_TOO_SMALL error |
| CEInvalidFileContent | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_INVALID_FILE_CONTENT error |
| CEInvalidInputParameter | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_INVALID_INPUT_PARAMETER error |
| CEInvalidListID | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_LIST_ID_INVALID error |
| CEInvalidParameterList | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_METHOD_INVALID_PARAM_LIST error |
| CEInvalidValue | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_INVALID_PROP_VALUE error |
| CEInvalidValueType | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_INVALID_PROP_VALUE_TYPE error |
| CEListEntryOccupied | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_LIST_ENTRY_OCCUPIED error |
| CEMethod | A base class for mvIMPACT::acquire::Method object related exceptions from the property module |
| CEMethodPtrInvalid | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_METHOD_PTR_INVALID error |
| CENoModifySizeRights | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_NO_MODIFY_SIZE_RIGHTS error |
| CENoReadRights | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_NO_READ_RIGHTS error |
| CENotAList | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_NOT_A_LIST error |
| CENotAMethod | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_NOT_A_METHOD error |
| CENotAProperty | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_NOT_A_PROPERTY error |
| CENoWriteRights | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_NO_WRITE_RIGHTS error |
| CEnumPropertyF | A template class to represent float properties and enumerated float properties |
| CEnumPropertyI | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CEnumPropertyI64 | A template class to represent 64 bit integer properties and enumerated 64 bit integer properties |
| CEProperty | A base class for mvIMPACT::acquire::Property related exceptions from the property module |
| CEPropertyHandling | A base class for exceptions related to the property module |
| CEPropertyList | A base class for component list related exceptions from the property module |
| CESizeMismatch | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_SIZE_MISMATCH error |
| CETranslationTableCorrupted | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_PROP_TRANSLATION_TABLE_CORRUPTED error |
| CETranslationTableNotDefined | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_PROP_TRANSLATION_TABLE_NOT_DEFINED error |
| CEUnsupportedOperation | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_UNSUPPORTED_OPERATION error |
| CEUnsupportedParameter | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_UNSUPPORTED_PARAMETER error |
| CEValidationFailed | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_PROP_VALIDATION_FAILED error |
| CEValIDOutOfBounds | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_PROP_VAL_ID_OUT_OF_BOUNDS error |
| CEValTooLarge | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_PROP_VAL_TOO_LARGE error |
| CEValTooSmall | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_PROP_VAL_TOO_SMALL error |
| CEWrongParamCount | An exception thrown in case of a mvIMPACT::acquire::PROPHANDLING_WRONG_PARAM_COUNT error |
| CExceptionFactory | A factory class to raise Impact Acquire related exceptions |
| CFirmwareUpdater | A class to perform a firmware update of a specific device |
| CFullSettingsBase | A base class that provides access to the most common settings for a device |
| CFunctionInterface | The function interface to devices supported by this interface |
| CGainOffsetKneeChannelParameters | Properties for configuring settings belonging to a certain channel of the GainOffsetKnee filter |
| CHDRControl | A class to control the HDR (High Dynamic Range) parameters of a device (Device specific interface layout only) |
| CHDRKneePoint | A class to configure a HDR (High Dynamic Range) knee point (Device specific interface layout only) |
| CI2CControl | Properties for accessing features belonging to the I2C control(Device specific interface layout only) |
| CImageBuffer | Fully describes a captured image |
| CImageBufferDesc | A wrapper class to handle mvIMPACT::acquire::ImageBuffer structures |
| CImageDestination | Properties to define the format of resulting images |
| CImageMemoryManager | An interface class to access DMA memory related properties(Device specific interface layout only) (deprecated) |
| CImageProcessing | Base class for image processing related properties |
| CImageRequestControl | A helper class to control the way an image request will be processed |
| CImpactAcquireException | A base class for exceptions generated by Impact Acquire |
| CInfo | A base class to access various general information about the device and its driver |
| CInfoBlueCOUGAR | A more specific class to query information about a mvBlueCOUGAR devices and its driver(Device specific interface layout only) |
| CInfoBlueDevice | A more specific class to query information about a mvBlueDevice device and its driver(Device specific interface layout only) |
| CInfoBlueFOX | A more specific class to query information about a mvBlueFOX device and its driver(Device specific interface layout only) |
| CIOSubSystem | A base class to handle digital inputs and outputs(Device specific interface layout only) |
| CIOSubSystemBlueFOX | A class to handle the digital inputs and outputs for mvBlueFOX USB cameras(Device specific interface layout only) |
| CIOSubSystemCommon | A base class to handle the digital inputs and outputs for devices (Device specific interface layout only) |
| CIOSubSystemFrameGrabber | A class to handle the digital inputs and outputs for frame grabber devices(Device specific interface layout only) (deprecated) |
| CLUTParameters | Properties for configuring settings belonging to a certain LUT (Look Up Table) to be applied to a captured image |
| CMethod | A class to call arbitrary driver functions |
| CMirrorParameters | Properties for configuring settings belonging to the mirror filter that processes a certain channel of a captured image |
| CMotorFocusControl | Properties for configuring settings belonging to the motor focus control (Device specific interface layout only) |
| COutputSignalGeneratorBlueDevice | A class to create complex digital output signals(Device specific interface layout only) |
| COutputSignalGeneratorFrameGrabber | A class to create complex digital output signals(Device specific interface layout only) (deprecated) |
| CProperty | A base class for properties |
| CPropertyPtr | A class to represent pointer properties |
| CPropertyS | A class to represent string properties |
| CPulseStartConfiguration | A class to configure the creation of digital signals passed to one or more of the digital outputs of a device(Device specific interface layout only) |
| CRequest | Contains information about a captured buffer |
| CRequestFactory | A default request factory |
| CRequestInfoConfiguration | Properties to configure which information shall be attached to the resulting images |
| CRTCtrProgram | A class to represent real time control programs(Device specific interface layout only) |
| CRTCtrProgramStep | A class to represent one step of a real time control(RTCtr) program (Device specific interface layout only) |
| CSettingsBlueFOX | This class provides access to general settings as well as to settings which are unique for the mvBlueFOX(Device specific interface layout only) |
| CStatistics | Contains basic statistical information |
| CSyncOutput | A class to represent a sync. output pin(Device specific interface layout only) |
| CSystemBlueFOX | A class containing mvBlueFOX specific settings to control the overall behaviour of the driver(Device specific interface layout only) |
| CSystemSettings | A base class for accessing settings that control the overall behaviour of a device driver |
| CSystemV4L2 | A class containing mvV4L2 specific settings to control the overall behaviour of the driver(Device specific interface layout only) |
| CTriggerControl | A class to configure the behaviour of trigger signals |
| CUserData | A helper class to work with the device specific non-volatile memory(if available) |
| CUserDataEntry | A helper class that represents one entry in the devices non-volatile memory |
| CWhiteBalancer | Convenience class to provide an easy way for a more precise white balance calibration |
| CWhiteBalanceSettings | Properties for adjusting the colors during a Bayer conversion |