Impact Acquire SDK C++
Loading...
Searching...
No Matches
Deprecated List
Member AcquisitionControl::mvAcquisitionMemoryMaxFrameCount
Maximum number of frames that can be recorded in the current configuration(deprecated, use the maximum value of 'mvAcquisitionMemoryFrameCount' instead).
Class CameraDescriptionBase
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class CameraDescriptionCameraLink
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class CameraDescriptionDigital
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class CameraDescriptionDigitalBase
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class CameraDescriptionDigitalBase2
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class CameraDescriptionManager
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member CameraDescriptionManager::CameraDescriptionManager (Device *pDev)
This constructor has been declared deprecated to alarm everyone still using this class.
Class CameraDescriptionNonStandard
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class CameraDescriptionSDI
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class CameraDescriptionStandard
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class CameraDescriptionStandardBase
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class CameraSettingsFrameGrabber
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member CameraSettingsFrameGrabber::CameraSettingsFrameGrabber (Device *pDev, const std::string &settingName="Base")
This constructor has been declared deprecated to alarm everyone still using this class.
Member ChunkDataControl::chunkImageComponent
This feature is deprecated (See ChunkComponentID). It was representing the component of the payload image.
Member ChunkDataControl::chunkPartSelector
This feature is deprecated (See ChunkComponentSelector). It was selecting the individual parts of a multi-component/multi-part buffer to access.
Member DeviceControl::deviceID
This feature is deprecated (See DeviceSerialNumber). It was representing the Device unique identifier (serial number).
Member DeviceControl::deviceMessageChannelCount
This feature is deprecated (See DeviceEventChannelCount). It indicates the number of message/event channels supported by the device.
Member DeviceControl::mvDeviceStatusLEDEnable
This feature is deprecated (See DeviceIndicatorMode). If enabled, the color of the LED changes depending on the state of the camera. Otherwise the LED is Off.
Member DeviceModule::deviceID
This feature is deprecated (See DeviceSerialNumber). It was representing the Device unique identifier (serial number).
Member ImageFormatControl::imageComponentEnable
This feature is deprecated (See ComponentEnable). It was used to control if the selected component streaming is active.
Member ImageFormatControl::imageComponentSelector
This feature is deprecated (See ComponentSelector). It was used to select a component.
Member ImageFormatControl::pixelCoding
This feature is deprecated. It represents the coding of the pixels in the image. Raw gives the data in the native format of the sensor.
Member ImageFormatControl::testImageSelector
This feature is deprecated (See TestPattern). Selects the type of test image that is sent by the device.
Class ImageMemoryManager
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member InterfaceModule::deviceID
This feature is deprecated (See DeviceSerialNumber). It was representing the Device unique identifier (serial number).
Member InterfaceModule::InterfaceModule (mvIMPACT::acquire::Device *pDev, int64_t index)
This constructor has been declared deprecated as it doesn't allow to access features from 3rd party GenTL producers. Use a constructor that allows the selection of the desired GenTL producer instead.
Member InterfaceModule::InterfaceModule (int64_t index)
This constructor has been declared deprecated as it doesn't allow to access features from 3rd party GenTL producers. Use a constructor that allows the selection of the desired GenTL producer instead.
Member InterfaceModule::mvDeviceCommandChannelRetryCount
Indicates the number of retransmissions allowed when command channel message timed out (no ACK was received from the device). This feature has been declared deprecated. Use 'LinkCommandRetryCount' of the DeviceModule instead.
Member InterfaceModule::mvDeviceCommandChannelTransmissionTimeout
Defines the maximum time in milli-seconds the host driver will wait for an ACK from the device to a previously sent command. This feature has been declared deprecated. Use 'LinkCommandTimeout' of the DeviceModule instead.
Class IOSubSystemFrameGrabber
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member IOSubSystemFrameGrabber::IOSubSystemFrameGrabber (Device *pDev)
This constructor has been declared deprecated to alarm everyone still using this class.
Member mvIMPACT::acquire::afAny
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::afAuto
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::afEven
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::afOdd
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::amCentered
Up to version 2.36.0 the AOI had just a size of 50*50 pixels. The behavior was the following:
  • Assume a device that can deliver 640*480 pixels.
  • The user selects to capture an rectangular AOI starting at 100/100 with a width of 200*200 Now in the centered AOI mode a processing function will use a window smaller than the AOI in the middle of the user defined AOI. This e.g. could be a rectangle starting at 150/150 with a width of 100*100.
Member mvIMPACT::acquire::cdfBayer
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cdfBayerPacked
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cdfMono
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cdfRGB
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cdfUnknown
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cdfYUV
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ceseFallingEdge
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ceseNo
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ceseRisingEdge
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cesoAuto
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cesoBlue
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cesoExtern
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cesoGreen
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cesoRed
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::citInterlaced
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::citInvertedInterlaced
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::citNone
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cldvmActive
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cldvmInactive
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::co2xComposite
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::co3GSDI
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::co3xComposite
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::co4xComposite
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coAuto
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coBase
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coComposite
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coDigital
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coFull
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coHDSDI
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coMedium
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ComponentIterator
These days this class is just a typedef mapping the class mvIMPACT::acquire::Component to this type for compatibility reasons. New applications should work with the mvIMPACT::acquire::Component class instead.
Member mvIMPACT::acquire::coRGB
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coSDSDI
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coSVideo
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::coUndefined
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cspbr115200
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cspbr19200
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cspbr230400
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cspbr38400
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cspbr460800
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cspbr57600
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cspbr921600
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::cspbr9600
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dilDeviceSpecific
This interface layout has been declared deprecated for GenICam™ compliant devices(mvBlueCOUGAR-S, mvBlueCOUGAR-X and mvBlueCOUGAR-XD). For these products please use mvIMPACT::acquire::dilGenICam instead. Newer devices like the mvBlueFOX3 will not support this interface layout at all.
Member mvIMPACT::acquire::ditAfterDigOutSignals
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ditImmediately
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::docmRTC
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::docmSoftware
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsNone
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsomInterlaced
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsomNonInterlaced
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsomOff
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseFrame
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseFrameAfterTrigger
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseFVALPassThrough
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseFVALPassThroughInv
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseFVALRisingEdge
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsosePeriodically
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseSyncInFallingEdge
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseSyncInPassThrough
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseSyncInPassThroughInv
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseSyncInRisingEdge
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseTrigger
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseTriggerInPassThrough
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsoseTriggerInPassThroughInv
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsrmAuto
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsrmUser
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal1
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal10
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal11
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal12
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal13
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal14
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal15
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal16
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal2
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal3
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal4
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal5
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal6
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal7
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal8
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dsSignal9
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmFallingEdge
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmLevelHigh
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmLevelLow
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmOff
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmOn
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmOnDemand
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmPeriodically
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmRisingEdge
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmStartFallingStopRising
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtmStartRisingStopFalling
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtoOff
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtoPreviousFrame
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::dtoReadOut
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ecmAuto
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ecmUser
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::efmAuto
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::efmUser
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::imOff
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::imOn
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::InfoBase
This class has been declared deprecated and might not be available in future releases. All features of this class are available in mvIMPACT::acquire::Info as well, so please use this class instead.
Member mvIMPACT::acquire::lcOff
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::lcOn
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::obmmDefault
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::obmmUser
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::scAnalogue
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::scAuto
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::scDigital
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ssITU601
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ssSquare
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::ssUser
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::StatisticsBase
This class has been declared deprecated and might not be available in future releases. All features of this class are available in mvIMPACT::acquire::Statistics as well, so please use this class instead.
Member mvIMPACT::acquire::SystemBase
This class has been declared deprecated and might not be available in future releases. All features of this class are available in mvIMPACT::acquire::SystemSettings as well, so please use this class instead.
Member mvIMPACT::acquire::SystemBlueCOUGAR
This class has been declared deprecated and might not be available in future releases. All features of this class are now available in mvIMPACT::acquire::SystemSettings as well, so please use this class instead.
Member mvIMPACT::acquire::TAcquisitionField
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TCameraDataFormat
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TCameraExternalSyncEdge
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TCameraExternalSyncOutput
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TCameraInterlacedType
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TCameraLinkDataValidMode
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TCameraOutput
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TCameraSerialPortBaudRate
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TClampMode
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TDeviceImageTrigger
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TDeviceScanRateMode
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TDeviceSignalOutputStartEvent
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TDeviceSyncOutMode
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TDeviceTriggerMode
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TDeviceTriggerOverlap
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TDigitalOutputControlMode
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TDigitalSignal
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TFieldGateMode
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TInterlacedMode
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TLineCounter
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TOnBoardMemoryMode
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TScanClock
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member mvIMPACT::acquire::TScanStandard
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Class OutputSignalGeneratorFrameGrabber
Beginning with the release of 3.0.0 of Impact Acquire everything specifically related to frame grabber boards will be considered as deprecated and might be removed without further notice!
Member OutputSignalGeneratorFrameGrabber::OutputSignalGeneratorFrameGrabber (Device *pDev)
This constructor has been declared deprecated to alarm everyone still using this class.
Member Property::isConstDefined (TPropertyLimits constant) const
This function has been declared deprecated and will be removed in future versions of this interface. Use mvIMPACT::acquire::Property::hasMaxValue(), mvIMPACT::acquire::Property::hasMinValue() and mvIMPACT::acquire::Property::hasStepWidth() instead and see the corresponding 'Porting existing code' section in the documentation.
Member TransportLayerControl::gevDeviceClass
This feature is deprecated (See DeviceType). It was representing the class of the device.
Member TransportLayerControl::gevDeviceModeCharacterSet
This feature is deprecated (See DeviceCharacterSet). It was representing the character set used by all the strings of the device.
Member TransportLayerControl::gevDeviceModeIsBigEndian
This feature is deprecated (See DeviceRegistersEndianness). It was representing the Endianness of the device registers.
Member TransportLayerControl::gevGVCPHeartbeatDisable
This feature is deprecated (See DeviceLinkHeartbeatMode). It was used to disable the GVCP heartbeat.
Member TransportLayerControl::gevGVCPPendingTimeout
This feature is deprecated (See DeviceLinkCommandTimeout). It was used to indicate the longest GVCP command execution time before a device returns a PENDING_ACK.
Member TransportLayerControl::gevHeartbeatTimeout
This feature is deprecated (See DeviceLinkHeartbeatTimeout). It was controlling the current heartbeat timeout in milliseconds.
Member TransportLayerControl::gevIEEE1588
This feature is deprecated (See PtpEnable). It was used to enable the IEEE 1588 Precision Time Protocol to control the timestamp register.
Member TransportLayerControl::gevIEEE1588ClockAccuracy
This feature is deprecated (See PtpClockAccurarcy). It was used to indicate the expected accuracy of the device clock when it is the grandmaster, or in the event it becomes the grandmaster.
Member TransportLayerControl::gevIEEE1588Status
This feature is deprecated (See PtpStatus). It was used to Provide the status of the IEEE 1588 clock.
Member TransportLayerControl::gevLinkSpeed
This feature is deprecated (See DeviceLinkSpeed). It was representing the speed of transmission negotiated by the given logical link.
Member TransportLayerControl::gevMessageChannelCount
This feature is deprecated (See DeviceEventChannelCount). It was representing the number of message channels supported by this device.
Member TransportLayerControl::gevNumberOfInterfaces
This feature is deprecated (See DeviceLinkSelector). It was representing the number of logical links supported by this device.
Member TransportLayerControl::gevSCPDirection
This feature is deprecated (See DeviceStreamChannelType). It was used to report the direction of the stream channel.
Member TransportLayerControl::gevSCPSBigEndian
This feature is deprecated (See DeviceStreamChannelEndianness). It was used to control the endianness of multi-byte pixel data for this stream.
Member TransportLayerControl::gevStreamChannelCount
This feature is deprecated (See DeviceStreamChannelCount). It was representing the number of stream channels supported by this device.
Member TransportLayerControl::gevTimestampControlLatch
This feature is deprecated (See TimestampLatch). It was used to latche the current timestamp counter into GevTimestampValue.
Member TransportLayerControl::gevTimestampControlReset
This feature is deprecated (See TimestampReset). It was used to reset the timestamp counter to 0. This feature is not available or as no effect when PTP is used.
Member TransportLayerControl::gevTimestampTickFrequency
This feature is deprecated (See the increment of the TimestampLatchValue feature). It was used to indicate the number of timestamp ticks in 1 second (frequency in Hz). If PTP is used, this feature must return 1,000,000,000 (1 GHz).
Member TransportLayerControl::gevTimestampValue
This feature is deprecated (See TimestampLatchValue). It was used to return the latched 64-bit value of the timestamp counter.
Member TransportLayerControl::gevVersionMajor
This feature is deprecated (See DeviceTLVersionMajor). It was representing the major version of the specification.
Member TransportLayerControl::gevVersionMinor
This feature is deprecated (See DeviceTLVersionMinor). It was representing the minor version of the specification.
Member UserSetControl::userSetDefaultSelector
This feature is deprecated (See UserSetDefault). Selects the feature User Set to load and make active when the device is reset.