|
Impact Acquire SDK C++
|
The tables within this section list all operating systems that are/were supported by Impact Acquire
| Windows® Version | Release Date | First compatible Impact Acquire release | Last compatible Impact Acquire release | |
|---|---|---|---|---|
| Windows® 11 | Oct 05 2021 | 2.18.0 (Dec 13 2016) | ||
| Windows® 10 | Aug 02 2016 (>= 1607) | 64-bit | 2.18.0 (Dec 13 2016) | |
| 32-bit | 2.18.0 (Dec 13 2016) | 3.5.1 (May 23 2025) | ||
| Jul 29 2015 (< 1607) | 64-bit | 2.17.0 (Aug 4 2016) | ||
| 32-bit | 2.17.0 (Aug 4 2016) | 3.5.1 (May 23 2025) | ||
| Windows® 8.1 | Oct 17 2013 | 1.10.64*, a (Mar 2 2009) | 3.4.0b (Nov 14 2024) | |
| Windows® 8 | Oct 26 2012 | 1.10.64*, a (Mar 2 2009) | 3.4.0b (Nov 14 2024) | |
| Windows® 7 | Oct 22 2009 | 1.10.64*, a (Mar 2 2009 | 3.4.0b (Nov 14 2024) | |
| Windows® Vista | Jan 30 2007 | 64-bit | 1.9.3* (May 23 2007) | 3.4.0b (Nov 14 2024) |
| 32-bit | 1.8.6* (Mar 14 2007) | 3.4.0b (Nov 14 2024) | ||
| Windows® XP | Oct 25 2001 | 64-bit | 1.9.3 (May 23 2007) | 2.26.0 (Apr 12 2018) |
| 32-bit | 1.0.0 (Somewhere in 2005) | 2.26.0 (Apr 12 2018) | ||
In contrast to Windows®, on Linux the compiler used to build the SDK is more important than the actual operating system on which the code is intended to run on later. In addition to that the device driver code usually shipped as part of the installation needs to be compatible with the kernel running on the target system. Therefore the Building, Linking And Running Applications Using Impact Acquire (especially for the C/C++ API) as well as the table from the previous chapter are more relevant here.
The following table lists which version of Impact Acquire was built with which version of gcc.
| Impact Acquire version | gcc version[glibc version] (Linux x86_64) | gcc version[glibc version] (Linux ARMhf) | gcc version[glibc version] (Linux ARM64) |
|---|---|---|---|
| < 2.33.0 | 4.2.4[2.8] | 4.6.3[2.14] | 4.8.3[2.14] |
| since 2.33.0 | 4.8.5[2.14] | 4.9.4[2.14] | |
| since 2.50.0 | 5.5.0[2.21] | ||
Using compilers older than that or Linux systems with a glibc smaller than that mentioned in the table above or a libstdc++/libgcc older than bundled with the gcc versions mentioned above will most certainly not work and these systems will not be supported anymore. So in case you are bound to an older Linux system you might want to stick with an appropriate Impact Acquire version as indicated in the table above.
Apart from that the amount of Linux Distributions out there makes it practically impossible to test all these systems and assemble a complete list out of these results. Therefore this section will only present a condensed version of the supported target platforms.
| Target Platform | First compatible Impact Acquire release | Last compatible Impact Acquire release |
|---|---|---|
| ARM64 | 2.17.2 (Sep 21 2016) | |
| ARMhf | 2.11.5 (Nov 24 2014) | |
| ARMsf | 2.11.5 (Nov 24 2014) | 2.37.0 (Mar 03 2020) |
| x86_64 | 1.9.9 (Sep 04 2007) | |
| x86 | 1.0.0 (Somewhere in 2005) | 2.37.0 (Mar 03 2020) |
Although macOS, like Linux, is also based on Unix, macOS is more customer-centric than the majority of Linux-based distributions. Hence we cannot assume developer tools to be available on installations. Therefore building a native version of wxWidgets on the target system is not an option so apps are built and linked with a certain version of wxWidgets during development. This version has to be installed on systems that want to work with the GUI tools coming with the Impact Acquire package. The expected availability of the linked wxWidgets library version via the Homebrew package manager thus also limits the usability of the apps on different macOS versions.
| macOS Version | Release Date | First compatible Impact Acquire release | Availability of the used wxWidgets version | |
|---|---|---|---|---|
| macOS 12 Monterey | Oct 25 2021 | 2.50.0 (Dec 13 2016) | 3.2:no | |
| macOS 13 Ventura | Oct 24 2022 | (2.50.0)* | 3.2:yes | |
| macOS 14 Sonoma | Sep 26 2023 | (2.50.0)** | 3.2:yes | |
| macOS 15 Sequoia | Sep 22 2024 | (2.50.0)*** | 3.2:yes | |
| macOS 26 Tahoe | Sep 22 2025 | (2.50.0)*** | 3.2:yes | |
*: Support for this macOS version has not been verified but should work as well. **: Support for this macOS version has been tested and should work as well. ***: Support for this macOS version has not been tested, but should work as well.
Since version 2.50.0, the native libraries and binaries of Impact Acquire have been compiled using the following compiler:
| Target Platform | First compatible Impact Acquire release | Last compatible Impact Acquire release |
|---|---|---|
| ARM64 | 2.50.0 (Jul 28 2023) |