Balluff - BVS CA-BN Technical Documentation
Toggle main menu visibility
Loading...
Searching...
No Matches
Related Pages
Here is a list of all related documentation pages:
Order Code Nomenclature
What's inside and accessories
Technical Data
Sensor Overview
Summary of CMOS sensors
Filters
APIs And Tools
GenICam™ GenTL Software Stack
The Impact Acquire Software Stack
Developing Applications Using The Impact Acquire SDK
GUI Tools
Relationship Between Framework, Firmware And SDK
GenICam™ And Advanced Features
About Settings
DirectShow Interface
Troubleshooting
Error Code List
Accessing log files
General Issues
The error counter increases
Which PC power settings are useful and possibly necessary?
Why does updating the device list take so long
Windows®
Bluescreen On Machines Running Windows® 10 Or Higher When Streaming Is Started
VLC Media Player Issues
Linux
No GenICam™ devices are detected on a Linux system
DMA Memory
Lost Frames when using NVIDIA® Jetson™ Boards
Capturing Images with Raspberry Pi Not Working
Glossary
Related Manuals
Use Cases
Introducing acquisition / recording possibilities
Acquiring a number of images
Generating very long exposure times
Working with multiple AOIs (mv Multi Area Mode)
Using the BlockScan feature
Working with Event Control
Improving the acquisition / image quality
Correcting image errors of a sensor
Optimizing the color/luminance fidelity of the camera
Setting a flicker-free auto expose and auto gain
Working with binning / decimation
Working with the Dual ADC feature of Sony Gen4 sensors
Working with the dual exposure feature ("mvMultiZone")
Working with triggers
Processing triggers from an incremental encoder
Generating a pulse width modulation (PWM)
Outputting a pulse at every other external trigger
Creating different exposure times for consecutive images
Detecting overtriggering
Triggering of an indefinite sequence with precise starting time
Low latency triggering
Working with I/Os
Controlling strobe or flash at the outputs
Creating a debouncing filter at the inputs
Saving data on the device
Creating user data entries
Creating user set entries
Working with the UserFile section (Flash memory)
Working with device features
Working with the temperature sensors
Reset timestamp by hardware
Synchronizing camera timestamps
Working With The Serial Interface (mv Serial Interface Control)
Working with several cameras simultaneously
Creating synchronized acquisitions
Working with 3rd party tools
Using VLC Media Player
Working with GStreamer - The Impact Acquire GenICam GStreamer Plugin
Appendix A. Specific Camera / Sensor Data
A.1 Pregius CMOS (Mono)
BVS CA-BN2
BVS CA-BN2-0016ZG (1.6 Mpix [1456 x 1088])
Device Feature And Property List
BVS CA-BN2-0032ZG (3.2 Mpix [2064 x 1544])
Device Feature And Property List
BVS CA-BN2-0051ZG (5.1 Mpix [2464 x 2056])
Device Feature And Property List
BVS CA-BN2-0089ZG (8.9 Mpix [4112 x 2176])
Device Feature And Property List
BVS CA-BN2-0124ZG (12.4 Mpix [4112 x 3008])
Device Feature And Property List
BVS CA-BN2-0246AG (24.6 Mpix [5328 x 4608])
Device Feature And Property List
BVS CA-BN4
BVS CA-BN4-0051BG (5.1 Mpix [2464 x 2064])
Device Feature And Property List
BVS CA-BN4-0081ZG (8.1 Mpix [2848 x 2848])
Device Feature And Property List
BVS CA-BN4-0124BG (12.4 Mpix [4128 x 3008])
Device Feature And Property List
BVS CA-BN4-0162ZG (16.2 Mpix [5328 x 3040])
Device Feature And Property List
BVS CA-BN4-0204ZG (20.4 Mpix [4512 x 4512])
Device Feature And Property List
BVS CA-BN4-0246ZG (24.6 Mpix [5328 x 4608])
Device Feature And Property List
A.2 Pregius CMOS (Color)
BVS CA-BN2
BVS CA-BN2-0016ZC (1.6 Mpix [1456 x 1088])
Device Feature And Property List
BVS CA-BN2-0032ZC (3.2 Mpix [2064 x 1544])
Device Feature And Property List
BVS CA-BN2-0051ZC (5.1 Mpix [2464 x 2056])
Device Feature And Property List
BVS CA-BN2-0089ZC (8.9 Mpix [4096 x 2176])
Device Feature And Property List
BVS CA-BN2-0124ZC (12.3 Mpix [4096 x 3008])
Device Feature And Property List
BVS CA-BN2-0246AC (24.6 Mpix [5328 x 4608])
Device Feature And Property List
BVS CA-BN4
BVS CA-BN4-0051BC (5.1 Mpix [2464 x 2064])
Device Feature And Property List
BVS CA-BN4-0081ZC (8.1 Mpix [2848 x 2848])
Device Feature And Property List
BVS CA-BN4-0124BC (12.4 Mpix [4128 x 3008])
Device Feature And Property List
BVS CA-BN4-0162ZC (16.2 Mpix [5328 x 3040])
Device Feature And Property List
BVS CA-BN4-0204ZC (20.4 Mpix [4512 x 4512])
Device Feature And Property List
BVS CA-BN4-0246ZC (24.6 Mpix [5328 x 4608])
Device Feature And Property List
Appendix B. Product Comparison
Appendix C. Tested ARM platforms
C.1 ARM64 based devices
NVIDIA Jetson™ AGX Orin
NVIDIA Jetson™ AGX Xavier
NVIDIA Jetson™ Xavier NX
Raspberry Pi Compute Module 4
i.MX8M Mini
Generated on
3.8.0