Balluff - BVS CA-BN Technical Documentation
Loading...
Searching...
No Matches
NVIDIA Jetson™ AGX Xavier

General

CPUNVIDIA Carmel ARMv8.2 @ 2.26GHz
Cores8
RAM32GB
USB2.0 Interfaces4
USB3.1 Interfaces3
Ethernet10/100/1000 MBit
PCIe1x8 + 1x4 + 1x2 + 2x1
Gen 4.0
Note
The above table describes the specification of the NVIDIA Jetson™ AGX Xavier Developer Kit.
The following tests were conducted on JetPack 4.6.0.

Test Setup

Test setup
Note
The BVS CA-BN device uses 4-lane PCIe 2.0 on the NVIDIA Jetson™ AGX Xavier.

Additional Settings

Set EMC clocks to Maximum

For JetPack >= 5.0.1, it might be necessary (to ensure a reliable data transmission) to set the EMC clock to maximum by calling jetson_clocks with sudo credentials via CLI:

$ sudo jetson_clocks
Note
After executing the above command, the clock will still be reset after the next system boot. A systemd service can be used to run the command line permanently at every system boot.

Benchmarks

The following tests have been performed using different de-Bayering scenarios to achieve the max. FPS while maintaining 0 lost images. The CPU load during the acquisition is also documented below.

Scenarios that have been tested are listed as follows:

  1. When de-Bayering is carried out on the camera: The camera delivers RGB8 image data to the host system. This setting results in a lower CPU load but a lower frame rate.
  2. When de-Bayering is carried out on the host system: The camera delivers Bayer8 image data to the host system. The Bayer8 image data then get de-Bayered to RGB8 format on the host system. This setting results in a higher frame rate but a higher CPU load as well.
  3. When no de-Bayering is performed: The camera delivers Bayer8 image data to the host system. No de-Bayering is performed. This settings results in a lower CPU load and a higher frame rate. The behavior is identical to monochrome cameras.
CameraResolutionPixel FormatFrame Rate [Frames/s]Bandwidth [MB/s]CPU Load With Image DisplayCPU Load Without Image Display
CA-BN2-0051ZC2464 x 2056RGB8 (on camera) → RGB8 (on host)86.831319.88~21%~12%
CameraResolutionPixel FormatFrame Rate [Frames/s]Bandwidth [MB/s]CPU Load With Image DisplayCPU Load Without Image Display
CA-BN2-0051ZC2464 x 2056BayerRG8 (on camera) → RGB8 (on host)138.93703.94~42%~31%
CameraResolutionPixel FormatFrame Rate [Frames/s]Bandwidth [MB/s]CPU Load With Image DisplayCPU Load Without Image Display
CA-BN2-0051ZC2464 x 2056BayerRG8 (on camera) → BayerRG8/Raw (on host)138.93703.97~21%~14%