|
Impact Acquire SDK .NET
|
| CEventArgs | |
| CComponentChangedEventArgs | A class containing data generated by a component changed event |
| CDeviceWillBeClosedEventArgs | A class containing data generated by an event triggered when a device is about to get closed |
| CRequestReadyEventArgs | A class containing data generated by a request ready event fired by instances of the class mv.impact.acquire.helper.RequestProvider |
| CException | |
| CImpactAcquireException | An base class for exceptions generated by Impact Acquire |
| CEDeviceManager | A base class for device manager related exceptions |
| CEPropertyHandling | A base class for exceptions related to the property module |
| CECantAllocateNewList | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_CANT_ALLOCATE_LIST error |
| CECantSerializeData | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_CANT_SERIALIZE_DATA error |
| CEComponent | A base class for mv.impact.acquire.Component object related exceptions from the property module |
| CEIncompatibleComponents | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INCOMPATIBLE_COMPONENTS error |
| CEMethod | A base class for mv.impact.acquire.Method object related exceptions from the property module |
| CEInvalidParameterList | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_METHOD_INVALID_PARAM_LIST error |
| CEMethodPtrInvalid | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_METHOD_PTR_INVALID error |
| CENoModifySizeRights | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NO_MODIFY_SIZE_RIGHTS error |
| CENoReadRights | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NO_READ_RIGHTS error |
| CENoWriteRights | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NO_WRITE_RIGHTS error |
| CENotAList | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NOT_A_LIST error |
| CENotAMethod | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NOT_A_METHOD error |
| CENotAProperty | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_NOT_A_PROPERTY error |
| CEProperty | A base class for mv.impact.acquire.Property related exceptions from the property module |
| CEInvalidValue | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_PROP_VALUE error |
| CEInvalidValueType | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_PROP_VALUE_TYPE error |
| CETranslationTableCorrupted | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_TRANSLATION_TABLE_CORRUPTED error |
| CETranslationTableNotDefined | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_TRANSLATION_TABLE_NOT_DEFINED error |
| CEValIDOutOfBounds | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VAL_ID_OUT_OF_BOUNDS error |
| CEValTooLarge | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VAL_TOO_LARGE error |
| CEValTooSmall | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VAL_TOO_SMALL error |
| CEValidationFailed | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_PROP_VALIDATION_FAILED error |
| CEPropertyList | A base class for component list related exceptions from the property module |
| CECantAccessData | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_LIST_CANT_ACCESS_DATA error |
| CECantRegisterComponent | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_CANT_REGISTER_COMPONENT error |
| CEComponentIDInvalid | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_COMPONENT_ID_INVALID error |
| CEComponentNotFound | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_COMPONENT_NOT_FOUND error |
| CEInvalidListID | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_LIST_ID_INVALID error |
| CEListEntryOccupied | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_LIST_ENTRY_OCCUPIED error |
| CEImplementationMissing | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_IMPLEMENTATION_MISSING error |
| CEInputBufferTooSmall | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INPUT_BUFFER_TOO_SMALL error |
| CEInvalidFileContent | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_FILE_CONTENT error |
| CEInvalidInputParameter | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_INVALID_INPUT_PARAMETER error |
| CESizeMismatch | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_SIZE_MISMATCH error |
| CEUnsupportedOperation | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_UNSUPPORTED_OPERATION error |
| CEUnsupportedParameter | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_UNSUPPORTED_PARAMETER error |
| CEWrongParamCount | An exception thrown in case of a mv.impact.acquire.TPROPHANDLING_ERROR.PROPHANDLING_WRONG_PARAM_COUNT error |
| CIDisposable | |
| CFunctionInterface | The function interface to devices supported by this interface |
| CDevFileStream | A helper class derived from System.IO.Stream used to read from and write to a file on a device |
| CRequestBitmapData | A class containing a reference to a bitmap created from a request |
| CImageDisplay | A class that can be used for displaying images within existing windows or GUI elements that can provide a window handle |
| CImageDisplayWindow | A class that can be used to display images in a window |
| CRequestReadyEventData | A class containing data stored inside a mv.impact.acquire.helper.RequestReadyEventArgs event fired by instances of the class mv.impact.acquire.helper.RequestProvider when a new mv.impact.acquire.Request became ready |
| CVideoStreamPauseScope | A smaller helper class for pausing a video stream for a defined time |
| CIEnumerable | |
| CComponentCollection | A base class for sets of properties that can be modified by the user |
| CAutoControlParameters | A class to control the automatic control parameters of a device(Device specific interface layout only) |
| CBasicDeviceSettings | A base class for essential device related settings |
| CCameraSettingsBase | A base class for camera related settings(Device specific interface layout only) |
| CCameraSettingsBlueDevice | A base class for camera related settings belonging to the mvBlueXXX-series (Device specific interface layout only) |
| CCameraSettingsBlueCOUGAR | mvBlueCOUGAR related camera settings (Device specific interface layout only) |
| CCameraSettingsBlueFOX | mvBlueFOX related camera settings (Device specific interface layout only) |
| CCameraSettingsFrameGrabber | A class to access frame grabber related camera settings (Device specific interface layout only) |
| CCameraSettingsVirtualDevice | mvVirtualDevice related camera settings (Device specific interface layout only) |
| CBufferPart | Contains information about a specific part of a captured buffer |
| CCameraDescriptionBase | A base class to describe a camera(Device specific interface layout only) connected to a frame grabber |
| CCameraDescriptionDigitalBase | A base class to describe an arbitrary digital camera signal (Device specific interface layout only) |
| CCameraDescriptionDigitalBase2 | A base class to describe an arbitrary digital camera signal (Device specific interface layout only) |
| CCameraDescriptionCameraLink | A class to describe a CameraLink® compliant camera (Device specific interface layout only) |
| CCameraDescriptionDigital | A class to describe a non-standard digital video signal (Device specific interface layout only) |
| CCameraDescriptionSDI | A base class to describe a SDI (Serial Digital Interface) camera signal (Device specific interface layout only) |
| CCameraDescriptionStandard | A class describing analogue standard compliant video cameras (Device specific interface layout only) |
| CCameraDescriptionNonStandard | A class describing non-standard video cameras (Device specific interface layout only) |
| CConnector | A class describing how a video signal source(e.g. a camera or image sensor) is connected to a video signal sink (e.g. a frame grabber) (Device specific interface layout only) |
| CDigitalIOMeasurementControl | Properties for configuring settings belonging to the digital I/O measurement(Device specific interface layout only) |
| CGainOffsetKneeChannelParameters | Properties for configuring settings belonging to a certain channel of the GainOffsetKnee filter |
| CDataStreamModule | Category that contains items that belong to the data stream module of the transport layer |
| CDepthControl | Adjustment and triggering of the depth image for 3D control |
| CDeviceModule | Category contains items that belong to the device module of the transport layer |
| CGenTLDriverConfigurator | A class that contains items to configure the behaviour of the GenICam GenTL driver stack |
| CGenTLProducerConfiguration | A class that contains items to configure the behaviour of the GenICam GenTL driver stack |
| CInterfaceModule | Category that contains items that belong to the interface module of the transport layer |
| CSystemModule | Category that contains items that belong to the system module of the transport layer |
| CmvAutoFeatureControl | Contains features to control the image controllers. The properties are applied to Auto Gain Control(AGC) and Auto Exposure Control(AEC) controller. To take effect at least AEC or AGC must be enabled |
| CmvCurrentControl | Category that contains features to control the devices Current Control parameters |
| CmvDefectivePixelCorrectionControl | Contains features to control the device's defective pixel correction parameters |
| CmvFFCControl | Contains features to control the devices Flat Field Correction parameters |
| CmvFrameAverageControl | Category that contains features to control the frame averaging engine |
| CmvHDRControl | Category that contains features to control the devices High Dynamic Range parameters |
| CmvLensControl | Contains features to control motorized lenses |
| CmvLogicGateControl | Category that contains features to control the devices Logic Gate Control parameters |
| CmvPoDLDeviceControl | Category for device information and control |
| CmvPoDLPortControl | Category for status and control features for the camera ports |
| CmvSerialInterfaceControl | Contains features to control the serial interface |
| CHDRControl | A class to control the HDR (High Dynamic Range) parameters of a device (Device specific interface layout only) |
| CHDRKneePoint | A class to configure a HDR (High Dynamic Range) knee point (Device specific interface layout only) |
| CI2CControl | Properties for accessing features belonging to the I2C control(Device specific interface layout only) |
| CImageDestination | Properties to define the format of resulting images |
| CImageMemoryManager | An interface class to access DMA memory related properties(Device specific interface layout only) |
| CImageProcessing | Base class for image processing related properties |
| CImageRequestControl | A helper class to control the way an image request will be processed |
| CInfo | A class to query various general information about the device, its driver and other information |
| CInfoBlueDevice | A more specific class to query information about a mvBlueDevice device and its driver (Device specific interface layout only) |
| CInfoBlueCOUGAR | A more specific class to query information about a mvBlueCOUGAR devices and its driver (Device specific interface layout only) |
| CInfoBlueFOX | A more specific class to query information about a mvBlueFOX device and its driver (Device specific interface layout only) |
| CLUTParameters | Properties for configuring settings belonging to a certain LUT (Look Up Table) to be applied to a captured image |
| CMirrorParameters | Properties for configuring settings belonging to the mirror filter that processes a certain channel of a captured image |
| CMotorFocusControl | Properties for configuring settings belonging to the motor focus control (Device specific interface layout only) |
| COutputSignalGeneratorBlueDevice | A class to create complex digital output signals(Device specific interface layout only) |
| COutputSignalGeneratorFrameGrabber | A class to create complex digital output signals(Device specific interface layout only) |
| CPulseStartConfiguration | A class to configure the creation of digital signals passed to one or more of the digital outputs of a device(Device specific interface layout only) |
| CRTCtrProgram | A class to represent real time control programs (Device specific interface layout only) |
| CRTCtrProgramStep | A class to represent one step of a real time control (RTCtr) program (Device specific interface layout only) |
| CRequest | Contains information about a captured buffer |
| CRequestInfoConfiguration | Properties to configure which information shall be attached to the resulting images |
| CStatistics | Contains statistical information |
| CSyncOutput | A class to represent a sync. output pin(Device specific interface layout only) |
| CSystemSettings | A class for accessing general settings that control the overall behaviour of a device driver |
| CSystemBlueFOX | A class containing mvBlueFOX specific settings to control the overall behaviour of the driver(Device specific interface layout only) |
| CTriggerControl | A class to configure the behaviour of trigger signals |
| CWhiteBalanceSettings | Properties for adjusting the colors during a Bayer conversion |
| CComponentList | A class to provide access to component lists |
| CCameraDescriptionManager | Grants access to camera description objects (Device specific interface layout only) |
| CComponentAccess | A base class to implement access to internal driver objects |
| CComponent | A base class to implement access to internal driver components |
| CComponentList | A class to provide access to component lists |
| CMethod | A class to call arbitrary driver functions |
| CProperty | A base class for properties |
| CEnumPropertyF< T > | A template class to represent float properties and enumerated float properties |
| CPropertyF | Provided for convenience only. This type represents a standard float property type |
| CEnumPropertyI64< T > | A template class to represent 64-bit integer properties and enumerated 64 bit integer properties |
| CPropertyI64 | Provided for convenience only. This type represents a standard 64-bit integer property type |
| CEnumPropertyI< T > | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyI | Provided for convenience only. This type represents a standard 32-bit integer property type |
| CPropertyIBoolean | Provided for convenience only. This type represents a standard boolean property type |
| CPropertyPtr | A class to represent pointer properties |
| CPropertyS | A class to represent string properties |
| CComponentLocatorBase | A base class to locate components within the driver |
| CComponentLocator | A class to locate components within the driver |
| CDeviceComponentLocator | A class to locate components within the driver |
| CComponentCallback | A simple helper class to wrap the creation of a callback object |
| CDevice | This class and its functions represent an actual device detected by this interface in the current system |
| CDeviceManager | Grants access to devices that can be operated by this software interface |
| CDigitalIO | An abstract base class to represent a digital pin(Device specific interface layout only) |
| CDigitalInput | A class to represent a digital input pin(Device specific interface layout only) |
| CDigitalOutput | A class to represent a digital output pin(Device specific interface layout only) |
| CImageDisplayExtensions | Additional methods to extend the functionality of the class mv.impact.acquire.display.ImageDisplay |
| CExceptionFactory | A factory class to raise Impact Acquire related exceptions |
| CFirmwareUpdater | A class to perform a firmware update of a specific device |
| CFullSettingsBase | A base class that provides access to the most common settings for a device |
| CSettingsBlueFOX | This class provides access to general settings as well as to settings which are unique for the mvBlueFOX (Device specific interface layout only) |
| CAcquisitionControl | Category for the acquisition and trigger control features |
| CActionControl | Category that contains the Action control features |
| CAnalogControl | Category that contains the Analog control features |
| CChunkDataControl | Category that contains the Chunk Data control features |
| CColorTransformationControl | Category that contains the Color Transformation control features |
| CCounterAndTimerControl | Category that contains the Counter and Timer control features |
| CCustomCommandGenerator | Contains convenience functions to control features understood by a devices custom command interpreter |
| CDeviceControl | Category for device information and control |
| CDigitalIOControl | Category that contains the digital input and output control features |
| CEncoderControl | Category that contains the quadrature Encoder Control features |
| CEventControl | Category that contains Event control features |
| CFileAccessControl | Category that contains the File Access control features |
| CImageFormatControl | Category for Image Format Control features |
| CLensControlBase | Contains convenience functions to control features understood by generic lens adapters |
| CLensControlBirger | Contains convenience functions to control features understood by Birger Engineering, Inc. lens adapters |
| CLightControl | Category containing the Lighting control features |
| CLogicBlockControl | Category that contains the Logic Block control features |
| CLUTControl | Category that includes the LUT control features |
| CmvCameraIOPortControl | Category for Camera I/O Port Control features |
| CmvI2cInterfaceControl | Contains features to control the I2C interface |
| CmvIODeviceControl | Category for system wide I/O Control features |
| CmvSupplyVoltageControl | Category for controlling the supply voltages |
| CmvTriggerGeneratorControl | Category for controlling the trigger generator |
| COpticControl | Category for optical control features |
| CScan3dControl | Category for control of 3D camera specific features |
| CSequencerControl | Category for the Sequencer Control features |
| CSoftwareSignalControl | Category that contains the Software Signal Control features |
| CSourceControl | Category that contains the source control features |
| CTestControl | Category for Test Control features |
| CTransferControl | Category for the data Transfer Control features |
| CTransportLayerControl | Category that contains the transport Layer control features |
| CUserSetControl | Category that contains the User Set control features |
| CIntPtrExtension | Additional methods to extend the System.IntPtr structure's functionality |
| CIRequestBuffer | A default request buffer |
| CUserSuppliedHeapBuffer | A small helper class to create a user supplied buffer on the heap |
| CRequestProvider | A helper class that can be used to create a simple continuous acquisition from a device |
| CIOSubSystem | A base class to handle digital inputs and outputs (Device specific interface layout only) |
| CIOSubSystemBlueFOX | A class to handle the digital inputs and outputs for mvBlueFOX USB cameras (Device specific interface layout only) |
| CIOSubSystemCommon | A base class to handle the digital inputs and outputs for devices (Device specific interface layout only) |
| CIOSubSystemFrameGrabber | A class to handle the digital inputs and outputs for frame grabber devices (Device specific interface layout only) |
| CIRequestFactory | A default request factory |
| CVideoStream | A class to create compressed video stream from images captured or loaded using the Impact Acquire API |
| CLibraryPath | A small helper class to administer various library search path related variables and paths |
| CSystemDrawingBitmapSupport | A class to Bitmap support for .NET applications on supported platforms |
| CTImageBufferPixelFormatExtension | Additional methods to extend the functionality of the mv.impact.acquire.TImageBufferPixelFormat enumeration |
| CTImageDestinationPixelFormatExtension | Additional methods to extend the functionality of the mv.impact.acquire.TImageDestinationPixelFormat enumeration |
| CUserData | A helper class to work with the device specific non-volatile memory(if available) |
| CUserDataEntry | A helper class that represents one entry in the devices non-volatile memory (if available) |
| CWhiteBalancer | Convenience class to provide an easy way for a more precise white balance calibration |
| CStream | |
| CDevFileStream | A helper class derived from System.IO.Stream used to read from and write to a file on a device |