|
Impact Acquire SDK Python
|
| NmvIMPACT | |
| Nacquire | |
| CAcquisitionControl | Category for the acquisition and trigger control features |
| CActionControl | Category that contains the Action control features |
| CAnalogControl | Category that contains the Analog control features |
| CAutoControlParameters | A class to control the automatic control parameters of a device(Device specific interface layout only) |
| CBasicDeviceSettings | A base class for essential device related settings |
| CBasicDeviceSettingsWithAOI | A base class for camera related settings(Device specific interface layout only) |
| CBufferPart | Contains information about a specific part of a captured buffer |
| CCameraDescriptionBase | A base class to describe a camera (Device specific interface layout only) connected to a frame grabber (deprecated) |
| CCameraDescriptionCameraLink | A class to describe a CameraLink® compliant camera(Device specific interface layout only) (deprecated) |
| CCameraDescriptionDigital | A class to describe a non-standard digital video signal(Device specific interface layout only) (deprecated) |
| CCameraDescriptionDigitalBase | A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated) |
| CCameraDescriptionDigitalBase2 | A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated) |
| CCameraDescriptionManager | Grants access to camera description objects(Device specific interface layout only) (deprecated) |
| CCameraDescriptionNonStandard | A class describing non-standard video cameras(Device specific interface layout only) (deprecated) |
| CCameraDescriptionSDI | A base class to describe an SDI(Serial Digital Interface) camera signal (Device specific interface layout only) (deprecated) |
| CCameraDescriptionStandard | A class describing analogue standard compliant video cameras(Device specific interface layout only) (deprecated) |
| CCameraDescriptionStandardBase | An internal base class to describe standard analogue video cameras(Device specific interface layout only) (deprecated) |
| CCameraSettingsBase | A base class for camera related settings(Device specific interface layout only) |
| CCameraSettingsBlueCOUGAR | mvBlueCOUGAR related camera settings (Device specific interface layout only) |
| CCameraSettingsBlueDevice | A base class for camera related settings belonging to the mvBlueXXX-series (Device specific interface layout only) |
| CCameraSettingsBlueFOX | mvBlueFOX related camera settings(Device specific interface layout only) |
| CCameraSettingsFrameGrabber | A class to access frame grabber related camera settings(Device specific interface layout only) (deprecated) |
| CCameraSettingsV4L2Device | mvV4L2 related camera settings(Device specific interface layout only) |
| CCameraSettingsVirtualDevice | mvVirtualDevice related camera settings(Device specific interface layout only) |
| CChannelData | A structure for image buffer channel specific data Channel specific data in an image is data, that in e.g |
| CChunkDataControl | Category that contains the Chunk Data control features |
| CColorTransformationControl | Category that contains the Color Transformation control features |
| CComponent | A base class to implement access to internal driver components |
| CComponentAccess | A base class to implement access to internal driver objects |
| CComponentCallback | A simple helper class to wrap the creation of a callback object |
| CComponentCollection | A base class for sets of properties that can be modified by the user |
| CComponentList | A class to provide access to component lists |
| CComponentLocator | A class to locate components within the driver |
| CComponentLocatorBase | A base class to locate components within the driver |
| CConnector | A class describing how a video signal source(e.g |
| CCounterAndTimerControl | Category that contains the Counter and Timer control features |
| CCustomCommandGenerator | Contains convenience functions to control features understood by a devices custom command interpreter |
| CDataStreamModule | Category that contains items that belong to the data stream module of the transport layer |
| CDepthControl | Adjustment and triggering of the depth image for 3D control |
| CDevice | This class and its functions represent an actual device detected by this interface in the current system |
| CDeviceComponentLocator | A class to locate components within the driver |
| CDeviceControl | Classes and functions that will be available if the device is used with the GenICam interface layout |
| CDeviceManager | Grants access to devices that can be operated by this software interface |
| CDeviceModule | Category contains items that belong to the device module of the transport layer |
| CDigitalInput | A class to represent a digital input pin(Device specific interface layout only) |
| CDigitalIOControl | Category that contains the digital input and output control features |
| CDigitalIOMeasurementControl | Properties for configuring settings belonging to the digital I/O measurement(Device specific interface layout only) |
| CDigitalOutput | A class to represent a digital output pin(Device specific interface layout only) |
| CECantAccessData | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_LIST_CANT_ACCESS_DATA error |
| CECantAllocateNewList | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_CANT_ALLOCATE_LIST error |
| CECantRegisterComponent | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_CANT_REGISTER_COMPONENT error |
| CECantSerializeData | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_CANT_SERIALIZE_DATA error |
| CEComponent | A base class for mvIMPACT.acquire.Component object related exceptions from the property module |
| CEComponentIDInvalid | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_COMPONENT_ID_INVALID error |
| CEComponentNotFound | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_COMPONENT_NOT_FOUND error |
| CEDeviceManager | A base class for device manager related exceptions |
| CEImplementationMissing | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_IMPLEMENTATION_MISSING error |
| CEIncompatibleComponents | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_INCOMPATIBLE_COMPONENTS error |
| CEInputBufferTooSmall | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_INPUT_BUFFER_TOO_SMALL error |
| CEInvalidFileContent | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_INVALID_FILE_CONTENT error |
| CEInvalidInputParameter | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_INVALID_INPUT_PARAMETER error |
| CEInvalidListID | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_LIST_ID_INVALID error |
| CEInvalidParameterList | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_METHOD_INVALID_PARAM_LIST error |
| CEInvalidValue | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_INVALID_PROP_VALUE error |
| CEInvalidValueType | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_INVALID_PROP_VALUE_TYPE error |
| CEListEntryOccupied | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_LIST_ENTRY_OCCUPIED error |
| CEMethod | A base class for mvIMPACT.acquire.Method object related exceptions from the property module |
| CEMethodPtrInvalid | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_METHOD_PTR_INVALID error |
| CEncoderControl | Category that contains the quadrature Encoder Control features |
| CENoModifySizeRights | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_NO_MODIFY_SIZE_RIGHTS error |
| CENoReadRights | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_NO_READ_RIGHTS error |
| CENotAList | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_NOT_A_LIST error |
| CENotAMethod | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_NOT_A_METHOD error |
| CENotAProperty | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_NOT_A_PROPERTY error |
| CENoWriteRights | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_NO_WRITE_RIGHTS error |
| CEProperty | A base class for mvIMPACT.acquire.Property related exceptions from the property module |
| CEPropertyHandling | A base class for exceptions related to the property module |
| CEPropertyList | A base class for component list related exceptions from the property module |
| CESizeMismatch | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_SIZE_MISMATCH error |
| CETranslationTableCorrupted | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_PROP_TRANSLATION_TABLE_CORRUPTED error |
| CETranslationTableNotDefined | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_PROP_TRANSLATION_TABLE_NOT_DEFINED error |
| CEUnsupportedOperation | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_UNSUPPORTED_OPERATION error |
| CEUnsupportedParameter | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_UNSUPPORTED_PARAMETER error |
| CEValidationFailed | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_PROP_VALIDATION_FAILED error |
| CEValIDOutOfBounds | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_PROP_VAL_ID_OUT_OF_BOUNDS error |
| CEValTooLarge | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_PROP_VAL_TOO_LARGE error |
| CEValTooSmall | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_PROP_VAL_TOO_SMALL error |
| CEventControl | Category that contains Event control features |
| CEWrongParamCount | An exception thrown in case of a mvIMPACT.acquire.PROPHANDLING_WRONG_PARAM_COUNT error |
| CExceptionFactory | A factory class to raise Impact Acquire related exceptions |
| CFileAccessControl | Category that contains the File Access control features |
| CFirmwareUpdater | A class to perform a firmware update of a specific device |
| CFullSettingsBase | A base class that provides access to the most common settings for a device |
| CFunctionInterface | The function interface to devices supported by this interface |
| CGainOffsetKneeChannelParameters | Properties for configuring settings belonging to a certain channel of the GainOffsetKnee filter |
| CGenTLDriverConfigurator | A class that contains items to configure the behaviour of the GenICam GenTL driver stack |
| CGenTLProducerConfiguration | A class that contains items to configure the behaviour of the GenICam GenTL driver stack |
| CHDRControl | A class to control the HDR (High Dynamic Range) parameters of a device (Device specific interface layout only) |
| CHDRKneePoint | A class to configure a HDR (High Dynamic Range) knee point (Device specific interface layout only) |
| CI2CControl | Properties for accessing features belonging to the I2C control(Device specific interface layout only) |
| CImageBuffer | Fully describes a captured image |
| CImageBufferDesc | A wrapper class to handle mvIMPACT.acquire.ImageBuffer structures |
| CImageDestination | Properties to define the format of resulting images |
| CImageDisplay | A class that can be used for displaying images within existing windows or GUI elements that can provide a window handle |
| CImageDisplayWindow | A class that can be used to display images in a window |
| CImageFormatControl | Category for Image Format Control features |
| CImageMemoryManager | An interface class to access DMA memory related properties(Device specific interface layout only) (deprecated) |
| CImageProcessing | Base class for image processing related properties |
| CImageRequestControl | A helper class to control the way an image request will be processed |
| CImpactAcquireException | A base class for exceptions generated by Impact Acquire |
| CInfo | A base class to access various general information about the device and its driver |
| CInfoBlueCOUGAR | A more specific class to query information about a mvBlueCOUGAR devices and its driver(Device specific interface layout only) |
| CInfoBlueDevice | A more specific class to query information about a mvBlueDevice device and its driver(Device specific interface layout only) |
| CInfoBlueFOX | A more specific class to query information about a mvBlueFOX device and its driver(Device specific interface layout only) |
| CInterfaceModule | Category that contains items that belong to the interface module of the transport layer |
| CIOSubSystem | A base class to handle digital inputs and outputs(Device specific interface layout only) |
| CIOSubSystemBlueFOX | A class to handle the digital inputs and outputs for mvBlueFOX USB cameras(Device specific interface layout only) |
| CIOSubSystemCommon | A base class to handle the digital inputs and outputs for devices (Device specific interface layout only) |
| CIOSubSystemFrameGrabber | A class to handle the digital inputs and outputs for frame grabber devices(Device specific interface layout only) (deprecated) |
| CLightControl | Category containing the Lighting control features |
| CLogicBlockControl | Category that contains the Logic Block control features |
| CLUTControl | Category that includes the LUT control features |
| CLUTParameters | Properties for configuring settings belonging to a certain LUT (Look Up Table) to be applied to a captured image |
| CMethod | A class to call arbitrary driver functions |
| CMirrorParameters | Properties for configuring settings belonging to the mirror filter that processes a certain channel of a captured image |
| CMotorFocusControl | Properties for configuring settings belonging to the motor focus control (Device specific interface layout only) |
| CmvAutoFeatureControl | Contains features to control the image controllers |
| CmvCameraIOPortControl | Category for Camera I/O Port Control features |
| CmvCurrentControl | Category that contains features to control the devices Current Control parameters |
| CmvDefectivePixelCorrectionControl | Contains features to control the device's defective pixel correction parameters |
| CmvFFCControl | Contains features to control the devices Flat Field Correction parameters |
| CmvFrameAverageControl | Category that contains features to control the frame averaging engine |
| CmvHDRControl | Category that contains features to control the devices High Dynamic Range parameters |
| CmvI2cInterfaceControl | Contains features to control the I2C interface |
| CmvIODeviceControl | Category for system wide I/O Control features |
| CmvLensControl | Contains features to control motorized lenses Contains features to control motorized lenses |
| CmvLogicGateControl | Category that contains features to control the devices Logic Gate Control parameters |
| CmvPoDLDeviceControl | Category for device information and control |
| CmvPoDLPortControl | Category for status and control features for the camera ports Category for status and control features for the camera ports |
| CmvSerialInterfaceControl | Contains features to control the serial interface |
| CmvSupplyVoltageControl | Category for controlling the supply voltages |
| CmvTriggerGeneratorControl | Category for controlling the trigger generator |
| COpticControl | Category for optical control features |
| COutputSignalGeneratorBlueDevice | A class to create complex digital output signals(Device specific interface layout only) |
| COutputSignalGeneratorFrameGrabber | A class to create complex digital output signals(Device specific interface layout only) (deprecated) |
| CProperty | A base class for properties |
| CPropertyF | A template class to represent float properties and enumerated float properties |
| CPropertyI | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyI64 | A template class to represent 64 bit integer properties and enumerated 64 bit integer properties |
| CPropertyI64BayerMosaicParity | A template class to represent 64 bit integer properties and enumerated 64 bit integer properties |
| CPropertyI64BufferPartDataType | A template class to represent 64 bit integer properties and enumerated 64 bit integer properties |
| CPropertyI64DeviceTriggerOverlap | A template class to represent 64 bit integer properties and enumerated 64 bit integer properties |
| CPropertyIAcquisitionField | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIAcquisitionMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIAcquisitionStartStopBehaviour | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIAoiMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIAutoControlMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIAutoControlSpeed | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIAutoExposureControl | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIAutoGainControl | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIAutoOffsetCalibration | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBayerConversionMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBayerMosaicParity | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBayerWhiteBalanceResult | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBlueFOXDigitalInputThreshold | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBlueFOXFooterMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBlueFOXInfoSensorCapabilities | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBlueFOXOffsetAutoBlackSpeed | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBlueFOXSensorTiming | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBlueFOXTransferSize | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIBoolean | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraAoiMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraBinningMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraDataFormat | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraExposeMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraExternalSyncEdge | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraExternalSyncOutput | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraFlashMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraFlashType | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraHDRMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraInterlacedType | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraLinkDataValidMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraOutput | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraPixelClock | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraScanMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraSerialPortBaudRate | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraShutterMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraTapsXGeometry | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraTapsYGeometry | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraTestMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraTriggerMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyICameraTriggerSource | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIChannelSplitMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIClampMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIColorProcessingMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIColorTwistInputCorrectionMatrixMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIColorTwistOutputCorrectionMatrixMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDarkCurrentFilterMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDefectivePixelsFilterMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceAccessMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceAdvancedOptions | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceCapability | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceClass | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceDigitalOutputMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceImageTrigger | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceInterfaceLayout | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceLoadSettings | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDevicePowerMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceScanRateMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceSignalOutputStartEvent | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceState | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceSyncOutMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceTriggerInterface | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDeviceTriggerMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDigIOState | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDigitalIOMeasurementMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDigitalIOMeasurementSource | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDigitalOutputControlMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIDigitalSignal | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIFieldGateMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIFlatFieldFilterCorrectionMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIFlatFieldFilterMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIHWUpdateResult | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyII2COperationMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyII2COperationStatus | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIImageBufferFormatReinterpreterMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIImageBufferPixelFormat | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIImageDestinationPixelFormat | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIImageProcessingFilter | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIImageProcessingMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIImageProcessingOptimization | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIImageProcessingResult | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIImageRequestControlMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIInfoSensorColorMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIInfoSensorType | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIInterfaceEnumerationBehaviour | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIInterlacedMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyILineCounter | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyILUTGammaMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyILUTImplementation | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyILUTInterpolationMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyILUTMapping | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyILUTMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIMemoryManagerMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIMemoryManagerPoolMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIMirrorMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIMirrorOperationMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIOnBoardMemoryMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIPayloadType | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIPolarizedDataExtractionInterpolationMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIPolarizedDataExtractionMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIPulseStartTrigger | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIRequestImageMemoryMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIRequestResult | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIRequestState | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIRTCtrlModes | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIRTProgOpCodes | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIScalerInterpolationMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIScalerMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIScanClock | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIScanStandard | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyITriggerMoment | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIUserDataAccessRight | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIUserDataReconnectBehaviour | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIVideoStandard | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIVirtualDeviceImageType | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIVirtualDeviceTestMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIWhiteBalanceCalibrationMode | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyIWhiteBalanceParameter | A template class to represent 32 bit integer properties and 32 bit enumerated integer properties |
| CPropertyPtr | A class to represent pointer properties |
| CPropertyS | A class to represent string properties |
| CPulseStartConfiguration | A class to configure the creation of digital signals passed to one or more of the digital outputs of a device(Device specific interface layout only) |
| CRequest | Contains information about a captured buffer |
| CRequestFactory | A default request factory |
| CRequestInfoConfiguration | Properties to configure which information shall be attached to the resulting images |
| CRTCtrProgram | A class to represent real time control programs(Device specific interface layout only) |
| CRTCtrProgramStep | A class to represent one step of a real time control(RTCtr) program (Device specific interface layout only) |
| CScan3dControl | Category for control of 3D camera specific features |
| CSequencerControl | Category for the Sequencer Control features |
| CSettingsBlueFOX | This class provides access to general settings as well as to settings which are unique for the mvBlueFOX(Device specific interface layout only) |
| CSoftwareSignalControl | Category that contains the Software Signal Control features |
| CSourceControl | Category that contains the source control features |
| CStatistics | Contains basic statistical information |
| CSwigPyIterator | |
| CSyncOutput | A class to represent a sync |
| CSystemBlueFOX | A class containing mvBlueFOX specific settings to control the overall behaviour of the driver(Device specific interface layout only) |
| CSystemModule | Category that contains items that belong to the system module of the transport layer |
| CSystemSettings | A base class for accessing settings that control the overall behaviour of a device driver |
| CSystemV4L2 | A class containing mvV4L2 specific settings to control the overall behaviour of the driver(Device specific interface layout only) |
| CTestControl | Category for Test Control features |
| CTransferControl | Category for the data Transfer Control features |
| CTransportLayerControl | Category that contains the transport Layer control features |
| CTriggerControl | A class to configure the behaviour of trigger signals |
| CUserData | A helper class to work with the device specific non-volatile memory(if available) |
| CUserDataEntry | A helper class that represents one entry in the devices non-volatile memory (if available) |
| CUserSetControl | Category that contains the User Set control features |
| CVideoStream | A class to create compressed video stream from images captured or loaded using the Impact Acquire API |
| CVideoStreamPauseScope | A smaller helper class for pausing a video stream for a defined time |
| CWhiteBalancer | Convenience class to provide an easy way for a more precise white balance calibration |
| CWhiteBalanceSettings | Properties for adjusting the colors during a Bayer conversion |