Troubleshooting¶
Hardware issues¶
LED does not illuminate
The 3D stereo camera does not start up.
- Ensure that cables are connected and secured properly.
- Ensure that adequate DC voltage (24 V) with correct polarity is applied to the power connector at the pins labeled as Power and Ground as described in the device’s pin assignment specification. Connecting the camera to voltage outside of the specified range, to alternating current, with reversed polarity, or to a supply with voltage spikes will lead to permanent hardware damage.
Reliability issues and/or mechanical damage
This may be an indication of ambient conditions (vibration, shock, resonance, and temperature) being outside of specified range. Please refer to the specification of environmental conditions.
- Operating the 3D stereo camera outside of specified ambient conditions might lead to damage and will void the warranty.
Electrical shock when touching the projector
This indicates an electrical fault in camera, cabling, or power supply or adjacent system.
- Immediately turn off power to the system, disconnect cables, and have a qualified electrician check the setup.
- Ensure that the projector housing is properly grounded; check for large ground loops.
Sparse depth images¶
The depth images of the 3D stereo camera, which can be seen by using the SGM®Producer, may have missing values, which are shown in black. Missing values near object borders are normal. If major parts of the depth image are invalid, then this may be due to the following reasons:
- The scene may be out of the current working range of the 3D stereo camera. Depending on the depth quality, reducing the parameter Maximum Distance also reduces the possible minimum distance. See also Table 2 for examples of possible depth ranges.
- Depth values may be missing on objects without texture. In this case, the internal random dot projector should be used for projecting an artificial texture. For single shot depth images, the Single+Out1 mode should be selected as DepthAcquisitionMode in the category DepthControl. For continuously computing depth images, the projector should be turned on for every second image by setting Out1 to ExposureAlternateActive in the category DigitalIOControl.
- The focus may be inadequate for the working range. Please check the focus using a calibration grid as described in Adjust focus.
- The calibration of the 3D stereo camera may be inaccurate. Please check the calibration as described in Calibration.