Applicable standards¶
Approvals¶
The 3D stereo camera has received the following approvals:

- EC Declaration of Conformity

- UK Conformity Assessed

- IP54 ingress protection according IEC standard 60529

- ROHS compliant according to EU directive 2011/65/EU

- WEEE compliant according to EU directive 2012/19/EC
Electronical and safety standards¶
The 3D stereo camera has been designed to be in compliance with 2014/30/EU and 2011/65/EU. The 3D stereo camera consists of the projector and two industrial vision cameras.
The projector has been tested based on the following harmonized standards:
- EN 61000-6-4:2007 + A1:2011 : Interference Emission
- EN 61000-6-2:2005 : Interference Immunity
- EN 62471:2008 / IEC 62471:2008 : Photobiological safety of lamps and lamp systems
The industrial cameras have been tested based on the following harmonized standards:
- EN 61000-6-4:2007 + A1:2011 : Interference Emission
- EN 61000-6-2:2005 : Interference Immunity
The 3D stereo camera is intended for use in the US only in industrial plants and is, therefore, exempt from specific technical standards and other requirements of CFR Title 47, Part 15:
47 CFR § 15.103 - Exempted devices
The following devices are subject only to the general conditions of operation in §§ 15.5 and 15.29 and are exempt from the specific technical standards and other requirements contained in this part. The operator of the exempted device shall be required to stop operating the device upon a finding by the Commission or its representative that the device is causing harmful interference. Operation shall not resume until the condition causing the harmful interference has been corrected. Although not mandatory, it is strongly recommended that the manufacturer of an exempted device endeavor to have the device meet the specific technical standards in this part. (b) A digital device used exclusively as an electronic control or power system utilized by a public utility or in an industrial plant. The term public utility includes equipment only to the extent that it is in a dedicated building or large room owned or leased by the utility and does not extend to equipment installed in a subscriber’s facility.
The 3D stereo camera is intended for use in Canada only in industrial plants/factories and, therefore, does not fall under the scope of ICES-003:
1.5.1 General exemptions
ICES-003 does not apply to the following types of equipment:
c. ITE or digital apparatus used exclusively as an electronic control or power system either by a public utility, in a dedicated building/facility owned or leased by the utility and which is not the subscriber facility, or in an industrial plant/factory.
Environmental regulation¶
EU RoHS Directive¶
All components of the 3D stereo camera, including the projector, the industrial cameras, cabling, and structure comply with the provisions in EU RoHS 2 Directive 2011/65/EU on the restriction of the use of certain hazardous substances in electrical and electronic equipment. Items that are exempted in the RoHS Directive are excluded from these standards.
REACH Regulation¶
All components of the 3D stereo camera, including the projector, the industrial cameras, cabling, and structure comply with REACH Regulation 1907/2006/CE. These products are not classified as hazardous. We hereby certify that these products do not contain any Substance of Very High Concern (SVHC) in amounts >0.1% (w/w).
Available certificates¶
Copies of the various certificates can be downloaded from the corresponding product page on https://www.balluff.com.