Safety¶
Warning
The operator must have read and understood all of the instructions in this manual before handling the 3D stereo camera product.
Note
The term “operator” refers to anyone responsible for any of the following tasks performed in conjunction with the 3D stereo camera:
- Installation
- Maintenance
- Inspection
- Calibration
- Programming
- Decommissioning
This manual explains the 3D stereo camera’s various components and general operations regarding the product’s whole life-cycle, from installation through operation to decommissioning.
The drawings and photos in this documentation are representative examples; differences may exist between them and the delivered product.
General warnings¶
Note
Any use of the 3D stereo camera in noncompliance with these warnings is inappropriate and may cause injury or damage as well as void the warranty.
Warning
- The 3D stereo camera is protected according to IP54. High humidity or temperature can damage the device. Do not operate in an environment where combustible or explosive fumes may occur.
- The 3D stereo camera needs to be properly mounted before use.
- All cable sets need to be secured to the 3D stereo camera and the mount.
- Cables must not be longer than 30 m. The 8-Pin power supply cable must not be longer than 15 m.
- Power to the 3D stereo camera must be supplied through an appropriate, separate DC power source.
- An appropriate power supply, which conforms to the EN 62368-1 standard must be used to supply power to the 3D stereo camera.
- Check polarity and connections.
- The 3D stereo camera’s housing must be grounded.
Warning
- The 3D stereo camera’s and any related equipment’s safety guidelines must always be satisfied.
- The 3D stereo camera does not fall under the purview of the machinery or medical directives.
Risk assessment and final application: The 3D stereo camera may be used with a robot. Robot, 3D stereo camera, and any other equipment used in the final application must be evaluated with a risk assessment. The system integrator’s duty is to ensure respect for all local safety measures and regulations. Depending on the application, there may be risks that need additional protection/safety measures.
Intended use¶
The 3D stereo camera is intended to be used in combination with the SGM®Producer. The 3D stereo camera is intended for installation with automated machinery, a mobile platform, or stationary equipment. It can also be used for data acquisition in other applications.
Warning
The 3D stereo camera is NOT intended for safety critical applications.
Warning
The 3D stereo camera is NOT to be used in dynamic environments or mounted to a robot end-effector.
The 3D stereo camera may be used only within the scope of its technical specification. Any other use of the product is deemed unintended use. Balluff will not be liable for any damages resulting from any improper or unintended use.
Warning
Always comply with local and/or national laws, regulations and directives on automation safety and general machine safety.