GripperDB¶
Introduction¶
The GripperDB module (gripper database module) is an optional on-board module of the rc_visard and is licensed with any of the modules ItemPick and BoxPick or SilhouetteMatch. Otherwise it requires a separate CollisionCheck license to be purchased.
The module provides services to set, retrieve and delete grippers which can then be used for checking collisions with a load carrier or other detected objects (only in combination with SilhouetteMatch). The specified grippers are available for all modules supporting collision checking on the rc_visard.
| Max. number of grippers | 50 |
| Supported gripper element geometries | Box, Cylinder, CAD Element |
| Max. number of elements per gripper | 15 |
| Collision checking available in | ItemPick and BoxPick, SilhouetteMatch |
Setting a gripper¶
The gripper is a collision geometry used to determine whether the grasp is in collision with the load carrier. The gripper consists of up to 15 elements connected to each other.
At this point, the gripper can be built of elements of the following types:
BOX, with dimensionsbox.x,box.y,box.z.CYLINDER, with radiuscylinder.radiusand heightcylinder.height.CAD, with the idcad.idof the chosen CAD element.
Additionally, for each gripper the flange radius, and information about the Tool Center Point (TCP) have to be defined.
The configuration of the gripper is normally performed offline during the setup of the desired application. This can be done via the REST-API interface or the rc_visard Web GUI.
Robot flange radius¶
Collisions are checked only with the gripper, the robot body is not considered.
As a safety feature, to prevent collisions between the load carrier and the robot, all grasps having any part of the
robot’s flange inside the load carrier can be designated as colliding (see Fig. 62).
This check is based on the defined gripper geometry and the flange radius value. It is optional to use
this functionality, and it can be turned on and off with the CollisionCheck module’s run-time parameter check_flange as described
in Parameter overview.
Uploading gripper CAD elements¶
A gripper can consist of boxes, cylinders and CAD elements. While boxes and cylinders can be parameterized when the gripper is created, the CAD elements must be uploaded beforehand to be available during gripper creation. A CAD element can be uploaded via the REST-API interface as described in Section CAD element API or via the rc_visard Web GUI. Supported file formats are STEP (*.stp, *.step), STL (*.stl), OBJ (*.obj) and PLY (*.ply). The maximum file size to be uploaded is limited to 10 MB. The files are internally converted to PLY and, if necessary, simplified. The CAD elements can be referenced during gripper creation by their ID.
Creating a gripper via the REST-API or the Web GUI¶
When creating a gripper via the REST-API interface or the Web GUI, each element of the gripper has a parent element, which defines how they are connected. The gripper is always built in the direction from the robot flange to the TCP, and at least one element must have ‘flange’ as parent. The elements’ IDs must be unique and must not be ‘tcp’ or ‘flange’. The pose of the child element has to be given in the coordinate frame of the parent element. The coordinate frame of an element is always in its geometric center. Accordingly, for a child element to be exactly below the parent element, the position of the child element must be computed from the heights of both parent and child element (see Fig. 63).
In case a CAD element is used, the element’s origin is defined in the CAD data and is not necessarily located in the center of the element’s bounding box.
It is recommended to create a gripper via the Web GUI, because it provides a 3D visualization of the gripper geometry and also allows to automatically attach the child element to the bottom of its parent element, when the corresponding option for this element is activated. In this case, the elements also stay attached when any of their sizes change. Automatic attachment of CAD elements uses the element’s bounding box as reference. Automatic attachment is only possible when the child element is not rotated around the x or y axis with respect to its parent.
The reference frame for the first element for the gripper creation is always the center of the robot’s flange with the z axis pointing outwards. It is possible to create a gripper with a tree structure, corresponding to multiple elements having the same parent element, as long as they are all connected.
Calculated TCP position¶
After gripper creation via the set_gripper service call, the TCP position in the flange coordinate
system is calculated and returned as tcp_pose_flange.
It is important to check if this value is the same as the robot’s true TCP position. When creating a
gripper in the Web GUI the current TCP position is always displayed in the 3D gripper visualization.
Creating rotationally asymmetric grippers¶
For grippers which are not rotationally symmetric around the z axis, it is crucial to ensure that the gripper is properly mounted, so that the representation stored in the GripperDB module corresponds to reality.
Services¶
The GripperDB module is called rc_gripper_db in the REST-API and is represented in the
Web GUI under
.
The user can explore and call the GripperDB module’s services,
e.g. for development and testing, using the
REST-API interface or
the Web GUI.
The GripperDB module offers the following services.
set_gripper¶
Persistently stores a gripper on the rc_visard. All configured grippers are persistent over firmware updates and rollbacks.
Details
get_grippers¶
Returns the configured grippers with the requested
gripper_ids.Details
delete_grippers¶
Deletes the configured grippers with the requested
gripper_ids.Details
Return codes¶
Each service response contains a return_code,
which consists of a value plus an optional message.
A successful service returns with a return_code value of 0.
Negative return_code values indicate that the service failed.
Positive return_code values indicate that the service succeeded with additional information.
The smaller value is selected in case a service has multiple return_code values,
but all messages are appended in the return_code message.
The following table contains a list of common codes:
| Code | Description |
|---|---|
| 0 | Success |
| -1 | An invalid argument was provided |
| -7 | Data could not be read or written to persistent storage |
| -9 | No valid license for the module |
| -10 | New gripper could not be added as the maximum storage capacity of grippers has been exceeded |
| 10 | The maximum storage capacity of grippers has been reached |
| 11 | Existing gripper was overwritten |
CAD element API¶
For gripper CAD element upload, download, listing and removal, special REST-API endpoints are provided. CAD elements can also be uploaded, downloaded and removed via the Web GUI. Up to 50 CAD elements can be stored persistently on the rc_visard.
The maximum file size to be uploaded is limited to 10 MB.
-
GET/cad/gripper_elements¶ Get list of all CAD gripper elements.
Template request
GET /api/v2/cad/gripper_elements HTTP/1.1
Template response
HTTP/1.1 200 OK Content-Type: application/json [ { "id": "string" } ]
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation (returns array of GripperElement)
- 404 Not Found – element not found
Referenced Data Models:
-
GET/cad/gripper_elements/{id}¶ Get a CAD gripper element. If the requested content-type is application/octet-stream, the gripper element is returned as file.
Template request
GET /api/v2/cad/gripper_elements/<id> HTTP/1.1
Template response
HTTP/1.1 200 OK Content-Type: application/json { "id": "string" }
Parameters: - id (string) – id of the element (required)
Response Headers: - Content-Type – application/json application/ubjson application/octet-stream
Status Codes: - 200 OK – successful operation (returns GripperElement)
- 404 Not Found – element not found
Referenced Data Models:
-
PUT/cad/gripper_elements/{id}¶ Create or update a CAD gripper element.
Template request
PUT /api/v2/cad/gripper_elements/<id> HTTP/1.1 Accept: multipart/form-data application/json
Template response
HTTP/1.1 200 OK Content-Type: application/json { "id": "string" }
Parameters: - id (string) – id of the element (required)
Form Parameters: - file – CAD file (required)
Request Headers: - Accept – multipart/form-data application/json
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation (returns GripperElement)
- 400 Bad Request – CAD is not valid or max number of elements reached
- 404 Not Found – element not found
- 413 Request Entity Too Large – File too large
Referenced Data Models:
-
DELETE/cad/gripper_elements/{id}¶ Remove a CAD gripper element.
Template request
DELETE /api/v2/cad/gripper_elements/<id> HTTP/1.1 Accept: application/json application/ubjson
Parameters: - id (string) – id of the element (required)
Request Headers: - Accept – application/json application/ubjson
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation
- 404 Not Found – element not found