CADMatch¶
Introduction¶
The CADMatch module is an optional module of the rc_visard and requires a separate CADMatch license to be purchased.
This module provides an out-of-the-box perception solution for 3D object detection and grasping. CADMatch targets the detection of 3D objects based on a CAD template for picking with a general gripper. The objects can be located in a bin or placed arbitrarily in the field of view of the camera.
For the CADMatch module to work, special object templates are required for each type of object to be detected. Please get in touch with the Roboception support (Contact) to order a template for your CAD file.
The CADMatch module offers:
- A dedicated page on the rc_visard Web GUI for easy setup, configuration, testing, and application tuning.
- A REST-API interface and a KUKA Ethernet KRL Interface.
- The definition of regions of interest to select relevant volumes in the scene (see RoiDB).
- A load carrier detection functionality for bin-picking applications (see LoadCarrier), to provide grasps for objects inside a bin only.
- The definition of compartments inside a load carrier to provide grasps for specific volumes of the bin only.
- Storing of up to 50 templates.
- The definition of up to 100 grasp points for each template via an interactive visualization in the Web GUI.
- Collision checking between the gripper and the load carrier, other detected objects and/or the point cloud.
- Collision checking between the object in the gripper and the load carrier walls during retraction.
- Support for static and robot-mounted cameras and optional integration with the Hand-eye calibration module, to provide grasps in the user-configured external reference frame.
- Selection of a sorting strategy to sort the detected objects and returned grasps.
- 3D visualization of the detection results with grasp points and gripper animations in the Web GUI.
Setting of grasp points¶
The CADMatch module detects 3D objects in a scene based on a CAD template and returns the poses of the object origins. To use CADMatch directly in a robot application, up to 100 grasp points can be defined for each template. A grasp point represents the desired position and orientation of the robot’s TCP (Tool Center Point) to grasp an object.
Please consult Setting of grasp points for further details.
Setting grasp points in the Web GUI¶
The rc_visard Web GUI provides an intuitive and interactive way of defining grasp points for object templates. In a first step, the object template has to be uploaded to the rc_visard. This can be done in the Web GUI in any pipeline under by clicking on + Add a new Template in the Templates, Grasps and Pose Priors section, or in in the CADMatch Templates, Grasps and Pose Priors section. Once the template upload is complete, a dialog with a 3D visualization of the object template is shown for adding or editing grasp points. The same dialog appears when editing an existing template.
More details are given in Setting grasp points in the Web GUI.
Setting grasp points via the REST-API¶
Grasp points can be set via the REST-API interface
using the set_grasp or set_all_grasps services
(see Internal services).
More details are given in Setting grasp points via the REST-API.
Setting of pose priors¶
The CADMatch module to define prior poses of the objects to be detected. A pose prior represents the approximate position and orientation of the object to be detected. The pose can be defined in the camera or the external coordinate frame, if a hand-eye calibration is available.
Each pose prior consists of an id which must be
unique within all pose priors for an object template, the template_id representing the template the pose
prior applies to, the pose and the pose_frame of the prior.
Pose priors can be set via the REST-API interface,
or by using the interactive visualization in the Web GUI. The Web GUI allows to interactively position the object
in the current point cloud. This can be done in the “Pose Priors” tab during editing a template.
The rc_visard can store up to 50 pose priors per template.
Setting the preferred orientation of the TCP¶
The CADMatch module determines the reachability of grasp points based on the preferred orientation of the
TCP. The preferred orientation can be set via the set_preferred_orientation service call or on
the CADMatch page in the Web GUI.
The resulting direction of the TCP’s z axis is used to reject grasps which cannot be reached by the gripper.
Furthermore, the preferred orientation can be used to sort the reachable grasps by setting the corresponding
sorting strategy.
The preferred orientation can be set in the camera coordinate frame or in the external coordinate frame, in case a hand-eye calibration is available. If the preferred orientation is specified in the external coordinate frame and the sensor is robot mounted, the current robot pose has to be given to each object detection call. If no preferred orientation is set, the orientation of the left camera (see Coordinate frames ) will be used as the preferred orientation of the TCP.
Setting the sorting strategies¶
The objects and grasps returned by the detect_object service call are sorted according to a sorting strategy which can be
chosen by the user. The following sorting strategies are available and
can be set in the Web GUI
or using the set_sorting_strategies service call:
gravity: highest matches and grasp points along the gravity direction are returned first,match_score: matches with the highest match score and grasp points on objects with the highest match score are returned first,preferred_orientation: matches and grasp points with minimal rotation difference between their orientation and the preferred orientation of the TCP are returned first,direction: matches and grasp points with the shortest distance along a defined directionvectorin a givenpose_frameare returned first.distance_to_point: matches and grasp points with the shortest or farthest (iffarthest_firstis true) distance from apointin a givenpose_frameare returned first.
If no sorting strategy is set or default sorting is chosen in the Web GUI, sorting is done based on a combination of
match_score and the minimal distance from the camera along the z axis of the preferred orientation of the TCP.
Detection of objects¶
The CADMatch module requires an object template for object detection. This template contains information about the 3D shape of the object and prominent edges that can be visible in the camera images. CADMatch also supports partial object templates, which contain only a specific part of the object that can be detected well, e.g., in case of occlusions.
For triggering the object detection, in general, the following information can be provided to the CADMatch module:
Optionally, further information can be given to the CADMatch module:
- The ID of the load carrier which contains the items to be detected.
- A compartment inside the load carrier where to detect objects (see Load carrier compartments).
- The ID of the 3D region of interest where to search for the load carriers if a load carrier is set. Otherwise, the ID of the 3D region of interest where to search for the objects.
- The current robot pose in case the camera is mounted on the robot and
the chosen coordinate frame for the poses is
external, or the preferred orientation is given in the external frame, or the chosen region of interest is defined in the external frame. - Collision detection information: The ID of the gripper to enable collision checking and optionally a pre-grasp offset to define a pre-grasp position. Details on collision checking are given below in CollisionCheck.
- Data acquisition mode: The user can choose if a new image dataset is acquired for the detection (default), or if the detection should be performed on the previously used image dataset. This saves data acquisition time, e.g. in case several detections with different templates have to be run on the same image.
On the Web GUI the detection can be tested in the Try Out section of the CADMatch module’s page.
The detected objects are returned in a list of matches, sorted according to the selected sorting strategy
(see Setting the sorting strategies).
Each detected object
includes a uuid (Universally Unique Identifier) and the
timestamp of the oldest image that was used to detect it.
The pose of a detected object corresponds to the pose of the origin of the object template used for detection.
Furthermore, the matching score is given to indicate the quality of the detection.
If the chosen template also has grasp points attached
(see Setting of grasp points),
a list of grasps for all objects is returned in addition to the list of detected objects.
The grasps are sorted according to the selected sorting strategy
(see Setting the sorting strategies).
The grasp poses are given in the desired coordinate frame. There are references between the detected objects
and the grasps via their uuids.
For objects with a discrete symmetry (e.g. prismatic objects), all collision-free symmetries of each grasp point which are reachable according to the given preferred TCP orientation are returned, ordered by the given sorting strategy.
For objects with a continuous symmetry (e.g. cylindrical objects), all grasps symmetric to each grasp point on an object are checked for reachability and collisions, and only the best one according to the given sorting strategy is returned.
Interaction with other modules¶
Internally, the CADMatch module depends on, and interacts with other on-board modules as listed below.
Note
All changes and configuration updates to these modules will affect the performance of the CADMatch modules.
Stereo camera and Stereo matching¶
The CADMatch module makes internally use of the following data:
- Rectified images from the Camera module
(
rc_camera); - Disparity, error, and confidence images from the Stereo matching module
(
rc_stereomatching).
The quality parameter of the stereo matching module must be set to Medium
or higher (see Parameters). We recommend Full or High quality for using CADMatch.
All processed images are guaranteed to be captured after the module trigger time.
IO and Projector Control¶
In case the rc_visard is used in conjunction with an external random dot projector and
the IO and Projector Control module (rc_iocontrol),
it is recommended to connect the projector to GPIO Out 1 and set
the stereo-camera module’s acquisition mode to SingleFrameOut1
(see Stereo matching parameters), so that
on each image acquisition trigger an image with and without projector pattern is acquired.
Alternatively, the output mode for the GPIO output in use should be set to ExposureAlternateActive
(see Description of run-time parameters).
In either case,
the Auto Exposure Mode exp_auto_mode should be set to AdaptiveOut1 to optimize the exposure
of both images (see Stereo camera parameters).
Hand-eye calibration¶
In case the camera has been calibrated to a robot, the CADMatch module
can automatically provide poses in the robot coordinate frame.
For the CADMatch node’s Services, the frame of the
output poses can be controlled with the pose_frame argument.
Two different pose_frame values can be chosen:
- Camera frame (
camera). All poses provided by the modules are in the camera frame, and no prior knowledge about the pose of the camera in the environment is required. This means that the configured regions of interest and load carriers move with the camera. It is the user’s responsibility to update the configured poses if the camera frame moves (e.g. with a robot-mounted camera). - External frame (
external). All poses provided by the modules are in the external frame, configured by the user during the hand-eye calibration process. The module relies on the on-board Hand-eye calibration module to retrieve the sensor mounting (static or robot mounted) and the hand-eye transformation. If the mounting is static, no further information is needed. If the sensor is robot-mounted, therobot_poseis required to transform poses to and from theexternalframe.
Note
If no hand-eye calibration is available, all pose_frame values should be set to camera.
All pose_frame values that are not camera or external are rejected.
If the sensor is robot-mounted, the current robot_pose has to be provided depending on the value of pose_frame,
the definition of the preferred TCP orientation and the sorting direction or sorting point:
- If
pose_frameis set toexternal, providing the robot pose is obligatory. - If the preferred TCP orientation is defined in
external, providing the robot pose is obligatory. - If the sorting direction is defined in
external, providing the robot pose is obligatory. - If the distance-to-point sorting strategy is defined in
external, providing the robot pose is obligatory. - In all other cases, providing the robot pose is optional.
LoadCarrier¶
The CADMatch module uses the load carrier detection functionality provided by the
LoadCarrier module (rc_load_carrier),
with the run-time parameters specified for this module. However, only one load carrier will be
returned and used in case multiple matching load carriers could be found in the scene. In case multiple
load carriers of the same type are visible, a region of interest should be set to ensure that always the
same load carrier is used for the CADMatch module.
CollisionCheck¶
Collision checking can be easily enabled for
grasp computation of the CADMatch module by passing a collision_detection argument to the
detect_object service call. It contains the ID of the used gripper and
optionally a pre-grasp offset. The gripper has to be
defined in the GripperDB module
(see Setting a gripper)
and details about collision checking are given in
Collision checking within other modules.
Alternatively, grasp points can be assigned individual gripper IDs, and collision checking can be enabled for all
grasp points with gripper IDs by enabling the run-time parameter check_collisions.
If the selected CADMatch template contains a collision geometry and the run-time parameter check_collisions_with_matches is true,
also collisions between the gripper and all other detected objects (not limited to max_matches) will be checked. The object
on which the grasp point to be checked is located, is excluded from the collision check.
If the run-time parameter check_collisions_with_point_cloud is true,
also collisions between the gripper and a watertight version of the point cloud are checked.
If this feature is used with suctions grippers, it should be ensured that the TCP is defined
to be outside the gripper geometry, or that the grasp points are defined above the object surface.
Otherwise every grasp will result in a collision between the gripper and the point cloud.
If the run-time parameter check_collisions_during_retraction is true and a load carrier and a pre-grasp offset are given,
each grasp point will be checked for collisions between the object in the gripper and the load carrier walls during retraction.
This collision check is performed along the full linear trajectory from the grasp point back to the pre-grasp position.
If collision checking is enabled, only grasps which are collision free or could not be checked for collisions (e.g. because no gripper was given) will be returned. The result image on top of the CADMatch page of the Web GUI also shows collision-free grasps in green, unchecked grasps in yellow and colliding grasp points in red. The detected objects which are considered in the collision check are also visualized with their edges in red.
The CollisionCheck module’s run-time parameters affect the collision detection as described in CollisionCheck Parameters.
Parameters¶
The CADMatch module is called rc_cadmatch
in the REST-API and is represented in the
Web GUI
under
.
The user can explore and configure the rc_cadmatch
module’s run-time parameters, e.g. for development and testing, using the Web GUI or the
REST-API interface.
Parameter overview¶
This module offers the following run-time parameters:
| Name | Type | Min | Max | Default | Description |
|---|---|---|---|---|---|
check_collisions |
bool | false | true | false | Whether to check for collisions when a gripper is defined for a grasp |
check_collisions_-during_retraction |
bool | false | true | false | Whether to check for collisions between the object in the gripper and the load carrier during retraction |
check_collisions_with_matches |
bool | false | true | true | Whether to check for collisions between gripper and detected matches |
check_collisions_-with_point_cloud |
bool | false | true | false | Whether to check for collisions between gripper and point cloud |
edge_max_distance |
float64 | 0.5 | 5.0 | 2.0 | Maximum allowed distance in pixels between the template edges and the detected edges in the image |
edge_sensitivity |
float64 | 0.05 | 1.0 | 0.5 | Sensitivity of the edge detector |
grasp_filter_-orientation_threshold |
float64 | 0.0 | 180.0 | 45.0 | Maximum allowed orientation change between grasp and preferred orientation in degrees |
max_matches |
int32 | 1 | 30 | 10 | Maximum number of matches |
min_score |
float64 | 0.05 | 1.0 | 0.3 | Minimum score for matches |
only_highest_priority_grasps |
bool | false | true | false | Whether to return only the highest priority level grasps |
Description of run-time parameters¶
Each run-time parameter is represented by a row on the Web GUI’s CADMatch page. The name in the Web GUI is given in brackets behind the parameter name and the parameters are listed in the order they appear in the Web GUI:
max_matches (Maximum Matches)¶
is the maximum number of objects to detect.
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?max_matches=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?max_matches=<value>
min_score (Minimum Score)¶
is the minimum detection score after refinement. The higher this value, the better 2D edges and 3D point cloud must match the given template.
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?min_score=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?min_score=<value>
edge_sensitivity (Edge Sensitivity)¶
is the sensitivity of the edge detector. The higher the value of this parameter, the more edges will be used for pose refinement.
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?edge_sensitivity=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?edge_sensitivity=<value>
edge_max_distance (Maximum Edge Distance)¶
is the maximum allowed distance in pixels between the template edges and the detected edges in the image during the refinement step.
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?edge_max_distance=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?edge_max_distance=<value>
grasp_filter_orientation_threshold (Grasp Orientation Threshold)¶
is the maximum deviation of the TCP’s z axis at the grasp point from the z axis of the TCP’s preferred orientation in degrees. Only grasp points which are within this threshold are returned. When set to zero, any deviations are valid.
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?grasp_filter_orientation_threshold=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?grasp_filter_orientation_threshold=<value>
only_highest_priority_grasps (Only Highest Priority Grasps)¶
If set to true, only grasps with the highest priority will be returned. If collision checking is enabled, only the collision-free grasps among the group of grasps with the highest priority are returned. This can save computation time and reduce the number of grasps to be parsed on the application side.
Without collision checking, only grasps of highest priority are returned.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?only_highest_priority_grasps=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?only_highest_priority_grasps=<value>
check_collisions (Check Collisions)¶
If this parameter is enabled, collision checking will be performed for all grasps which have a gripper ID assigned, even when no default gripper is given in the
detect_objectservice call. If a load carrier is used, the collision check will always be performed between the gripper and the load carrier. Collision checking with the point cloud and other matches is only performed when the corresponding runtime parameters are enabled.Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?check_collisions=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?check_collisions=<value>
check_collisions_with_matches (Check Collisions with Matches)¶
This parameter is only used when collision checking is enabled by passing a gripper to the
detect_objectservice call or by enabling thecheck_collisionsruntime parameter. Ifcheck_collisions_with_matchesis set to true, all grasp points will be checked for collisions between the gripper and all other detected objects (not limited tomax_matches), and only grasp points at which the gripper would not collide with any other detected object will be returned.Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?check_collisions_with_matches=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?check_collisions_with_matches=<value>
check_collisions_with_point_cloud (Check Collisions with Point Cloud)¶
This parameter is only used when collision checking is enabled by passing a gripper to the
detect_objectservice call or by enabling thecheck_collisionsruntime parameter. Ifcheck_collisions_with_point_cloudis set to true, all grasp points will be checked for collisions between the gripper a watertight version of the point cloud, and only grasp points at which the gripper would not collide with this point cloud will be returned.Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?check_collisions_with_point_cloud=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?check_collisions_with_point_cloud=<value>
check_collisions_during_retraction (Check Collisions during Retraction)¶
This parameter is only used when collision checking is enabled by passing a gripper to the
detect_objectservice call or by enabling thecheck_collisionsruntime parameter. Whencheck_collisions_during_retractionis enabled and a load carrier and a pre-grasp offset are given, each grasp point will be checked for collisions between the object in the gripper and the load carrier walls during retraction. This collision checking is performed along the full linear trajectory from the grasp point back to the pre-grasp position. Only collision-free grasp points will be returned.Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_cadmatch/parameters?check_collisions_during_retraction=<value>PUT http://<host>/api/v1/nodes/rc_cadmatch/parameters?check_collisions_during_retraction=<value>
Status values¶
The rc_cadmatch module reports the following status values:
| Name | Description |
|---|---|
data_acquisition_time |
Time in seconds required by the last active service to acquire images |
last_timestamp_processed |
The timestamp of the last processed dataset |
last_request_timestamp |
The timestamp of the last detection request |
load_carrier_detection_time |
Processing time of the last load carrier detection in seconds |
object_detection_time |
Processing time of the last last object detection in seconds |
processing_time |
Processing time of the last detection (including load carrier detection) in seconds |
state |
The current state of the rc_cadmatch node |
The reported state can take one of the following values.
| State name | Description |
|---|---|
| IDLE | The module is idle. |
| RUNNING | The module is running and ready for load carrier detection and object detection. |
| FATAL | A fatal error has occurred. |
Services¶
The user can explore and call the rc_cadmatch module’s services,
e.g. for development and testing, using the
REST-API interface or
the rc_visard
Web GUI.
The CADMatch modules offer the following services.
detect_object¶
Triggers the detection of objects as described in Detection of objects based on an object template.
Details
set_preferred_orientation¶
Persistently stores the preferred orientation of the TCP to compute the reachability of the grasps, which is used for filtering and, optionally, sorting the grasps returned by the
detect_objectservice (see Setting the preferred orientation of the TCP).Details
get_preferred_orientation¶
Returns the preferred orientation of the TCP to compute the reachability of the grasps, which is used for filtering and, optionally, sorting the grasps returned by the
detect_objectservice (see Setting the preferred orientation of the TCP).Details
set_sorting_strategies¶
Persistently stores the sorting strategy for sorting the grasps and matches returned by the
detect_objectservice (see Detection of objects).Details
get_sorting_strategies¶
Returns the sorting strategy for sorting the grasps and matches returned by the
detect_objectservice (see Detection of objects).Details
start¶
Starts the module. If the command is accepted, the module moves to state
RUNNING.Details
stop¶
Stops the module. If the command is accepted, the module moves to state
IDLE.Details
reset_defaults¶
Resets all parameters of the module to its default values, as listed in above table. Also resets preferred orientation and sorting strategies. The reset does not apply to templates.
Details
Internal services¶
The following services for configuring grasps and pose priors can change in future without notice. Setting, retrieving and deleting grasps and pose priors is recommended to be done via the Web GUI.
set_grasp¶
Persistently stores a grasp for the given object template on the rc_visard. All configured grasps are persistent over firmware updates and rollbacks.
Details
set_all_grasps¶
Replaces the list of grasps for the given object template on the rc_visard.
Details
get_grasps¶
Returns all configured grasps which have the requested
grasp_idsand belong to the requestedtemplate_ids.Details
delete_grasps¶
Deletes all grasps with the requested
grasp_idsthat belong to the requestedtemplate_ids.Details
get_symmetric_grasps¶
Returns all grasps that are symmetric to the given grasp.
Details
set_pose_prior¶
Persistently stores a pose prior for the given object template on the rc_visard. All configured pose priors are persistent over firmware updates and rollbacks.
Details
set_all_pose_priors¶
Replaces the list of pose priors for the given object template on the rc_visard.
Details
get_pose_priors¶
Returns all configured pose priors which have the requested
pose_prior_idsand belong to the requestedtemplate_ids.Details
delete_pose_priors¶
Deletes all pose priors with the requested
pose_prior_idsthat belong to the requestedtemplate_ids.Details
Return codes¶
Each service response contains a return_code,
which consists of a value plus an optional message.
A successful service returns with a return_code value of 0.
Negative return_code values indicate that the service failed.
Positive return_code values indicate that the service succeeded with additional information.
The smaller value is selected in case a service has multiple return_code values,
but all messages are appended in the return_code message.
The following table contains a list of common codes:
| Code | Description |
|---|---|
| 0 | Success |
| -1 | An invalid argument was provided. |
| -2 | An internal error occurred. |
| -3 | An internal timeout occurred. |
| -4 | Data acquisition took longer than allowed. |
| -8 | Not applicable, stereo quality must be at least Medium. |
| -9 | No valid license for the module. |
| -10 | New element could not be added as the maximum storage capacity of load carriers or regions of interest has been exceeded. |
| -11 | Sensor not connected, not supported or not ready. |
| 10 | The maximum storage capacity of load carriers or regions of interest has been reached. |
| 11 | Existing data was overwritten. |
| 100 | The requested load carrier was not detected in the scene. |
| 101 | None of the detected grasps is reachable. |
| 102 | The detected load carrier is empty. |
| 103 | All detected grasps are in collision. |
| 106 | The list of returned grasps has been trimmed to the 100 best grasps. |
| 110 | Hints for setting up the application, e.g. reducing the distance from the camera, setting a region of interest. |
| 113 | No gripper was found for collision checking. |
| 114 | Collision checking during retraction was skipped, e.g. because no load carrier or no pre-grasp offset were given. |
| 151 | The object template has a continuous symmetry. |
| 152 | The objects are outside the given region of interest, outside the load carrier or outside the image. |
| 153 | No edges could be detected in the camera image. Check the Edge Sensitivity. |
| 999 | Additional hints for application development |
Template API¶
For template upload, download, listing and removal, special REST-API endpoints are provided. Templates can also be uploaded, downloaded and removed via the Web GUI. The templates include the grasp points and pose priors, if grasp points or pose priors have been configured. Up to 50 templates can be stored persistently on the rc_visard.