Appendix¶
Pose formats¶
A pose consists of a translation and rotation. The translation defines the
shift along the ,
and
axes.
The rotation can be defined in many different ways. The
rc_visard uses quaternions to define rotations and translations are given in meters.
This is called the
XYZ+quaternion format. This chapter explains the conversion between different
common conventions and the XYZ+quaternion format.
It is quite common to define rotations in 3D by three angles that define rotations around the three coordinate axes. Unfortunately, there are many different ways to do that. The most common conventions are Euler and Cardan angles (also called Tait-Bryan angles). In both conventions, the rotations can be applied to the previously rotated axis (intrinsic rotation) or to the axis of a fixed coordinate system (extrinsic rotation).
We use ,
and
to denote the three coordinate axes.
,
and
refer to the axes that have been rotated
one time. Similarly,
,
and
are the axes
after two rotations.
In the (original) Euler angle convention, the first and the third axis are
always the same. The rotation order -
-
means
rotating around the
-axis, then around the already rotated
-axis and finally around the (two times) rotated
-axis. In
the Cardan angle convention, three different rotation axes are used, e.g.
-
-
. Cardan angles are often also just called
Euler angles.
For each intrinsic rotation order, there is an equivalent extrinsic rotation
order, which is inverted, e.g. the intrinsic rotation order
-
-
is equivalent to the extrinsic rotation order
-
-
.
Rotations around the ,
and
axes can be defined
by quaternions as
or by rotation matrices as
The extrinsic rotation order -
-
can be computed by
multiplying the individual rotations in inverse order, i.e.
.
Based on these definitions, the following sections explain the conversion between common conventions and the XYZ+quaternion format.
Note
Please be aware of units for positions and orientations. rc_visard devices always specify positions in meters, while most robot manufacturers use millimeters or inches. Angles are typically specified in degrees, but may sometimes also be given in radians.