CollisionCheck¶
Introduction¶
The CollisionCheck module is an optional on-board module of the rc_visard and is licensed with any of the modules ItemPick and BoxPick or SilhouetteMatch. Otherwise it requires a separate CollisionCheck license to be purchased.
The module provides an easy way to check if a gripper is in collision with a load carrier, the point cloud (only in combination with SilhouetteMatch), or other detected objects (only in combination with SilhouetteMatch). It is integrated with the ItemPick and BoxPick and SilhouetteMatch modules, but can be used as standalone product. The models of the grippers for collision checking have to be defined in the GripperDB module.
Warning
Collisions are checked only between the load carrier and the gripper, not the robot itself, the flange, other objects or
the item located in the robot gripper. Only in combination with SilhouetteMatch,
and only in case the selected template contains a collision
geometry and check_collisions_with_matches is enabled in the respective detection module,
also collisions between the gripper and other detected objects will be checked.
Collisions with objects that cannot be detected will not be checked.
Only in combination with SilhouetteMatch and
only if check_collisions_with_point_cloud is enabled in the respective detection module,
collisions between the gripper and a watertight version of the point cloud will be checked.
| Collision checking with | detected load carrier, detected objects (only SilhouetteMatch), baseplane (only SilhouetteMatch), point cloud (only SilhouetteMatch) |
| Collision checking available in | ItemPick and BoxPick, SilhouetteMatch |
Collision checking¶
Stand-alone collision checking¶
The check_collisions service call triggers collision checking between the chosen gripper and the provided load carriers
for each of the provided grasps. Checking collisions with other objects or the point cloud
is not possible with the stand-alone check_collisions service.
The CollisionCheck module checks if the chosen gripper is
in collision with at least one of the load carriers, when the TCP of the gripper is positioned in the
grasp position. It is possible to check the collision with multiple load carriers simultaneously. The grasps
which are in collision with any of the defined load carriers will be returned as colliding.
The pre_grasp_offset can be used for additional collision checking.
The pre-grasp offset is the offset between the grasp point
and the pre-grasp position
in the grasp’s coordinate frame (see Fig. 47).
If the pre-grasp offset is defined, the grasp will be detected as colliding
if the gripper is in collision at any point
during motion from the pre-grasp position to the grasp position (assuming
a linear movement).
Collision checking within other modules¶
Collision checking is integrated in the following modules’ services:
- ItemPick:
compute_grasps(see compute_grasps) - BoxPick:
compute_grasps(see compute_grasps) - SilhouetteMatch:
detect_object(see detect_object)
Each of these services can take a collision_detection argument consisting of the gripper_id of the default gripper
and the pre_grasp_offset as described in the previous section
Stand-alone collision checking.
The default gripper given by the gripper_id argument is only used for grasp points which do not have an individual gripper ID assigned.
When the collision_detection argument is given, these services only return the
grasps at which the gripper is not in collision or which could not be checked for collisions.
When a load carrier ID is provided to these services,
collision checking will always be performed between the gripper and the load carrier.
Additional collision check features can be enabled depending on the module.
Only for SilhouetteMatch, and only in case the selected template contains a collision
geometry and check_collisions_with_matches is enabled in the respective detection module,
grasp points at which the gripper would be in collision with other detected objects are also rejected. The object
on which the grasp point to be checked is located, is excluded from the collision check.
When a gripper is defined for a grasp point in the object template for SilhouetteMatch, then this gripper will be used
for collision checking at that specific grasp point instead of the default gripper defined in the collision_detection argument
of the detect_object service (see Setting of grasp points).
The grasps returned by the detect_object service contain a flag collision_checked, indicating whether the grasp was checked for collisions,
and the field gripper_id. If collision_checked is true, the returned gripper_id contains the ID of the gripper that was used for the collision check.
That is the ID of the gripper defined for that specific grasp, or, if empty, the gripper that was given in the
collision_detection argument of the request. If collision_checked is false, the returned gripper_id
is the gripper ID that was defined for that grasp.
In SilhouetteMatch, collisions between
the gripper and the base plane can be checked, if check_collisions_with_base_plane is enabled in SilhouetteMatch.
Collisions between the gripper and a watertight version of the point cloud can be checked in SilhouetteMatch
if check_collisions_with_point_cloud is enabled in the respective module.
Warning
Collisions are checked only between the load carrier and the gripper, not the robot itself, the flange or other objects.
Only in combination with SilhouetteMatch,
and only in case the selected template contains a collision
geometry and check_collisions_with_matches is enabled in the respective detection module,
also collisions between the gripper and other detected objects are checked.
Collisions with objects that cannot be detected will not be checked.
Only in combination with SilhouetteMatch, and
only if check_collisions_with_point_cloud is enabled, collisions between the gripper and a watertight version of the point cloud are checked.
The collision-check results are affected by run-time parameters, which are listed and explained further below.
Parameters¶
The CollisionCheck module is called rc_collision_check
in the REST-API and is represented in the
Web GUI
under .
The user can explore and configure the rc_collision_check
module’s run-time parameters, e.g. for development and testing, using the Web GUI or the
REST-API interface.
Parameter overview¶
This module offers the following run-time parameters:
| Name | Type | Min | Max | Default | Description |
|---|---|---|---|---|---|
check_bottom |
bool | false | true | true | Whether to enable collision checking with the bottom of the load carrier |
check_flange |
bool | false | true | true | Whether all grasps with the flange inside the load carrier should be marked as colliding |
collision_dist |
float64 | 0.0 | 0.1 | 0.01 | Minimum distance in meters between any element of the gripper and the load carrier or the base plane (only SilhouetteMatch) for a collision-free grasp |
Description of run-time parameters¶
Each run-time parameter is represented by a row in the Web GUI’s Settings section under . The name in the Web GUI is given in brackets behind the parameter name:
collision_dist (Collision Distance)¶
Minimal distance in meters between any part of the gripper and the load carrier and/or the base plane (only SilhouetteMatch) for a grasp to be considered collision free.
Note
The collision distance is not applied when checking collisions between the gripper and the point cloud, or the gripper and other detected objects. It is not applied when checking if the flange is inside the load carrier (
check_flange), either.Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_collision_check/parameters?collision_dist=<value>PUT http://<host>/api/v1/nodes/rc_collision_check/parameters?collision_dist=<value>
check_flange (Check Flange)¶
Performs an additional safety check as described in Robot flange radius. If this parameter is set, all grasps in which any part of the robot’s flange is inside the load carrier are marked as colliding.
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_collision_check/parameters?check_flange=<value>PUT http://<host>/api/v1/nodes/rc_collision_check/parameters?check_flange=<value>
check_bottom (Check Bottom)¶
When this check is enabled the collisions will be checked not only with the side walls of the load carrier but also with its bottom. It might be necessary to disable this check if the TCP is inside the collision geometry (e.g. is defined inside a suction cup).
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_collision_check/parameters?check_bottom=<value>PUT http://<host>/api/v1/nodes/rc_collision_check/parameters?check_bottom=<value>
Status values¶
The rc_collision_check module reports the following status values:
| Name | Description |
|---|---|
last_evaluated_grasps |
Number of evaluated grasps |
last_collision_free_grasps |
Number of collision-free grasps |
collision_check_time |
Collision checking runtime |
Services¶
The user can explore and call the rc_collision_check module’s services,
e.g. for development and testing, using
REST-API interface or
the rc_visard
Web GUI.
The CollisionCheck module offers the following services.
reset_defaults¶
Resets all parameters of the module to its default values, as listed in above table.
Details
This service can be called as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_collision_check/services/reset_defaultsPUT http://<host>/api/v1/nodes/rc_collision_check/services/reset_defaultsThis service has no arguments.The definition for the response with corresponding datatypes is:
{ "name": "reset_defaults", "response": { "return_code": { "message": "string", "value": "int16" } } }
check_collisions (deprecated)¶
Triggers a collision check between a gripper and a load carrier.
Details
This service can be called as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_collision_check/services/check_collisionsPUT http://<host>/api/v1/nodes/rc_collision_check/services/check_collisionsRequired arguments:
grasps: list of grasps that should be checked.
load_carriers: list of load carriers against which the collision should be checked. The fields of the load carrier definition are described in Detection of load carriers. The position frame of the grasps and load carriers has to be the same.
gripper_id: the id of the gripper that is used to check the collisions. The gripper has to be configured beforehand.Optional arguments:
pre_grasp_offset: the offset in meters from the grasp position to the pre-grasp position in the grasp frame. If this argument is set, the collisions will not only be checked in the grasp point, but also on the path from the pre-grasp position to the grasp position (assuming a linear movement).The definition for the request arguments with corresponding datatypes is:
{ "args": { "grasps": [ { "pose": { "orientation": { "w": "float64", "x": "float64", "y": "float64", "z": "float64" }, "position": { "x": "float64", "y": "float64", "z": "float64" } }, "pose_frame": "string", "uuid": "string" } ], "gripper_id": "string", "load_carriers": [ { "id": "string", "inner_dimensions": { "x": "float64", "y": "float64", "z": "float64" }, "outer_dimensions": { "x": "float64", "y": "float64", "z": "float64" }, "pose": { "orientation": { "w": "float64", "x": "float64", "y": "float64", "z": "float64" }, "position": { "x": "float64", "y": "float64", "z": "float64" } }, "pose_frame": "string", "rim_thickness": { "x": "float64", "y": "float64" } } ], "pre_grasp_offset": { "x": "float64", "y": "float64", "z": "float64" } } }
colliding_grasps: list of grasps in collision with one or more load carriers.
collision_free_grasps: list of collision-free grasps.
return_code: holds possible warnings or error codes and messages.The definition for the response with corresponding datatypes is:
{ "name": "check_collisions", "response": { "colliding_grasps": [ { "pose": { "orientation": { "w": "float64", "x": "float64", "y": "float64", "z": "float64" }, "position": { "x": "float64", "y": "float64", "z": "float64" } }, "pose_frame": "string", "uuid": "string" } ], "collision_free_grasps": [ { "pose": { "orientation": { "w": "float64", "x": "float64", "y": "float64", "z": "float64" }, "position": { "x": "float64", "y": "float64", "z": "float64" } }, "pose_frame": "string", "uuid": "string" } ], "return_code": { "message": "string", "value": "int16" } } }
set_gripper (deprecated)¶
Persistently stores a gripper on the rc_visard.
This service is not available in API version 2. Use set_gripper inrc_gripper_dbinstead.This service can be called as follows.
PUT http://<host>/api/v1/nodes/rc_collision_check/services/set_gripperThe definitions of the request and response are the same as described in set_gripper in
rc_gripper_db.
get_grippers (deprecated)¶
Returns the configured grippers with the requested
gripper_ids.This service is not available in API version 2. Use get_grippers inrc_gripper_dbinstead.This service can be called as follows.
PUT http://<host>/api/v1/nodes/rc_collision_check/services/get_grippersThe definitions of the request and response are the same as described in get_grippers in
rc_gripper_db.
delete_grippers (deprecated)¶
Deletes the configured grippers with the requested
gripper_ids.This service is not available in API version 2. Use delete_grippers inrc_gripper_dbinstead.This service can be called as follows.
PUT http://<host>/api/v1/nodes/rc_collision_check/services/delete_grippersThe definitions of the request and response are the same as described in delete_grippers in
rc_gripper_db.
Return codes¶
Each service response contains a return_code,
which consists of a value plus an optional message.
A successful service returns with a return_code value of 0.
Negative return_code values indicate that the service failed.
Positive return_code values indicate that the service succeeded with additional information.
The smaller value is selected in case a service has multiple return_code values,
but all messages are appended in the return_code message.
The following table contains a list of common codes:
| Code | Description |
|---|---|
| 0 | Success |
| -1 | An invalid argument was provided |
| -7 | Data could not be read or written to persistent storage |
| -9 | No valid license for the module |
| -10 | New gripper could not be added as the maximum storage capacity of grippers has been exceeded |
| 10 | The maximum storage capacity of grippers has been reached |
| 11 | Existing gripper was overwritten |