KUKA Ethernet KRL Interface¶
The rc_visard provides an Ethernet KRL Interface (EKI Bridge), which allows communicating with the rc_visard from KUKA KRL via KUKA.EthernetKRL XML.
Note
The component is optional and requires a separate Balluff’s EKIBridge license to be purchased.
Note
The KUKA.EthernetKRL add-on software package version 2.2 or newer must be activated on the robot controller to use this component.
The EKI Bridge can be used to programmatically
- do service calls, e.g. to start and stop individual computational nodes, or to use offered services such as the hand-eye calibration or the computation of grasp poses;
- set and get run-time parameters of computation nodes, e.g. of the camera, or disparity calculation.
Note
A known limitation of the EKI Bridge is that strings representing valid numbers will be converted to int/float. Hence user-defined names (like ROI IDs, etc.) should always contain at least one letter so they can be used in service call arguments.
Ethernet connection configuration¶
The EKI Bridge listens on port 7000 for EKI XML messages and transparently bridges the rc_visard’s REST-API v2. The received EKI messages are transformed to JSON and forwarded to the rc_visard’s REST-API. The response from the REST-API is transformed back to EKI XML.
The EKI Bridge gives access to run-time parameters and offered services of all computational nodes described in Software modules.
The Ethernet connection to the rc_visard on the robot controller is configured using XML configuration files. The EKI XML configuration files of all nodes running on the rc_visard are listed at EKI XML configuration files.
Each node offering run-time parameters has an XML configuration file
for setting and getting its parameters.
These are named following the scheme <node_name>-parameters.xml.
Each node’s service has its own XML configuration file.
These are named following the scheme <node_name>-<service_name>.xml.
The IP of the rc_visard in the network needs to be filled in the XML file.
These files must be stored in the directory
C:\KRC\ROBOTER\Config\User\Common\EthernetKRL
of the robot controller and they are read in when a connection is initialized.
As an example, an Ethernet connection to configure the rc_stereomatching
parameters is established with the following KRL code.
DECL EKI_Status RET RET = EKI_INIT("rc_stereomatching-parameters") RET = EKI_Open("rc_stereomatching-parameters") ; ----------- Desired operation ----------- RET = EKI_Close("rc_stereomatching-parameters")
Note
The EKI Bridge automatically terminates the connection to the client if the received XML telegram is invalid.
Generic XML structure¶
For data transmission, the EKI Bridge uses <req> as root XML element
(short for request).
The root tag always includes the following elements.
<node>. This includes a child XML element used by the EKI Bridge to identify the target node. The node name is already included in the XML configuration file.<end_of_request>. End of request flag that triggers the request.
The following listing shows the generic XML structure for data transmission.
<SEND> <XML> <ELEMENT Tag="req/node/<node_name>" Type="STRING"/> <ELEMENT Tag="req/end_of_request" Type="BOOL"/> </XML> </SEND>
For data reception, the EKI Bridge uses <res> as root XML element
(short for response).
The root tag always includes a <return_code> child element.
<RECEIVE> <XML> <ELEMENT Tag="res/return_code/@value" Type="INT"/> <ELEMENT Tag="res/return_code/@message" Type="STRING"/> <ELEMENT Tag="res" Set_Flag="998"/> </XML> </RECEIVE>
Note
By default the XML configuration files uses 998 as flag to notify KRL that the response data record has been received. If this value is already in use, it should be changed in the corresponding XML configuration file.
Return code¶
The <return_code> element consists of a value and a message attribute.
As for all other components, a successful request returns with a
res/return_code/@value of 0.
Negative values indicate that the request failed.
The error message is contained in res/return_code/@message.
Positive values indicate that the request succeeded with additional information,
contained in res/return_code/@message as well.
The following codes can be issued by the EKI Bridge component.
| Code | Description |
|---|---|
| 0 | Success |
| -1 | Parsing error in the conversion from XML to JSON |
| -2 | Internal error |
| -5 | Connection error from the REST-API |
| -9 | Missing or invalid license for EKI Bridge component |
Note
The EKI Bridge can also return return code values specific to individual nodes. They are documented in the respective software module.
Note
Due to limitations in KRL, the maximum length of a string returned by the EKI Bridge is 512 characters. All messages larger than this value are truncated.
Services¶
For the nodes’ services, the XML schema is generated from the service’s arguments and response in JavaScript Object Notation (JSON) described in Software modules. The conversion is done transparently, except for the conversion rules described below.
Conversions of poses:
A pose is a JSON object that includes
positionandorientationkeys.{ "pose": { "position": { "x": "float64", "y": "float64", "z": "float64", }, "orientation": { "x": "float64", "y": "float64", "z": "float64", "w": "float64", } } }This JSON object is converted to a KRL
FRAMEin the XML message.<pose X="..." Y="..." Z="..." A="..." B="..." C="..."></pose>Positions are converted from meters to millimeters and orientations are converted from quaternions to KUKA ABC (in degrees).
Note
No other unit conversions are included in the EKI Bridge. All dimensions and 3D coordinates that don’t belong to a pose are expected and returned in meters.
Arrays:
Arrays are identified by adding the child element
<le>(short for list element) to the list name. As an example, the JSON object{ "rectangles": [ { "x": "float64", "y": "float64" } ] }is converted to the XML fragment
<rectangles> <le> <x>...</x> <y>...</y> </le> </rectangles>
Use of XML attributes:
All JSON keys whose values are a primitive data type and don’t belong to an array are stored in attributes. As an example, the JSON object
{ "item": { "uuid": "string", "confidence": "float64", "rectangle": { "x": "float64", "y": "float64" } } }is converted to the XML fragment
<item uuid="..." confidence="..."> <rectangle x="..." y="..."> </rectangle> </item>
Request XML structure¶
The <SEND> element in the XML configuration file for a generic
service follows the specification below.
<SEND> <XML> <ELEMENT Tag="req/node/<node_name>" Type="STRING"/> <ELEMENT Tag="req/service/<service_name>" Type="STRING"/> <ELEMENT Tag="req/args/<argX>" Type="<argX_type>"/> <ELEMENT Tag="req/end_of_request" Type="BOOL"/> </XML> </SEND>
The <service> element includes a child XML element that is used by the
EKI Bridge to identify the target service from the XML telegram.
The service name is already included in the configuration file.
The <args> element includes the service arguments and should be configured
with EKI_Set<Type> KRL instructions.
As an example, the <SEND> element of the rc_load_carrier_db’s
get_load_carriers service
(see LoadCarrierDB) is:
<SEND> <XML> <ELEMENT Tag="req/node/rc_load_carrier_db" Type="STRING"/> <ELEMENT Tag="req/service/get_load_carriers" Type="STRING"/> <ELEMENT Tag="req/args/load_carrier_ids/le" Type="STRING"/> <ELEMENT Tag="req/end_of_request" Type="BOOL"/> </XML> </SEND>
The <end_of_request> element allows to have arrays in the request.
For configuring an array, the request is split into as many
packages as the size of the array.
The last telegram contains all tags, including the <end_of_request>
flag, while all other telegrams contain one array element each.
As an example, for requesting two load carrier models to the rc_load_carrier_db’s
get_load_carriers service, the user needs to send two XML messages.
The first XML telegram is:
<req> <args> <load_carrier_ids> <le>load_carrier1</le> </load_carrier_ids> </args> </req>
This telegram can be sent from KRL with the EKI_Send command,
by specifying the list element as path:
DECL EKI_STATUS RET RET = EKI_SetString("rc_load_carrier_db-get_load_carriers", "req/args/load_carrier_ids/le", "load_carrier1") RET = EKI_Send("rc_load_carrier_db-get_load_carriers", "req/args/load_carrier_ids/le")
The second telegram includes all tags and triggers the request to the
rc_load_carrier_db node:
<req> <node> <rc_load_carrier_db></rc_load_carrier_db> </node> <service> <get_load_carriers></get_load_carriers> </service> <args> <load_carrier_ids> <le>load_carrier2</le> </load_carrier_ids> </args> <end_of_request></end_of_request> </req>
This telegram can be sent from KRL by specifying req as path for EKI_Send:
DECL EKI_STATUS RET RET = EKI_SetString("rc_load_carrier_db-get_load_carriers", "req/args/load_carrier_ids/le", "load_carrier2") RET = EKI_Send("rc_load_carrier_db-get_load_carriers", "req")
Response XML structure¶
The <RECEIVE> element in the XML configuration file for a generic
service follows the specification below:
<RECEIVE> <XML> <ELEMENT Tag="res/<resX>" Type="<resX_type>"/> <ELEMENT Tag="res/return_code/@value" Type="INT"/> <ELEMENT Tag="res/return_code/@message" Type="STRING"/> <ELEMENT Tag="res" Set_Flag="998"/> </XML> </RECEIVE>
As an example, the <RECEIVE> element of the rc_april_tag_detect’s
detect service
(see TagDetect) is:
<RECEIVE> <XML> <ELEMENT Tag="res/timestamp/@sec" Type="INT"/> <ELEMENT Tag="res/timestamp/@nsec" Type="INT"/> <ELEMENT Tag="res/return_code/@message" Type="STRING"/> <ELEMENT Tag="res/return_code/@value" Type="INT"/> <ELEMENT Tag="res/tags/le/pose_frame" Type="STRING"/> <ELEMENT Tag="res/tags/le/timestamp/@sec" Type="INT"/> <ELEMENT Tag="res/tags/le/timestamp/@nsec" Type="INT"/> <ELEMENT Tag="res/tags/le/pose/@X" Type="REAL"/> <ELEMENT Tag="res/tags/le/pose/@Y" Type="REAL"/> <ELEMENT Tag="res/tags/le/pose/@Z" Type="REAL"/> <ELEMENT Tag="res/tags/le/pose/@A" Type="REAL"/> <ELEMENT Tag="res/tags/le/pose/@B" Type="REAL"/> <ELEMENT Tag="res/tags/le/pose/@C" Type="REAL"/> <ELEMENT Tag="res/tags/le/instance_id" Type="STRING"/> <ELEMENT Tag="res/tags/le/id" Type="STRING"/> <ELEMENT Tag="res/tags/le/size" Type="REAL"/> <ELEMENT Tag="res" Set_Flag="998"/> </XML> </RECEIVE>
For arrays, the response includes multiple instances of the same XML element.
Each element is written into a separate buffer within EKI and can be read
from the buffer with KRL instructions.
The number of instances can be requested with EKI_CheckBuffer and each
instance can then be read by calling EKI_Get<Type>.
As an example, the tag poses received after a call to the
rc_april_tag_detect’s detect service can be read in KRL using the
following code:
DECL EKI_STATUS RET DECL INT i DECL INT num_instances DECL FRAME poses[32] DECL FRAME pose = {X 0.0, Y 0.0, Z 0.0, A 0.0, B 0.0, C 0.0} RET = EKI_CheckBuffer("rc_april_tag_detect-detect", "res/tags/le/pose") num_instances = RET.Buff for i=1 to num_instances RET = EKI_GetFrame("rc_april_tag_detect-detect", "res/tags/le/pose", pose) poses[i] = pose endfor RET = EKI_ClearBuffer("rc_april_tag_detect-detect", "res")
Note
Before each request from EKI to the rc_visard, all buffers should be cleared in order to store only the current response in the EKI buffers.
Parameters¶
All nodes’ parameters can be set and queried from the EKI Bridge. The XML configuration file for a generic node follows the specification below:
<SEND> <XML> <ELEMENT Tag="req/node/<node_name>" Type="STRING"/> <ELEMENT Tag="req/parameters/<parameter_x>/@value" Type="INT"/> <ELEMENT Tag="req/parameters/<parameter_y>/@value" Type="STRING"/> <ELEMENT Tag="req/end_of_request" Type="BOOL"/> </XML> </SEND> <RECEIVE> <XML> <ELEMENT Tag="res/parameters/<parameter_x>/@value" Type="INT"/> <ELEMENT Tag="res/parameters/<parameter_x>/@default" Type="INT"/> <ELEMENT Tag="res/parameters/<parameter_x>/@min" Type="INT"/> <ELEMENT Tag="res/parameters/<parameter_x>/@max" Type="INT"/> <ELEMENT Tag="res/parameters/<parameter_y>/@value" Type="REAL"/> <ELEMENT Tag="res/parameters/<parameter_y>/@default" Type="REAL"/> <ELEMENT Tag="res/parameters/<parameter_y>/@min" Type="REAL"/> <ELEMENT Tag="res/parameters/<parameter_y>/@max" Type="REAL"/> <ELEMENT Tag="res/return_code/@value" Type="INT"/> <ELEMENT Tag="res/return_code/@message" Type="STRING"/> <ELEMENT Tag="res" Set_Flag="998"/> </XML> </RECEIVE>
The request is interpreted as a get request if all parameter’s
value attributes are empty.
If any value attribute is non-empty, it is interpreted as set request
of the non-empty parameters.
As an example, the current value of all parameters of rc_stereomatching
can be queried using the XML telegram:
<req> <node> <rc_stereomatching></rc_stereomatching> </node> <parameters></parameters> <end_of_request></end_of_request> </req>
This XML telegram can be sent out with Ethernet KRL using:
DECL EKI_STATUS RET RET = EKI_Send("rc_stereomatching-parameters", "req")
The response from the EKI Bridge contains all parameters:
<res> <parameters> <acquisition_mode default="Continuous" max="" min="" value="Continuous"/> <quality default="High" max="" min="" value="High"/> <static_scene default="0" max="1" min="0" value="0"/> <seg default="200" max="4000" min="0" value="200"/> <smooth default="1" max="1" min="0" value="1"/> <fill default="3" max="4" min="0" value="3"/> <minconf default="0.5" max="1.0" min="0.5" value="0.5"/> <mindepth default="0.1" max="100.0" min="0.1" value="0.1"/> <maxdepth default="100.0" max="100.0" min="0.1" value="100.0"/> <maxdeptherr default="100.0" max="100.0" min="0.01" value="100.0"/> </parameters> <return_code message="" value="0"/> </res>
The quality parameter of rc_stereomatching can be set to Low
by the XML telegram:
<req> <node> <rc_stereomatching></rc_stereomatching> </node> <parameters> <quality value="Low"></quality> </parameters> <end_of_request></end_of_request> </req>
This XML telegram can be sent out with Ethernet KRL using:
DECL EKI_STATUS RET RET = EKI_SetString("rc_stereomatching-parameters", "req/parameters/quality/@value", "Low") RET = EKI_Send("rc_stereomatching-parameters", "req")
In this case, only the applied value of quality is returned by the
EKI Bridge:
<res> <parameters> <quality default="High" max="" min="" value="Low"/> </parameters> <return_code message="" value="0"/> </res>
EKI XML configuration files¶
This section contains EKI XML configuration files for all
nodes running on the rc_visard. They are also available
for download in this
ZIP archive.
rc_april_tag_detect
Services:
rc_boxpick
rc_camera
Services:
rc_collision_check
Services:
rc_dynamics
rc_gripper_db
rc_hand_eye_calibration
rc_iocontrol
Services:
rc_itempick
rc_load_carrier
rc_load_carrier_db
rc_measure
Services:
rc_qr_code_detect
Services:
rc_roi_db
rc_silhouettematch
rc_slam
rc_stereocalib
Services:
rc_stereomatching
Services:
rc_stereovisodo
Services:
Migration to firmware version 22.01¶
From firmware version 22.01 on the EKI Bridge reflects rc_visard’s REST-API v2.
This requires the following changes:
- Configuring load carriers, grippers and regions of interest is now only accessible in the global database modules:
- Use the
rc_load_carrier_dbXML files for getting, setting and deleting of load carriers. - Use the
rc_gripper_dbXML files for getting, setting and deleting of grippers. - Use the
rc_roi_dbXML files for getting, setting and deleting of regions of interest.
- Use the
- Load carrier detection and filling level detection is now only accessible via the
rc_load_carriernode.- Use the
rc_load_carrierXML files fordetect_load_carriersanddetect_filling_levelservices.
- Use the
Example applications¶
More detailed robot application examples can be found at https://github.com/roboception/eki_examples.
Troubleshooting¶
SmartPad error message: Limit of element memory reached
This error may occur if the number of matches exceeds the memory limit.
- Increase BUFFERING and set BUFFSIZE in EKI config files. Adapt these settings to your particular KRC.
- Decrease the ‘Maximum Matches’ parameter in the detection module
- Even if the total memory limit (BUFFSIZE) of a message is not reached, the KRC might not be able to parse the number of child elements in the XML tree if the BUFFERING limit is too small. For example, if your application proposes 50 different grasps, the BUFFERING limit needs to be 50 too.