Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
DeviceConfigure

DeviceConfigure is mainly meant to update the firmware of Balluff devices and to configure the log-output of the Impact Acquire software stack. Apart from that this tool can

  • display a list of all devices connected to the system for which a corresponding Impact Acquire support currently is installed
  • register/unregister devices for the usage with DirectShow™ applications (Windows® only)
  • assign unique IDs to mvBlueFOX-1xx/mvBlueFOX-2xx devices
  • reserve system wide DMA memory for mvHYPERION frame grabber devices
Note
GigE Vision™ devices:
  • macOS: The app DeviceConfigure.app in "~/ImpactAcquire/bin" does not use the correct environment, so a double-click on the app will not find any GigE Vision™ devices. To start DeviceConfigure with the correct environment, start the shell script startDeviceConfigure.sh in "~/ImpactAcquire".
  • Windows®: Given that during the start DeviceConfigure searches the network for GigE Vision™ devices, it could be possible that - depending on the Windows® firewall settings - a Windows® security alert appears. Please click on "Unblock" or "Allow Access" depending on the version of Windows® you are working with so that the program works properly.
    Windows® security alert

Various things can also be done without user interaction (e.g. updating the firmware of a device). To find out how to do this please refer to the Command-line Interface section

Pressing F1 will also display a detailed list of the Command-line Interface available as well as keyboard shortcuts and some other useful information!