Balluff - BVS CA-SF Technical Documentation
Loading...
Searching...
No Matches
Sensor Overview

Image data flow

The following block diagrams show the data flow of the image data after being read from the sensor chip in the camera.

Figure 1: Block diagram

Output sequence of color sensors (RGB Bayer)

Figure 2: Output sequence of RAW data

Bilinear interpolation of color sensors (RGB Bayer)

For Bayer demosaicing in the camera, we use bilinear interpolation:

Figure 5: Bilinear interpolation
  1. Interpolation of green pixels: the average of the upper, lower, left and right pixel values is assigned as the G value of the interpolated pixel.
    For example:
              (G3+G7+G9+G13)
    G8     =  --------------
                    4 
    

    For G7:
                                (G1+G3+G11+G13)
    G7_new =  0.5 * G7 + 0.5 *  ---------------
                                       4
    
  2. Interpolation of red/blue pixels:
    Interpolation of a red/blue pixel at a green position: the average of two adjacent pixel values in corresponding color is assigned to the interpolated pixel.
    For example:
             (B6+B8)           (R2+R12)
    B7     = ------- ; R7    = --------
                2                 2
    

    Interpolation of a red/blue pixel at a blue/red position: the average of four adjacent diagonal pixel values is assigned to the interpolated pixel.
    For example:
             (R2+R4+R12+R14)             (B6+B8+B16+B18)
    R8     = --------------- ;  B12    = ---------------
                   4                           4
    

Any colored edge which might appear is due to Bayer false color artifacts.

Note
There are more advanced and adaptive methods (like edge sensitive ones) available if the host is doing this debayering.

CMOS sensors

Details of operation

The CMOS sensors offer two different modes of operation:

  • Free running mode (Overlapping integration and readout)
  • Snapshot mode (Sequential integration and readout)

Free running mode

In free running mode, the sensor reaches its maximum frame rate. This is done by overlapping erase, integration and readout phase. The sensor timing in free running mode is fixed, so there is no control when to start an acquisition. This mode is used with trigger mode Continuous.

Snapshot mode

In snapshot mode, the image acquisition process consists off several sequential phases:

  • Trigger
  • Erase, exposure and readout

Trigger

Snapshot mode starts with a trigger. This can be either a hardware or a software signal.

The CMOS sensors support the following trigger modes:

Description Setting in GenICam™
Free running, no external trigger signal needed (formerly known as Continuous)."TriggerSelector = FrameStart"
"TriggerMode = Off"
Image acquisition triggered by command (software trigger; formerly known as OnDemand)."TriggerSelector = FrameStart"
"TriggerMode = On"
"TriggerSource = Software"
"ExposureMode = Timed"

To trigger one frame execute the TriggerSoftware@i command then.
Start an exposure of a frame as long as the trigger input is below the trigger threshold (formerly known as OnLowLevel)."TriggerSelector = AcquisitionActive"
"TriggerMode = On"
"TriggerSource = <desired Line>"
"TriggerActivation = LevelLow"
"ExposureMode = Timed"
Start an exposure of a frame as long as the trigger input is above the trigger threshold (formerly known as OnHighLevel)."TriggerSelector = AcquisitionActive"
"TriggerMode = On"
"TriggerSource = <desired Line>"
"TriggerActivation = LevelHigh"
"ExposureMode = Timed"

If an external trigger signal occurs (e.g. high or low), the sensor will start to expose and readout one image. Now, if the trigger signal is still available, the sensor will start to expose and readout the next image (see figure 12, upper part). This will lead to an acquisition just like using continuous trigger.

Figure 3: External Trigger with CMOS sensors

If you want to avoid this effect, you have to adjust the trigger signal. As you can see in figure 3 (lower part), the possible period is small.

Example

External synchronized image acquisition (high active)

  • Trigger modes
    • OnHighLevel:
      The high level of the trigger has to be shorter than the frame time. In this case, the sensor will make one image exactly. If the high time is longer, there will be images with the possible frequency of the sensor as long as the high level takes. The first image will start with the low-high edge of the signal. The integration time of the exposure register will be used.
    • OnLowLevel:
      The first image will start with the high-low edge of the signal.

Erase, exposure and readout

All pixels are light sensitive at the same period of time. The whole pixel core is reset simultaneously and after the exposure time all pixel values are sampled together on the storage node inside each pixel. The pixel core is read out line-by-line after integration.

Models

The CMOS sensor modules incorporate the following features:

Sony Pregius S

Sensors 5.1 Mpix (-2051d)8.1 Mpix (-2081a)12.4 Mpix (-2124d)12.4 Mpix (-2124f)16.2 Mpix (-2162)20.4 Mpix (-2204)24.6 Mpix (-2246)
Sensor supplier SonySonySonySonySonySonySony
Sensor name IMX547IMX546IMX545IMX902IMX542IMX541IMX540
Res. 2472 x 2064
gray scale / RGB
2856 x 2848
gray scale / RGB
4128 x 3008
gray scale / RGB
6048 x 2048
gray scale / RGB
5328 x 3040
gray scale / RGB
4512 x 4512
gray scale / RGB
5328 x 4608
gray scale / RGB
Sensor size 1/1.8" 2/3" 1/1.1" 1/1.1" 1.1" 1.1" 1.2"
Max. FPS (in free-running full frame mode) 74.0 46.7 30.6 30.6 23.4 18.7 15.5
FPS exactnessxxxxxxx
ADC resolution / Out 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8
SNRmax [dB]1/40.5 43.8 40.3 39.6 39.8 39.7 39.8
DR (normal / HDR) [dB]1/70.3 70.2 70.1 69.46 70.6 70.7 70.4
Rolling shutterxxxxxxx
Global shutter√√√√√√√
Global Resetxxxxxxx
Trigger (HW / SW)√/√√/√√/√√/√√/√√/√√/√
Pipelined GS√√√√√√√
Linescan modexxxxxxx
High color reproductivity (for color version) √√√√√√√
Power consumption [W] approx. 2.7 approx. 2.7 approx. 2.7 approx. tbd approx. 3.0 approx. 3.2 approx. 4.0
More specific data mvBlueFOX3-2051d / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0051D (5.1 Mpix [2472 x 2064]) mvBlueFOX3-2081a / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0081A (8.1 Mpix [2856 x 2848]) mvBlueFOX3-2124d / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0124D (12.4 Mpix [4128 x 3008]) mvBlueFOX3-2124f / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0124F (12.4 Mpix [6048 x 2048]) mvBlueFOX3-2162 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0162A (16.2 Mpix [5328 x 3040]) mvBlueFOX3-2204 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0204A (20.5 Mpix [4512 x 4512]) mvBlueFOX3-2246 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0246A (24.6 Mpix [5328 x 4608])

Sony Pregius

Sensors 0.4 Mpix (-2004)1.6 Mpix (-2016)1.7 Mpix (-2017)2.4 Mpix (-2024)2.4 Mpix (-2024a)2.4 Mpix (-0024B)3.2 Mpix (-2032)3.2 Mpix (-2032a)5.1 Mpix (-2051)5.1 Mpix (-2051a)7.1 Mpix (-2071)7.1 Mpix (-2071a)8.9 Mpix (-2089)8.9 Mpix (-2089a)12.4 Mpix (-2124)12.4 Mpix (-2124a)16.9 Mpix (-0169Z)19.6 Mpix (-0196Z)31.5 Mpix (-0315Z)
Sensor supplier SonySonySonySonySonySonySonySonySonySonySonySonySonySonySonySonySonySonySony
Sensor name IMX287IMX273IMX425IMX174IMX249IMX392IMX252IMX265IMX250IMX264IMX420IMX428IMX255IMX267IMX253IMX304IMX387IMX367IMX342
Res. 728 x 544
gray scale / RGB
1456 x 1088
gray scale / RGB
1600 x 1104
gray scale / RGB
1936 x 1216
gray scale / RGB
1936 x 1216
gray scale / RGB
1936 x 1216
gray scale / RGB
2064 x 1544
gray scale / RGB
2064 x 1544
gray scale / RGB
2464 x 2056
gray scale / RGB
2464 x 2056
gray scale / RGB
3216 x 2208
gray scale / RGB
3216 x 2208
gray scale / RGB
4112 x 2176
gray scale / RGB
4112 x 2176
gray scale / RGB
4112 x 3008
gray scale / RGB
4112 x 3008
gray scale / RGB
5472 x 3084
gray scale / RGB
4432 x 4432
gray scale / RGB
6480 x 4856
gray scale / RGB
Sensor size 1/2.9" 1/2.9" 1.1" 1/1.2" 1/1.2" 1/2.3" 1/1.8" 1/1.8" 2/3" 2/3" 1.1" 1.1" 1" 1" 1.1" 1.1" 4/3" 4/3" APS-C
Max. FPS (in free-running full frame mode) 436.9 226.5 212.9 164 166 46.9 123 55 80 35 53.5 50.9 47 32 34 23 22.5 19.3 12.1
FPS exactnessxxxxxxxxxxxxxxxxxxx
ADC resolution / Out 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8
SNRmax [dB]1/43.3 40.2 49.9 45.1 45.1 40.2 40.3 40.2 40.3 40.1 43.8 43.9 40.2 40.2 40.2 40.2 40.2 40.1 39.7
DR (normal / HDR) [dB]1/74.2 / 71.4 / 72.4 / 66.4 / 73.0 / 71.4 / 71.1 / 71.3 / 71.2 / 71.3 / 71.7 71.8 71.1 / 71.0 70.9 / 71.0 70.8 70.7 69.8
Rolling shutterxxxxxxxxxxxxxxxxxxx
Global shutter√√√√√√√√√√√√√√√√√√√
Global Resetxxxxxxxxxxxxxxxxxxx
Trigger (HW / SW)√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√√/√
Pipelined GS√√√√√√√√√√√√√√√√√√√
Linescan modexxxxxxxxxxxxxxxxxxx
High color reproductivity (for color version) √√√√√√√√√√√√√√√√√√√
Power consumption [W] approx. 3.2 approx. 3.5 approx. 4.5 approx. 3.4 approx. 2.8 approx. 3.4 approx. 3.6 approx. 3.0 approx. 3.6 approx. 3.0 approx. 4.4 approx. 4.0 approx. 4.0 approx. 4.0 approx. 4.0 approx. 4.0 approx. 4.9 approx. 4.9 approx. 4.9 (BVS CA-SF4) | 5 (BVS CA-SF5)2
More specific data mvBlueFOX3-2004 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0004F (0.4 Mpix [728 x 544]) mvBlueFOX3-2016 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0016Z (1.6 Mpix [1456 x 1088]) mvBlueFOX3-2017 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0017Z (1.8 Mpix [1600 x 1104]) mvBlueFOX3-2024 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0024ZG (2.4 Mpix [1936 x 1216]) mvBlueFOX3-2024a / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0024A (2.4 Mpix [1936 x 1216]) mvBlueFOX3-2024b / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0024B (2.4 Mpix [1936 x 1216]) mvBlueFOX3-2032 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0032Z (3.2 Mpix [2064 x 1544]) mvBlueFOX3-2032a / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0032A (3.2 Mpix [2064 x 1544]) mvBlueFOX3-2051 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0051Z (5.1 Mpix [2464 x 2056]) mvBlueFOX3-2051a / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0051A (5.1 Mpix [2464 x 2056]) mvBlueFOX3-2071 / BVS CA-SF2-0071Z (7.1 Mpix [3216 x 2208]) mvBlueFOX3-2071a / BVS CA-SF2-0071A (7.1 Mpix [3216 x 2208]) mvBlueFOX3-2089 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0089Z (8.9 Mpix [4112 x 2176]) mvBlueFOX3-2089a / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0089A (8.9 Mpix [4112 x 2176]) mvBlueFOX3-2124 / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0124Z (12.4 Mpix [4112 x 3008]) mvBlueFOX3-2124a / [BVS CA-SF2|BVS CA-SF5|BF3-5M]-0124A (12.4 Mpix [4112 x 3008]) [BVS CA-SF4|BF3-4]-0169Z / [BVS CA-SF5|BF3-5M]-0169Z (16.9 Mpix [5472 x 3080]) [BVS CA-SF4|BF3-4]-0196Z / [BVS CA-SF5|BF3-5M]-0196Z (19.6 Mpix [4432 x 4432]) [BVS CA-SF4|BF3-4]-0315Z / [BVS CA-SF5|BF3-5M]-0315Z (31.5 Mpix [6480 x 4856])

1 Measured accord. to EMVA1288 with gray scale version of the camera
2 Connection via Type C recommended VBUS>900mA

Sony Starvis

Sensors 6.4 Mpix (-064)12.4 Mpix (-124r)20.5 Mpix (-205)
Sensor supplier SonySonySony
Sensor name IMX178IMX226IMX183
Res. 3096 x 2080
gray scale / RGB
4064 x 3044
gray scale / RGB
5544 x 3692
gray scale / RGB
Sensor size 1/1.8" 1/1.7" 1"
Max. FPS (in free-running full frame mode) 59 30.7 18.6
FPS exactnessxxx
ADC resolution / Out 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8
SNRmax [dB]1/41.6 40.3 41.6
DR (normal / HDR) [dB]1/71.6 69.2 71.5
Rolling shutter√√√
Global shutterxxx
Global Resetxxx
Trigger (HW / SW)- /√- /√- /√
Pipelined GSxxx
Linescan modexxx
High color reproductivity (for color version) √√√
Power consumption [W] approx. 2.9 approx. 2.9 approx. 2.9
More specific data -0064Z-0124R-0205Z

1 Measured accord. to EMVA1288 with gray scale version of the camera

Sony Polarsens

Sensors 5.1 Mpix (-2051p)
Sensor supplier Sony
Sensor name IMX250_POL
Res. 2464 x 2056
gray scale / RGB
Sensor size 2/3"
Max. FPS (in free-running full frame mode) 80
FPS exactnessx
ADC resolution / Out 12 / 12, 10, 8
SNRmax [dB]1/40.2
DR (normal / HDR) [dB]1/71.2
Rolling shutterx
Global shutter√
Global Resetx
Trigger (HW / SW)√/√
Pipelined GS√
Linescan modex
High color reproductivity (for color version) √
Power consumption [W] approx. 3.6
More specific data -0051P

1 Measured accord. to EMVA1288 with gray scale version of the camera

Sony SenSWIR

Sensors 0.3 Mpix (-2003s)1.3 Mpix (-2013s)1.3 Mpix (-2032s)5.3 Mpix (-2053s)
Sensor supplier SonySonySonySony
Sensor name IMX991IMX990IMX993IMX992
Res. 656 x 520
gray scale
1296 x 1032
gray scale
2080 x 1544
gray scale
2592 x 2056
gray scale
Sensor size 1/4" 1/2" 1/1.8" 1/1.4"
Max. FPS (in free-running full frame mode) 239.3 [burst mode required] / 239.3 [streaming] 124.9 [burst mode required] / 124.9 [streaming] 114.6 [burst mode required] / 114.6 [streaming] 72.6 [burst mode required] / 71.3 [streaming]
FPS exactnessxxxx
ADC resolution / Out 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / 12, 10, 8
SNRmax [dB]1/51.1 51.1 46.2 tbd
DR (normal / HDR) [dB]1/56.89 56.84 50.53 tbd
Rolling shutterxxxx
Global shutter√√√√
Global Resetxxxx
Trigger (HW / SW)√/√√/√√/√√/√
Pipelined GS√√√√
Linescan modexxxx
High color reproductivity (for color version) xxxx
Power consumption @ 24 V [W] approx. 1.9 W approx. 2.1 W approx. 3.2 W approx. tbd W
More specific data -0003S-0013S-0032S-0053S

1 Measured accord. to EMVA1288 with gray scale version of the camera

Aptina, CMOSIS, e2v

Sensors 1.2 Mpix (-x012b)1.2 Mpix (-x012d)1.3 Mpix (-x013)2 Mpix (-x020)2 Mpix (-x020a)3.1 Mpix (-x031)10 Mpix (-x100)14 Mpix (-x140)
Sensor supplier AptinaAptinae2ve2ve2vAptinaAptinaAptina
Sensor name MT9M031MT9M034EV76C560EV76C570EV76C570AR0331MT9J003MT9F002
Res. 1280 x 960
gray scale / RGB
1280 x 960
gray scale / RGB
1280 x 1024
gray scale / RGB
1600 x 1200
gray scale / RGB
1600 x 1200
gray scale / RGB
2048 x 1536
RGB
3856 x 2764
gray scale / RGB
4384 x 3288
RGB Bayer mosaic
Sensor size 1/3" 1/3" 1/1.8" 1/1.8" 1/1.8" 1/3" 1/2.3" 1/2.3"
Pixel clock [MHz]40 / 66 / 74.2540 / 66 / 74.2585 85 85 25 / 50 81.25 96.88
Max. FPS (in free-running full frame mode) 45.6 45.6 60 51 60 22.2 7 6
FPS exactnessxxxxxxxx
ADC resolution / Out [bit]12 / 12, 10, 8 12 / 12, 10, 8 10 / (12), 10, 8 10 / (12)(HW / SW), 10, 8 10 / (12), 10, 8 12 / 12, 10, 8 12 / 12, 10, 8 12 / (12), 10, 8
SNRmax [dB]1/37.437.7 39 38.9 38.9 37.2 35.1
DR (normal / HDR) [dB]1/54.3 / 63.4 / 50.5 / 50.7 / 50.5 / / 56 / 57.3 /
Rolling shutterx√xxx√√√
Global shutter√x√√√xxx
Global Resetxxxxx√√√
Trigger (HW / SW)√/√√/√√/√√/√√/√√/√√/√√/√
Pipelined GSxxxxxxxx
Linescan modexxavailable available available xxx
High color reproductivity (for color version) √√√√√√√√
Power consumption [W] approx. 2.25 approx. 2.3 approx. 2.3 approx. 2.25 approx. 2.25 approx. 2.45 approx. 2.55 approx. 2.25
More specific data -1012b-1012d-0013Z-0020Z-0020A-0031Z-0107Z-1140

1 Measured accord. to EMVA1288 with gray scale version of the camera

Supported image formats

Gray scale versionColor version
Mono8
Mono10
Mono12
Mono14
Mono16
 RGB8Packed
 BGR8Packed
 BGRA8Packed
 BGR10V2Packed
 YUV422Packed
 YUV422_YUYVPacked
 YUV444Packed
See also
For more details about the image formats, please have a look at the enums "TImageDestinationPixelFormat" and "TImageBufferPixelFormat" in the C++ developers section.
An example application about the pixel formats is also available.