Impact Acquire SDK Python
Loading...
Searching...
No Matches
Device Specific Interface Layout

Classes and functions that will be available if the device is used in device specific interface layout. More...

Data Structures

class  AutoControlParameters
 A class to control the automatic control parameters of a device(Device specific interface layout only). More...
class  BasicDeviceSettingsWithAOI
 A base class for camera related settings(Device specific interface layout only). More...
class  CameraDescriptionBase
 A base class to describe a camera (Device specific interface layout only) connected to a frame grabber (deprecated). More...
 A class to describe a CameraLink® compliant camera(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionDigital
 A class to describe a non-standard digital video signal(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionDigitalBase
 A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionDigitalBase2
 A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionManager
 Grants access to camera description objects(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionNonStandard
 A class describing non-standard video cameras(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionSDI
 A base class to describe an SDI(Serial Digital Interface) camera signal (Device specific interface layout only) (deprecated). More...
class  CameraDescriptionStandard
 A class describing analogue standard compliant video cameras(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionStandardBase
 An internal base class to describe standard analogue video cameras(Device specific interface layout only) (deprecated). More...
class  CameraSettingsBase
 A base class for camera related settings(Device specific interface layout only). More...
class  CameraSettingsBlueCOUGAR
 mvBlueCOUGAR related camera settings (Device specific interface layout only). More...
class  CameraSettingsBlueDevice
 A base class for camera related settings belonging to the mvBlueXXX-series (Device specific interface layout only). More...
class  CameraSettingsBlueFOX
 mvBlueFOX related camera settings(Device specific interface layout only). More...
class  CameraSettingsFrameGrabber
 A class to access frame grabber related camera settings(Device specific interface layout only) (deprecated). More...
class  CameraSettingsV4L2Device
 mvV4L2 related camera settings(Device specific interface layout only). More...
class  CameraSettingsVirtualDevice
 mvVirtualDevice related camera settings(Device specific interface layout only). More...
class  Connector
 A class describing how a video signal source(e.g. More...
class  DigitalInput
 A class to represent a digital input pin(Device specific interface layout only). More...
class  DigitalIOMeasurementControl
 Properties for configuring settings belonging to the digital I/O measurement(Device specific interface layout only). More...
class  DigitalOutput
 A class to represent a digital output pin(Device specific interface layout only). More...
class  HDRControl
 A class to control the HDR (High Dynamic Range) parameters of a device (Device specific interface layout only). More...
class  HDRKneePoint
 A class to configure a HDR (High Dynamic Range) knee point (Device specific interface layout only). More...
class  I2CControl
 Properties for accessing features belonging to the I2C control(Device specific interface layout only). More...
class  ImageMemoryManager
 An interface class to access DMA memory related properties(Device specific interface layout only) (deprecated). More...
class  InfoBlueCOUGAR
 A more specific class to query information about a mvBlueCOUGAR devices and its driver(Device specific interface layout only). More...
class  InfoBlueDevice
 A more specific class to query information about a mvBlueDevice device and its driver(Device specific interface layout only). More...
class  InfoBlueFOX
 A more specific class to query information about a mvBlueFOX device and its driver(Device specific interface layout only). More...
class  IOSubSystem
 A base class to handle digital inputs and outputs(Device specific interface layout only). More...
class  IOSubSystemBlueFOX
 A class to handle the digital inputs and outputs for mvBlueFOX USB cameras(Device specific interface layout only). More...
class  IOSubSystemCommon
 A base class to handle the digital inputs and outputs for devices (Device specific interface layout only). More...
class  IOSubSystemFrameGrabber
 A class to handle the digital inputs and outputs for frame grabber devices(Device specific interface layout only) (deprecated). More...
class  MotorFocusControl
 Properties for configuring settings belonging to the motor focus control (Device specific interface layout only). More...
class  OutputSignalGeneratorBlueDevice
 A class to create complex digital output signals(Device specific interface layout only). More...
class  OutputSignalGeneratorFrameGrabber
 A class to create complex digital output signals(Device specific interface layout only) (deprecated). More...
class  PulseStartConfiguration
 A class to configure the creation of digital signals passed to one or more of the digital outputs of a device(Device specific interface layout only). More...
class  RTCtrProgram
 A class to represent real time control programs(Device specific interface layout only). More...
class  RTCtrProgramStep
 A class to represent one step of a real time control(RTCtr) program (Device specific interface layout only). More...
class  SettingsBlueFOX
 This class provides access to general settings as well as to settings which are unique for the mvBlueFOX(Device specific interface layout only). More...
class  SystemBlueFOX
 A class containing mvBlueFOX specific settings to control the overall behaviour of the driver(Device specific interface layout only). More...
class  SystemV4L2
 A class containing mvV4L2 specific settings to control the overall behaviour of the driver(Device specific interface layout only). More...

Detailed Description

Classes and functions that will be available if the device is used in device specific interface layout.

This group contains classes and functions that will be available if the device is used in mvIMPACT.acquire.dilDeviceSpecific interface layout.