Impact Acquire SDK Java
Loading...
Searching...
No Matches
Device Specific Interface Layout

Classes and functions that will be available if the device is used in device specific interface layout. More...

Classes

class  AutoControlParameters
 A class to control the automatic control parameters of a device(Device specific interface layout only). More...
class  BasicDeviceSettingsWithAOI
 A base class for camera related settings(Device specific interface layout only). More...
class  CameraDescriptionBase
 A base class to describe a camera (Device specific interface layout only) connected to a frame grabber (deprecated). More...
 A class to describe a CameraLink® compliant camera(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionDigital
 A class to describe a non-standard digital video signal(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionDigitalBase
 A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionDigitalBase2
 A base class to describe an arbitrary digital camera signal(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionManager
 Grants access to camera description objects(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionNonStandard
 A class describing non-standard video cameras(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionSDI
 A base class to describe an SDI(Serial Digital Interface) camera signal (Device specific interface layout only) (deprecated). More...
class  CameraDescriptionStandard
 A class describing analogue standard compliant video cameras(Device specific interface layout only) (deprecated). More...
class  CameraDescriptionStandardBase
 An internal base class to describe standard analogue video cameras(Device specific interface layout only) (deprecated). More...
class  CameraSettingsBase
 A base class for camera related settings(Device specific interface layout only). More...
class  CameraSettingsBlueCOUGAR
 mvBlueCOUGAR related camera settings (Device specific interface layout only). More...
class  CameraSettingsBlueDevice
 A base class for camera related settings belonging to the mvBlueXXX-series (Device specific interface layout only). More...
class  CameraSettingsBlueFOX
 mvBlueFOX related camera settings(Device specific interface layout only). More...
class  CameraSettingsFrameGrabber
 A class to access frame grabber related camera settings(Device specific interface layout only) (deprecated). More...
class  CameraSettingsV4L2Device
 mvV4L2 related camera settings(Device specific interface layout only). More...
class  CameraSettingsVirtualDevice
 mvVirtualDevice related camera settings(Device specific interface layout only). More...
class  Connector
 A class describing how a video signal source(e.g. More...
class  DigitalInput
 A class to represent a digital input pin(Device specific interface layout only). More...
class  DigitalIOMeasurementControl
 Properties for configuring settings belonging to the digital I/O measurement(Device specific interface layout only). More...
class  DigitalOutput
 A class to represent a digital output pin(Device specific interface layout only). More...
class  HDRControl
 A class to control the HDR (High Dynamic Range) parameters of a device (Device specific interface layout only). More...
class  HDRKneePoint
 A class to configure a HDR (High Dynamic Range) knee point (Device specific interface layout only). More...
class  I2CControl
 Properties for accessing features belonging to the I2C control(Device specific interface layout only). More...
class  ImageMemoryManager
 An interface class to access DMA memory related properties(Device specific interface layout only) (deprecated). More...
class  InfoBlueCOUGAR
 A more specific class to query information about a mvBlueCOUGAR devices and its driver(Device specific interface layout only). More...
class  InfoBlueDevice
 A more specific class to query information about a mvBlueDevice device and its driver(Device specific interface layout only). More...
class  InfoBlueFOX
 A more specific class to query information about a mvBlueFOX device and its driver(Device specific interface layout only). More...
class  IOSubSystem
 A base class to handle digital inputs and outputs(Device specific interface layout only). More...
class  IOSubSystemBlueFOX
 A class to handle the digital inputs and outputs for mvBlueFOX USB cameras(Device specific interface layout only). More...
class  IOSubSystemCommon
 A base class to handle the digital inputs and outputs for devices (Device specific interface layout only). More...
class  IOSubSystemFrameGrabber
 A class to handle the digital inputs and outputs for frame grabber devices(Device specific interface layout only) (deprecated). More...
class  MotorFocusControl
 Properties for configuring settings belonging to the motor focus control (Device specific interface layout only). More...
class  OutputSignalGeneratorBlueDevice
 A class to create complex digital output signals(Device specific interface layout only). More...
class  OutputSignalGeneratorFrameGrabber
 A class to create complex digital output signals(Device specific interface layout only) (deprecated). More...
class  PulseStartConfiguration
 A class to configure the creation of digital signals passed to one or more of the digital outputs of a device(Device specific interface layout only). More...
class  RTCtrProgram
 A class to represent real time control programs(Device specific interface layout only). More...
class  RTCtrProgramStep
 A class to represent one step of a real time control(RTCtr) program (Device specific interface layout only). More...
class  SettingsBlueFOX
 This class provides access to general settings as well as to settings which are unique for the mvBlueFOX(Device specific interface layout only). More...
class  SystemBlueFOX
 A class containing mvBlueFOX specific settings to control the overall behaviour of the driver(Device specific interface layout only). More...
class  SystemV4L2
 A class containing mvV4L2 specific settings to control the overall behaviour of the driver(Device specific interface layout only). More...
class  TAcquisitionField
 Defines which field triggers the start of the acquisition (deprecated). More...
class  TAutoControlMode
 Defines valid auto control modes. More...
class  TAutoControlSpeed
 Defines valid auto-control speed modes. More...
class  TAutoExposureControl
 Defines valid AEC( Automatic Exposure Control ) modes. More...
class  TAutoGainControl
 Defines valid AGC( Automatic Gain Control ) modes. More...
class  TAutoOffsetCalibration
 Defines valid offset calibration modes. More...
class  TBlueFOXDigitalInputThreshold
 Defines valid thresholds( in Volt ) for the digital inputs of the. More...
class  TBlueFOXFooterMode
 Defines the footer mode of the mvBlueFOX. More...
class  TBlueFOXInfoSensorCapabilities
 Defines valid image sensor capabilities. More...
class  TBlueFOXOffsetAutoBlackSpeed
 Defines Offset Auto Calibration Controller Speed. More...
class  TBlueFOXSensorTiming
 Sensor timing options. More...
class  TBlueFOXTransferSize
 Defines the block size used for the USB transfer of the mvBlueFOX. More...
class  TCameraAoiMode
 Defines the camera Aoi modes. More...
class  TCameraBinningMode
 Defines valid binning modes for the camera. More...
class  TCameraExposeMode
 Defines recognized camera sensor expose modes. More...
class  TCameraExternalSyncEdge
 Some grabbers are able to get the video signal and sync signals ( HD-IN, VD-IN ) on separate lines. More...
class  TCameraExternalSyncOutput
 Some grabbers are able to get the video signal and the sync signal on different input pins. More...
class  TCameraFlashMode
 Defines valid camera flash modes. More...
class  TCameraFlashType
 Defines valid camera flash control types. More...
class  TCameraHDRMode
 Defines valid camera High Dynamic Range modes. More...
class  TCameraInterlacedType
 Defines how the camera transmits its video signal (deprecated). More...
class  TCameraLinkDataValidMode
 Defines how the camera transmits the DVAL signal defined in the CameraLink® standard (deprecated). More...
class  TCameraPixelClock
 Defines valid camera pixel frequencies. More...
class  TCameraScanMode
 Defines valid scan modes for the a camera. More...
class  TCameraSerialPortBaudRate
 Defines valid baud rates for serial port communication between frame grabber and camera (deprecated). More...
class  TCameraShutterMode
 Defines recognized camera sensor shutter modes. More...
class  TCameraTapsXGeometry
 Multitap cameras can transmit data in different ways. More...
class  TCameraTapsYGeometry
 Multi-tap cameras can transmit data in different ways. More...
class  TCameraTestMode
 Defines valid transmission modes for the camera. More...
class  TCameraTriggerMode
 Defines valid camera sensor trigger modes. More...
class  TCameraTriggerSource
 Defined valid camera sensor trigger source values. More...
class  TClampMode
 Clamp signal means, that an AC coupled video signal is clamped on the porch to get a signal transfer with less noise and independent from the d.c. More...
class  TDeviceAdvancedOptions
 Defines valid advanced options. More...
class  TDeviceDigitalOutputMode
 Defines grabber specific digital output modes. More...
class  TDeviceImageTrigger
 Defines acquisition start event if using pulse sequences (deprecated). More...
class  TDevicePowerMode
 Defines the power mode for this device. More...
class  TDeviceScanRateMode
 Defines valid device scan rate mode (deprecated). More...
class  TDeviceSignalOutputStartEvent
 Defines valid moments to start the signal generation on the digital outputs (deprecated). More...
class  TDeviceSyncOutMode
 Valid sync. More...
class  TDeviceTriggerInterface
 Defines which trigger interface is currently active for the device. More...
class  TDeviceTriggerMode
 Valid trigger modes for frame grabber boards (deprecated). More...
class  TDeviceTriggerOverlap
 Specifies the type trigger overlap permitted with the previous frame (deprecated). More...
class  TDigIOState
 Defines valid digital I/O states. More...
class  TDigitalIOMeasurementMode
 Defines valid IO Measurement Modes. More...
class  TDigitalIOMeasurementSource
 Defines valid IO Measurement Sources. More...
class  TDigitalOutputControlMode
 Defines valid ways to create signals on a digital output (deprecated). More...
class  TDigitalSignal
 Defines valid digital source signal constants that can be used to configure a devices behaviour in certain digital I/O related modes (deprecated). More...
class  TFieldGateMode
 The field gate is used to detect the field ( odd or even ) for interlaced video signals (deprecated). More...
class  TI2COperationMode
 Valid I2C operation modes. More...
class  TI2COperationStatus
 Valid I2C operation status values. More...
class  TInfoSensorColorMode
 Defines the type of camera sensor. More...
class  TInfoSensorColorPattern
 Defines the bayer pattern of the sensor. More...
class  TInfoSensorType
 Defines the type of camera sensor. More...
class  TInterlacedMode
 Defines how to handle interlaced image data (deprecated). More...
class  TLineCounter
 Currently available for mvTITAN/mvGAMMA-CL (deprecated). More...
class  TOnBoardMemoryMode
 Defines valid modes for the handling of the device' on board memory (if available) (deprecated). More...
class  TPulseStartTrigger
 Defines valid pulse start trigger values. More...
class  TRTCtrlModes
 Defines valid RTCtrl Modes. More...
class  TRTProgOpCodes
 Defines valid RTProg OpCodes. More...
class  TScanClock
 Analogue grabbers generate its scan clock on different ways (deprecated). More...
class  TScanStandard
 Defines valid scan modes for standard cameras (deprecated). More...
class  TTriggerMoment
 Defines a trigger moment for a digital signal. More...
class  TVirtualDeviceImageType
 Defines valid image types used when capturing data from a certain directory. More...
class  TVirtualDeviceTestMode
 Defines valid test modes for virtual devices. More...

Detailed Description

Classes and functions that will be available if the device is used in device specific interface layout.

This group contains classes and functions that will be available if the device is used in mvIMPACT.acquire.TDeviceInterfaceLayout.dilDeviceSpecific interface layout.