Balluff - BVS CA-GV Technical Documentation
Toggle main menu visibility
Loading...
Searching...
No Matches
Related Pages
Here is a list of all related documentation pages:
Order Code Nomenclature
What's inside and accessories
Technical Data
Sensor Overview
Summary of CMOS sensors
Filters
APIs And Tools
GenICam™ GenTL Software Stack
The Impact Acquire Software Stack
Developing Applications Using The Impact Acquire SDK
GUI Tools
Relationship Between Framework, Firmware And SDK
GenICam™ And Advanced Features
About Settings
DirectShow Interface
Troubleshooting
Error Code List
Accessing log files
General Issues
I can see the camera in IPConfigure, but I cannot access the camera
Image Data Is Lost (Incomplete Frames)
The error counter increases
I get an exception when setting OffsetX or OffsetY
I get an oscillating frame rate
Why does updating the device list take so long
Windows®
The 'LostImagesCount' increases
VLC Media Player Issues
Linux
No GenICam™ devices are detected on a Linux system
No GigE Vision™ devices are detected on a Linux system
Glossary
Related Manuals
Use Cases
Introducing acquisition / recording possibilities
Acquiring a number of images
Recording sequences with pre-trigger
Creating acquisition sequences (Sequencer Control)
Generating very long exposure times
Working with multiple AOIs (mv Multi Area Mode)
Using the mvMultiExposureCount feature
Using the BlockScan feature
Working with Event Control
Using Video Stream Recording
Introducing multicasting
Using the Particle Image Velocimetry (PIV) shutter feature
Working with the dual exposure feature ("mvMultiZone")
Improving the acquisition / image quality
Correcting image errors of a sensor
Optimizing the color/luminance fidelity of the camera
Setting a flicker-free auto expose and auto gain
Working with binning / decimation
Improving the communication
Optimizing the bandwidth
Discovering Devices In Different Subnets
Working with triggers
Processing triggers from an incremental encoder
Generating a pulse width modulation (PWM)
Outputting a pulse at every other external trigger
Creating different exposure times for consecutive images
Detecting overtriggering
Triggering of an indefinite sequence with precise starting time
Low latency triggering
Working with I/Os
Controlling strobe or flash at the outputs
Creating a debouncing filter at the inputs
Mapping UserOutputs to Physical Outputs in the Sequencer
Working with LUTs
Introducing LUTs
Working with LUTValueAll
Implementing a hardware-based binarization
Saving data on the device
Creating user data entries
Creating user set entries
Working with the UserFile section (Flash memory)
Working with device features
Working with the temperature sensors
Disabling the heartbeat
Reset timestamp by hardware
Synchronizing camera timestamps
Working With The Serial Interface (mv Serial Interface Control)
Working with several cameras simultaneously
Using Action Commands
Creating synchronized acquisitions
Using the primary application switchover functionality
Working with 3rd party tools
Using VLC Media Player
Working with ROS (Robot Operating System)
Working with GStreamer - The Impact Acquire GenICam GStreamer Plugin
Appendix A. Specific Camera / Sensor Data
A.1 Pregius S CMOS (Mono)
BVS CA-GV1-0032BG (3.2 Mpix [2064 x 1552])
Device Feature And Property List
BVS CA-GV1-0051DG (5.1 Mpix [2472 x 2064])
Device Feature And Property List
BVS CA-GV1-0081AG (8.1 Mpix [2856 x 2848])
Device Feature And Property List
BVS CA-GV1-0081UG (8.1 Mpix [2848 x 2848])
Device Feature And Property List
BVS CA-GV1-0124DG (12.4 Mpix [4128 x 3008])
Device Feature And Property List
BVS CA-GV2-0124FG (12.4 Mpix [6048 x 2048])
Device Feature And Property List
BVS CA-GV1-0162AG (16.2 Mpix [5328 x 3040])
Device Feature And Property List
BVS CA-GV2-0164AG (16.4 Mpix [8016 x 2048])
Device Feature And Property List
BVS CA-GV1-0204AG (20.4 Mpix [4512 x 4512])
Device Feature And Property List
BVS CA-GV1-0246AG (24.6 Mpix [5328 x 4608])
Device Feature And Property List
A.2 Pregius S CMOS (Color)
BVS CA-GV1-0032BC (3.2 Mpix [2064 x 1552])
Device Feature And Property List
BVS CA-GV1-0051DC (5.1 Mpix [2472 x 2064])
Device Feature And Property List
BVS CA-GV1-0081AC (8.1 Mpix [2856 x 2848])
Device Feature And Property List
BVS CA-GV1-0124DC (12.4 Mpix [4128 x 3008])
Device Feature And Property List
BVS CA-GV2-0124FC (12.4 Mpix [6048 x 2048])
Device Feature And Property List
BVS CA-GV1-0162AC (16.2 Mpix [5328 x 3040])
Device Feature And Property List
BVS CA-GV2-0164AC (16.4 Mpix [8016 x 2048])
Device Feature And Property List
BVS CA-GV1-0204AC (20.4 Mpix [4512 x 4512])
Device Feature And Property List
BVS CA-GV1-0246AC (24.6 Mpix [5328 x 4608])
Device Feature And Property List
A.3 SenSWIR CMOS (Mono)
BVS CA-GV2-0003TG (0.3 Mpix [656 x 520])
Device Feature And Property List
BVS CA-GV2-0013TG (1.3 Mpix [1296 x 1032])
Device Feature And Property List
BVS CA-GV1-0032SG (3.2 Mpix [2080 x 1544])
Device Feature And Property List
BVS CA-GV2-0032TG (3.2 Mpix [2080 x 1544])
Device Feature And Property List
BVS CA-GV1-0053SG (5.3 Mpix [2592 x 2056])
Device Feature And Property List
BVS CA-GV2-0053TG (5.3 Mpix [2592 x 2056])
Device Feature And Property List
Appendix B. Product Comparison
Generated on
3.8.0