|
Impact Acquire SDK GUI Applications
|
ImpactControlCenter will start with the Quick Setup Wizard if a device with a suitable feature set has been selected and used:
If supported the Quick Setup Wizard is the recommended way of capturing the first images. Later or when a third party device or a Balluff device without the feature required by this wizard is used when started the first time the application will look more or less like this:
On the left-hand side of the upper toolbar a drop down box will list all devices currently recognized by the Impact Acquire framework. If you find that a device is missing first make sure that you have its corresponding support files have been installed (e.g. by clicking on the "Info" button in the upper toolbar) and then make sure that the corresponding interface technology and the interface the device is connected to (e.g. a network card (NIC)) is enabled for enumeration. This can be seen by pressing the "Info" button in the upper toolbar. This would then open the Detailed Driver Information dialog.
To work with a device select it from the drop-down box and press the "Use" button.
Devices plugged into the system after the application has been started might not be listed until the "Update" button has been pressed. When this button is pressed every installed support library will rescan all interfaces for new devices so this will take some time.
In the middle of the upper toolbar various controls to either launch the Quick Setup Wizard or to start and stop the acquisition manually are located. In the right section of the upper toolbar recording of series of images into the RAM of the host computer can be configured. All these control will become available after a device has been initialized by pressing the "Use" button.
Depending on your experience and/or needs you might want to see/do more than shown above. This can be achieved via the "Settings" menu:
Once the left toolbar is available there is more that can be activated. The most interesting feature is probably the Image Analysis tab control on the lower right of the application:
With all features enabled ImpactControlCenter then will look somewhat like this:
Pressing F1 will also display a detailed list of available Command-line Interface options as well as keyboard shortcuts and some other useful information!
After having successfully initialized a device the tree control in the lower left part of the "Main Window" will display the properties (settings or parameters) (according to the "interface layout") accessible by the user.