Balluff - BVS CA-GX0 / BVS CA-GX2 Technical Documentation
Loading...
Searching...
No Matches
System Requirements

Host System

The BVS CA-GX0/BVS CA-GX2 is a high-performance camera which requires a high data throughput on the host system, for example, when processing large amount of image data and high CPU resources if processing color images on the host PC.

For this reason we recommend at least the following components:

ComponentRecommendation
ProcessorPreferably multi core Intel or ARM CPUs
RAM4 GB in 32-bit OS; 8 GB in 64-bit OS
MainboardLatest PC architecture and chipset
PCIe (for BVS CA-GX2)x1 or x4 slot for the Network interface card

Recommended Accessories

ComponentRecommendation
Network interface card (for BVS CA-GX2)With the latest "Link Aggregate Group" (LAG) capable device drivers

Several network interface cards have been tested successfully by Balluff. Please ask our support team.

See also
https://www.balluff.com/en-de/contact-support

Please ask your system vendor for further advice and consult our technical documentation.

Network interface card (NIC) settings

We recommend following network interface card (NIC) settings:

ParameterSetting
Receive bufferMaximum
Transmitter bufferMaximum
MTUMaximum; the network interface card should support at least 4 KB jumbo frames, preferably 9 KB
Interrupt moderationActive
Interrupt moderation rateExtreme / Aggressive
RSSActive
Number of RSS queuesNumber of physical CPU cores (Logical/Hyper-Threading will be ignored. E.g. 8 physical cores and Hyper-Threading = 16 logical CPU cores; for RSS receive queues a value smaller or equal to the number of physical cores should be selected.
Link Aggregation / Teaming / Bonding (for BVS CA-GX2)Active

For more information about network settings, please have a look at the troubleshooting chapter Optimizing Network Performance .

Supported Operating Systems

The following operating system are supported officially:

Windows®

  • Microsoft Windows® 10 (64-bit)
  • Microsoft Windows® 11

Other Windows® versions might work as well but will not be tested on a regular basis. A complete list of supported Windows® versions can be found here.

Linux

The latest version for the required target platform of the Impact Acquire framework can always be found here.

Currently supported Kernel versions are:

  • Kernel 3.5.x or greater

In case the target system runs an older Linux kernel, it is absolutely necessary to update the kernel to at least version 3.5.0. Please refer to the documentation of your Linux distribution for information on how to update your system's Linux kernel.

All Kernels starting from version 3.5.0 should work without problems.

macOS

The latest version for the required target platform of the Impact Acquire framework can always be found here.

The currently supported macOS version is 12 (Monterey)