|
Balluff - BVS CA-GX0 / BVS CA-GX2 Technical Documentation
|
When developing machine vision applications using Docker containers, it might be required to access GigE Vision™ devices inside the container. With the Impact Acquire framework this can be achieved fairly easily and this chapter will demonstrate how to build a basic Docker container where GigE Vision™ devices can be used. It is recommended to use a native Linux machine as host system for this type of application.
The Linux host network interface card has to be first configured for an optimized GigE Vision™ transmission: Checklist for Linux
The Windows® host NIC has to be first configured for an optimized GigE Vision™ transmission: Checklist for Windows®
The macOS host network interface card should be first configured for an optimized GigE Vision™ transmission: Checklist for macOS
The following demo Dockerfile builds a basic Docker image based on the latest stable release version of Debian, where the Impact Acquire GenTL framework including its sample programs are installed. This Dockerfile can be used in many ways:
Before building the Dockerfile, please download the Balluff Impact Acquire framework installer:
Create a directory called ImpactAcquire (as used in this demo Dockerfile) and move both installation files into this directory. In this example, both files are downloaded into the Downloads directory and the ImpactAcquire directory is created inside the Downloads directory:
Make the installation script ImpactAcquire-x86_64-linux-*.sh executable:
Navigate back into the directory where ImpactAcquire resides (e.g. Downloads) and create your Dockerfile:
$ cd ~/Downloads $ touch Dockerfile
Create the content of your Dockerfile. Our demo Dockerfile (for Linux x86_64) looks as follows:
# start with the latest stable release version of Debian
FROM debian:latest
ENV LC_ALL C
ENV DEBIAN_FRONTEND noninteractive
# entrypoint of Docker
CMD ["/bin/bash"]
# set environment variables
ENV TERM linux
ENV MVIMPACT_ACQUIRE_DIR /opt/ImpactAcquire
ENV MVIMPACT_ACQUIRE_DATA_DIR /opt/ImpactAcquire/data
ENV GENICAM_GENTL64_PATH /opt/ImpactAcquire/lib/x86_64
ENV GENICAM_ROOT /opt/ImpactAcquire/runtime
ENV container docker
# update packets and install minimal requirements
# after installation it will clean apt packet cache
RUN apt-get update && apt-get -y install build-essential \
iproute2 && \
apt-get clean && \
rm -rf /var/lib/apt/lists/* /tmp/* /var/tmp/*
# move the directory ImpactAcquire with *.sh file to the container
COPY ImpactAcquire /var/lib/ImpactAcquire
# execute the setup script in an unattended mode
RUN cd /var/lib/ImpactAcquire && \
./ImpactAcquire-x86_64-linux-3.8.1.sh -u -gev && \
rm -rf /var/lib/apt/lists/* /tmp/* /var/tmp/*
GENICAM_GENTL64_PATH defined in this demo Dockerfile should be relaced by GENICAM_GENTL32_PATH instead.Finally, build a Docker image using this Dockerfile:
$ sudo docker build -t [image_name] .
If built successfully, the newly built [image_name] will be listed when calling:
$ sudo docker images
Start the Docker container with --net=host flag, so that it will use the host network instead of the default bridge network:
$ sudo docker run -ti --net=host [image_name] /bin/bash
Since the Docker host mode networking doesn't work on Windows® due to the isolated network namespace of Docker daemon, the container needs to be started using the default bridge network with specific ports published for receiving GigE Vision™ streaming packets. For instance, port 49152 can be used for event messages and port 49153 for streaming packets:
$ sudo docker run -ti -p 49152:49152/udp -p 49153:49153/udp [image_name] /bin/bash
Inside the container, the GigE Vision™ device needs to be discovered first. Since the Docker bridge network resides in a different subnet, unicast needs to be applied in order to discover the GigE Vision™ device. Follow Unicast Device Discovery via IPConfigure or use Impact Acquire SDK (see InterfaceModule.mvUnicastDeviceDiscoveryCommandCount() etc.) to set up the unicast procedure.
Once the GigE Vision™ device has been discovered by unicast and initialized by Device.open(), several GVSP transport layer parameters still need to be configured before being able to receive streaming packets due to the WSL2 NAT network. Here are the parameters that need to be changed manually:
GevMCPHostPort GevSCPHostPort GevSCDA GevSCPSPacketSize manually to 1500After starting the container, the correct operation of GigE Vision™ devices can be validated by running one of the sample programs provided by the Impact Acquire (e.g. SingleCapture):
If the attached GigE Vision™ device appears in the device list of the program's output, access to it in the container by using the Impact Acquire has been established. Now the GigE Vision™ device can be used inside the Docker container for your machine vision applications.