|
Balluff - BVS CA-GX0 / BVS CA-GX2 Technical Documentation
|
A device that became unusable or is no longer needed must be disposed of in an environmentally responsible manner in accordance with the applicable, country-specific waste disposal regulations. Do not dispose of the product with household trash.
BVS CA-GX0/BVS CA-GX2 devices might offer options for storing personal data. The following sections provide an overview of the different types of personal data and the corresponding storage locations. If this section does not contain any information about personal data, the device does not offer any storage options.
In case a persistent network configuration has been stored on the device, it can be removed by overwriting the configuration with a new one and disabling the use of a persistent configuration. The easiest way to do this is to use IPConfigure.
In case custom user data such as calibration data or other information has been stored on the device, this can be deleted using the API that has been used for storing the data as described e.g. by Creating user data entries.
In case a user defined name (DeviceUserID in GenICam™ SFNC compliant devices) has been stored on the device, this can be deleted again by overwriting it.
In case user sets have been stored on the device, the easiest way to delete them is by applying a firmware update to the device, which unless configured specifically otherwise will delete all user sets in the process. One way to do this is by using DeviceConfigure.
In case a user file has been stored on the device using the GenICam™ SFNC compliant FileAccessControl features, this can be deleted again by overwriting it. See Working with the UserFile section (Flash memory) for more information.