|
Balluff - BVS CA-GX0 / BVS CA-GX2 Technical Documentation
|
BVS CA-GX0/BVS CA-GX2 devices offer a 64 KByte section in the Flash memory that can be used to upload a custom file to (UserFile).
To read or write this file you can use the following GenICam File Access Control and its interfaces:
ImpactControlCenter offers a wizard for the File Access Control usage:
The header providing the file access related classes must be included into the application:
#include <mvIMPACT_CPP/mvIMPACT_acquire_GenICam_FileStream.h>
A write access then will look like:
const string fileNameDevice("UserFile");
// uploading a file
mvIMPACT::acquire::GenICam::ODevFileStream file;
file.open( pDev, fileNameDevice.c_str() );
if( !file.fail() )
{
// Handle the successful upload.
}
else
{
// Handle the error.
}
A read access will look like:
const string fileNameDevice("UserFile");
// downloading a file works in a similar way
mvIMPACT::acquire::GenICam::IDevFileStream file;
file.open( pDev, fileNameDevice.c_str() );
if( !file.fail() )
{
// Handle the successful upload.
}
else
{
// Handle the error.
}
You can find a detailed code example in the C++ API manual in the documentation of the classes mvIMPACT::acquire::GenICam::IDevFileStream and mvIMPACT::acquire::GenICam::ODevFileStream