Power supply
| UUSBPOWER_IN | Power supply via USB | 4.75 | 5 | 5.25 | V |
| IUSBPOWER_IN (@ 5V / 40MHz) | | | 280 | 500 | mA |
| IUSBPOWER_IN (Power Off Mode - only with BVS CA-IGC / BVS CA-MLC) | | | 66 | | mA |
Standard version (mvBlueFOX-xxx)
Dimensions and connectors
Figure 1: Connectors mvBlueFOX
| Size without lens (w x h x l) | 38.8 x 38.8 x 58.5 mm (CCD version)
38.8 x 38.8 x 53.1 mm (CMOS version) |
| General tolerance | DIN ISO 2768-1-m (middle) |
Figure 2: Dimensional drawing of tripod adapter
D-Sub 9-pin (male)
Figure 3: D-Sub 9-pin (male), digital I/O
| 1 | IN0- | Negative terminal of opto-isolated input 1 |
| 2 | OUT0- | Negative terminal of opto-isolated output (emitter of npn-phototransistor) |
| 3 | OUT1- | Negative terminal of opto-isolated output (emitter of npn-phototransistor) |
| 4 | IN1- | Negative terminal of opto-isolated input * |
| 5 | N/C | |
| 6 | IN0+ | Positive terminal of opto-isolated input * |
| 7 | OUT0+ | Positive terminal of opto-isolated output (collector of npn-phototransistor) |
| 8 | OUT1+ | Positive terminal of opto-isolated output (collector of npn-phototransistor) |
| 9 | IN1+ | Positive terminal of opto-isolated input * |
1 Voltage between + and - may be up to 26V, input current is 17mA.
Characteristics of the digital inputs
Open inputs will be read as a logic zero.
When the input voltage rises above the trigger level, the input will deliver a logic one.
| UIN_TTL | High level input voltage TTL logic | 3 | 5 | 6.5 | V |
| Low level input voltage TTL logic | -0.7 | | 1 | V |
| IIN_TTL | Current TTL logic | | 8.5 | 12 | mA |
| |
| UIN_PLC | High level input voltage PLC logic | 12 | | 24 | V |
| Low level input voltage PLC logic | -0.7 | | 8 | V |
| IIN_PLC | Current PLC logic | | 17 | 25 | mA |
Figure 4: DigIn mvBlueFOX-xxx In ImpactControlCenter you can change between
- TTL (
"DigitalInputThreshold = 2V") and
- PLC (
"DigitalInputThreshold = 10V")
input behavior of the digital inputs using the DigitalInputThreshold property in "Digital I/O -> DigitalInputThreshold":
Figure 5: ImpactControlCenter - DigitalInputThreshold
Characteristics of the digital outputs
| Output | | 30 | | 100 (on state current) |
Figure 6: DigOut mvBlueFOX-xxx
Connecting flash to digital output
You can connect a flash in series to the digital outputs as shown in the following figure, however, you should only use LEDs together with a current limiter:
Figure 7: Connecting flash (LEDs) to DIG OUT
USB connector, type B (USB 2.0)
Figure 8: USB B connector (female)
| 1 | USBPOWER_IN |
| 2 | D- |
| 3 | D+ |
| 4 | GND |
| Shell | shield |
- Note
- The mvBlueFOX is an USB device!
- Attention
- "Surge"
Using both USB ports at the same time can damage the device.
→ Do not connect both USB ports at the same time.
4-pin circular plug-in connector with lock (USB 2.0)
Figure 9: 4-pin circular plug-in connector (female)
| 1 | USBPOWER_IN | Power out from USB |
| 2 | D+ | not connected |
| 3 | GND | GND |
| 4 | D- | not connected |
Manufacturer: Binder
Part number: 99-3390-282-04
- Note
- Differentiation between 'R' and 'U' version is obsolete. New mvBlueFOX versions have both connectors (circular connector and standard USB). The pin assignment corresponds to the description of 'R' version.
-
While mvBlueFOX is connected and powered via standard USB, it is possible to connect additional power via circular connector (only power; the data lines must be disconnected!). Only in this case, the power switch will change the power supply, if the current entry via standard USB is equal to or under the power supply of "circular connector".
- Attention
- "Surge"
Using both USB ports at the same time can damage the device.
→ Do not connect both USB ports at the same time.
LED states
| Camera is not connected or defect | LED off |
| Camera is connected and active | Green light on |
Board-level version (mvBlueFOX-Mxxx)
Dimensions and connectors
Figure 10: mvBlueFOX-M12x (CCD) with C-mount
Figure 11: mvBlueFOX-M10x (CMOS)
| Type | "FB" |
| C-Mount | 17.526 |
| CS-Mount | 12.526 |
Figure 12: Backside view of the board - Note
- The mvBlueFOX-M has a serial I²C bus EEPROM with 64 KBit of which 512 Bytes can be used to store custom arbitrary data.
- See also
- UserDataEntry class description
4-pin Wire-to-Board header (USB 2.0)
| 1 | USBPOWER_IN | Supply voltage | red |
| 2 | USB_DATA- | Data | white |
| 3 | USB_DATA+ | Data | green |
| 4 | GND | Ground | black |
Manufacturer: JST
Part number: B4B-PH-K
12-pin Wire-to-Board header (Dig I/O)
| 1 | FPGA_IO0 | Digital In 0 |
| 2 | FPGA_IO1 | Digital In 1 |
| 3 | FPGA_IO2 | Digital In 2 |
| 4 | FPGA_IO3 | Digital In 3 |
| 5 | FPGA_IO4 | Digital Out 0 |
| 6 | FPGA_IO5 | Digital Out 1 |
| 7 | FPGA_IO6 | Digital Out 2 |
| 8 | FPGA_IO7 | Digital Out 3 |
| 9 | MAINPOWER | Current from the USB cable |
| 10 | GND | Ground |
| 11 | VCC24V | 24 V output (10mA) |
| 12 | GND | Ground |
Manufacturer: JST
Part number: B12B-PH-K
- Attention
- "False tensions or short-circuits"
The digital I/O's are connected directly via a resistor to the FPGA pins and therefore they are not protected. If you connect the digital I/Os without providing a protection you will risk damaging the device.
→ - Provide a protection circuit to the digital I/O's of mvBlueFOX-M. - Afterwards connect the digital I/Os to the FPGA pins.
- See also
- High-Speed USB design guidelines
Contact
Figure 13: Contact, dimensions in mm (in.)
| mm2 | AWG # | Insulation O.D. mm (in.) | |
| 0.05 to 0.22 | 30 to 24 | 0.9 to 1.5 (.035 to .059) | 8.000 |
Material and finish: phosphor bronze, tin-plated
Manufacturer: JST
Part number: SPH-002T-P0.5S
Housing
Figure 14: Housing, dimensions in mm (in.)
| | A | B | |
| 4 | 6.0 (.236) | 9.8 (.386) | 1.000 |
| 12 | 22.0 (.866) | 25.8 (1.016) | 1.000 |
Material and finish: nylon 66, UL94V-0, natural (white)
Manufacturer: JST
Part number: PHR-4 / PHR-12
- See also
- Suitable assembled cable accessories for mvBlueFOX-M: What's inside and accessories
Characteristics of the mvBlueFOX-Mxxx digital I/Os
Dig I/O max. values
| UDIG_IN | Input voltage | -0.3 | 3.6 | V |
Characteristics of the digital inputs
| UDIG_IN_LOW | low level input voltage (IIN = 1.67mA) | -0.3 | 0 | 0.9 | V |
| UDIG_IN_HIGH | high level input voltage (IIN = 1.67mA) | 2.2 | 3.3 | 3.6 | V |
| IIN | input current (@ 3.3V) | 0.4 | | 1.7 | mA |
Figure 15: Digital input mvBlueFOX-Mxxx
Characteristics of the digital outputs
| IDIG_OUT | current at digital output | +-12 | | +-24 | mA |
| UDIG_OUT_HIGH | digital output (IOUT=12mA) | 1.6 | | | V |
| Digital output (IOUT<2mA) | 2.6 | | 3.4 | V |
| UDIG_OUT_LOW | digital output (IOUT=2mA) | | | 0.2 | V |
UDIG_OUT_HIGH min = 2.8 - IOUT * 100
Figure 16: Digital output mvBlueFOX-Mxxx - Attention
- "False tensions or short-circuits"
The digital I/O's are connected directly via a resistor to the FPGA pins and therefore they are not protected. If you connect the digital I/Os without providing a protection you will risk damaging the device.
→ - Provide a protection circuit to the digital I/O's of mvBlueFOX-M. - Afterwards connect the digital I/Os to the FPGA pins.
- Note
- The Dig I/O characteristics of the mvBlueFOX-M are not compatible to the Dig I/O of the mvBlueFOX standard version.
LED states
| Camera is not connected or defect | LED off |
| Camera is connected and active | Green light on |
Accessories mvBlueFOX-Mxxx
mvBlueFOX-M-FC-S
The mvBF-M-FC-S contains high capacity condensers with switching electronics for transferring stored energy of the condensers to external flash LEDs. It is possible to connect 2 pushbuttons/switches to the 8-pin header (CON3 - Control connector). Additionally, 2 LED interfaces are available. There are two version of mvBF-M-FC-S:
- Model 1 can be connected to mvBlueFOX-M with a cable via CON5.
- Model 2 can be mounted on the mvBlueFOX-M via CON1 directly.
Figure 17: Model 1 with CON5 connector
Figure 18: Model 2 with CON1 connector
CON2 - Flash connector
| 1 | Flash + | Flash power |
| 2 | Flash - | Switched to ground (low side switch) |
Manufacturer: JST
Part number: B-2B-PH
CON3 - Control connector
| 1 | GND | LED2 cathode connector / board ground |
| 2 | LED2 output | LED2 anode connector1 |
| 3 | GND | LED1 cathode connector / board ground |
| 4 | LED1 output | LED1 anode connector |
| 5 | GND | Board ground |
| 6 | Input2 | Switch to ground for setting Input2 |
| 7 | GND | Board ground |
| 8 | Input1 | Switch to ground for setting Input1 |
Manufacturer: JST
Part number: B-8B-PH-SM4 TB
Electrical characteristic
| GND | Board ground | | | 0 | V |
| LED 1/2 output (anode) | Output voltage 2 | | 5 | | V |
| Internal series resistance | 465.3 | 470 | 474.4 | Ohm |
| Forward current IF at ULED = 2V 1 | | 6 | | mA |
| Input 1/2 (internal 10k pull up to 3.3V) | Voltage (open contact) | | | 3.3 | V |
| VIL (low level input voltage) | | | 0.9 | V |
| VIH (high level input voltage) | 2.5 | | 5.5 | V |
| Flash + | Voltage (open contact) | 23 | 24 | 25 | V |
| Flash output capacitance | 528 | 660 | 792 | uF |
| Internal capacitance storage energy | | 0.190 | | Ws |
| Flash capacitance charge current / output DC current | | 20 | | mA |
| Flash 2 | IOUT | | | -2 | A |
| On voltage at IOUTMAX | | | 0.15 | V |
| Off voltage | 23 | 24 | 25 | V |
1 Depends on mvBlueFOX-M power supply
2 Attention: No over-current protection!
Figure 19: CON3 schematic
Single-board version (BVS CA-MLC)
Typical Power consumption @ 5V
| -200w | 1.09 | W |
| -202a | 1.39 | W |
| -202b | 1.58 | W |
| -202d | 1.28 | W |
| -202v | 1.35 | W |
| -205 | 1.37 | W |
Dimensions and connectors
Figure 20: BVS CA-MLC-xxxxxx-1600OX-001 - Note
- The BVS CA-MLC has a serial I²C bus EEPROM with 16 KByte of which 8 KByte are reserved for the firmware and 8 KByte can be used to store custom arbitrary data.
- See also
- UserDataEntry class description
Sensor's optical midpoint and orientation
The sensor's optical midpoint is in the center of the board (Figure 21: intersection point of the holes diagonals). The (0,0) coordinate of the sensor is located at the one bottom left corner of the sensor (please notice that Mini-B USB connector is located at the bottom at the back).
- Note
- Using a lens, the (0,0) coordinate will be mirrored and will be shown at the top left corner of the screen as usual!
Figure 21: Sensor's optical midpoint and orientation
Mini-B USB (USB 2.0)
Figure 22: Mini-B USB
| 1 | USBPOWER_IN | Supply voltage |
| 2 | USB_DATA- | Data |
| 3 | USB_DATA+ | Data |
| 4 | ID | Not connected |
| 5 | GND | Ground |
12-pin Wire-to-Board header (USB 2.0 / Dig I/O)
- Note
- If you have the BVS CA-MLC variant which uses the standard Mini-B USB connector, pin 2 and 3 (USB_DATA+ / USB_DATA-) of the header won't be connected!
| 1 | GND | Ground | GND | Ground | GND | |
| 2 | USB_DATA+ | Data | USB_DATA+ | Data | USB_DATA+ | |
| 3 | USB_DATA- | Data | USB_DATA- | Data | USB_DATA- | |
| 4 | USBPOWER_IN | Supply voltage | USBPOWER_IN | Supply voltage | USBPOWER_IN | |
| 5 | I2C SDA | Serial data line (the I2C interface is master-only, which means that I2C slaves can only be connected externally) | I2C SDA | Serial data line | | |
| 6 | I2C SCL | Serial clock line (the I2C interface is master-only, which means that I2C slaves can only be connected externally) | I2C SCL | Serial clock line | | |
| 7 | USBPOWER_IN | Supply voltage | USBPOWER_IN | Supply voltage | red | |
| 8 | GND | Ground | GND | Ground | black | black |
| 9 | OUT0- | Opto-isolated digital output 0 (Negative voltage) | OUT1 | TTL compliant digital output 1 | blue | blue |
| 10 | OUT0+ | Opto-isolated digital output 0 (Positive voltage) | OUT0 | TTL compliant digital output 0 | violet | violet |
| 11 | IN0- | Opto-isolated digital input 0 (Negative voltage) | IN1 | TTL compliant digital input 1 | gray | gray |
| 12 | IN0+ | Opto-isolated digital input 0 (Positive voltage) | IN0 | TTL compliant digital input 0 | pink | pink |
- Note
- I2C bus uses 3.3 Volts. Signals have a 2kOhm pull-up resistor. Access to the I2C bus from an application is possible for BVS CA-MLC devices using an mvBlueFOX driver with version 1.12.44 or newer.
Manufacturer (suitable board-to-wire connector): Molex
Part number: 0510211200 1.25mm Housing
Link: http://www.molex.com/molex/products/datasheet.jsp?part=active/0510211200_CRIMP_HOUSINGS.xml&channel=Products&Lang=en-US
Manufacturer (multi-pin connector for board-to-board connection): e.g. Garry
Link: http://www.mpe-connector.de/index.php?lang=de&menu=16&mating=1841&id_product=6591 (recommended variant: 659-1-012-O-F-RS0-xxxx; xxxx = length of the pins)
- See also
- Suitable assembled cable accessories for BVS CA-MLC: What's inside and accessories
-
High-Speed USB design guidelines
-
More information about the usage of retrofittable ferrite
Electrical characteristic
Digital inputs TTL
Figure 23: TTL digital inputs block diagram - Note
- If the digital input is not connected, the state of the input will be "1" (as you can see in ImpactControlCenter).
| IIN | ILOW (INx) | | | -0.5 | mA |
| UIN | VIH | 3.6 | | 5.5 | V |
| VIL | -0.3 | | 1.3 | V |
| IIN | ILOW (INx) | | | -0.5 | mA |
| UIN | VIH | 2 | | 3.8 | V |
| VIL | -0.3 | | 0.8 | V |
TTL input low level / high level time: Typ. < 210ns
Digital outputs TTL
Figure 24: TTL digital outputs block diagram
| IOUT | Dig_out power | | | +-32 | mA |
| UOUT | VOH (IOUT=32mA) | 3.8 | | | V |
| VOH | | | 5.25 | |
| VOL (IOUT=32mA) | | | 0.55 | V |
| VOL | 0.1 | | | |
TTL output low level / high level time: Typ. < 40ns
Opto-isolated digital inputs
Figure 25: Opto-isolated digital inputs block diagram with example circuit Delay
The inputs can be connected directly to +3.3 V and 5 V systems. If a higher voltage is used, an external resistor must be placed in series (Figure 25).
| 3.3V .. 5V | none |
| 12V | 680 Ohm |
| 24V | 2 KOhm |
| UIN | VIH | 3 | | 5.5 | V |
| VIL | -5.5 | | 0.8 | V |
Opto-isolated digital outputs
Figure 26: Opto-isolated digital outputs block diagram with example circuit Delay
Figure 27: Output switching times
| Turn-On time | tON | RL = 1.9 kOhm, VCC 5V, IC = 16mA | 2 | us |
| Storage time | tS | 25 |
| Turn-Off time | tOFF | 40 |
| Ion | load current | | | 15 | mA |
| Ioff | leakage current | | | 10 | uA |
| Von Sat. at 2.4 mA | VIH | 0 | (0.2) | 0.4 | V |
| Voff | | | | 30 | V |
LED states
| Camera is not connected or defect | LED off |
| Camera is connected but not initialized or in "Power off" mode. | Orange light on |
| Camera is connected and active | Green light on |
Assembly variants
The BVS CA-MLC is available with following differences:
- Mini-B USB connector and digital I/O pin header
- 1/1 opto-isolated or 2/2 TTL compliant digital I/O
- USB via header without Mini-B USB connector
- female board connector instead of pin header (board-to-board connection)
- 3 different S-mount depths
- C(S)-mount compatibility using mvBlueCOUGAR-X flange
- ambient temperature operation: 5..55 deg C / 30..80 RH
- ambient temperature storage: -25..60 deg C / 20..90 RH
Single-board version with housing (BVS CA-IGC)
Dimensions and connectors
Figure 28: BVS CA-IGC-xxxxxx-16xxxx-001 with CS-mount without adjustable backfocus (standard)
Figure 29: BVS CA-IGC-xxxxxx-19xxxx-001 with C-mount and adjustable backfocus
| X | 8 mm (9.5 mm with max. Ø 20 mm) |
- Note
- The BVS CA-IGC has a serial I²C bus EEPROM with 16 KByte of which 8 KByte are reserved for the firmware and 8 KByte can be used to store custom arbitrary data.
- See also
- UserDataEntry class description
Mini-B USB (USB 2.0)
Figure 30: Mini-B USB
| 1 | USBPOWER_IN | Supply voltage |
| 2 | USB_DATA- | Data |
| 3 | USB_DATA+ | Data |
| 4 | ID | Not connected |
| 5 | GND | Ground |
4-pin circular plug-in connector with lock (I/O)
Figure 31: 4-pin circular plug-in connector (female)
| 1 | IN0 + | Opto-isolated digital input 0 (Positive voltage) | brown |
| 2 | IN0 - | Opto-isolated digital input 0 (Negative voltage) | white |
| 3 | OUT0 + | Opto-isolated digital output 0 (Positive voltage) | blue |
| 4 | OUT0 - | Opto-isolated digital output 0 (Negative voltage) | black |
Manufacturer: Binder
Part number: 79-3107-52-04
Electrical characteristic
Please have a look at the BVS CA-MLC digital I/O characteristics (opto-isolated model) of the 12-pin Wire-to-Board Header (USB / Dig I/O).
LED states
| Camera is not connected or defect | LED off |
| Camera is connected but not initialized or in "Power off" mode. | Orange light on |
| Camera is connected and active | Green light on |
Positioning tolerances of sensor chip
The sensor's optical midpoint is in the center of the housing. However, several positioning tolerances in relation to the housing are possible because of:
- Tolerance of mounting holes of the printed circuit board in relation to the edge of the lens holder housing is not specified but produced according to general tolerance DIN ISO 2768 T1 fine.
- Tolerance of mounting holes on the printed circuit board because of the excess of the holes ± 0.1 mm (Figure 32; 2).
- Tolerance between conductive pattern and mounting holes on the printed circuit board.
Because there is no defined tolerance between conductive pattern and mounting holes, the general defined tolerance of ± 0.1 mm is valid (Figure 32; 1 in the Y-direction ± 0.1 mm; 3 in the Z-direction ± 0.1 mm)
There are further sensor specific tolerances, e.g. for model BVS CA-MLC-0004ZG:
- Tolerance between sensor chip MT9V034 (die) and its package (connection pad)
- Chip position in relation to the mechanical center of the package: 0.2 mm (± 0.1mm) in the X- and Y-direction (dimensions in the sensor data sheet according to ISO 1101)
- Tolerance between copper width of the sensor package and the pad width of the printed circuit board
During the soldering the sensor can swim to the edge of the pad: width of the pad 0.4 mm (possible tolerance is not considered), width of pin at least 0.35 mm, max. offset: ± 0,025mm
Further specific tolerances of other models on request.
Figure 32: Positioning tolerances of sensor chip - Note
- There are also tolerances in lens which could lead to optical offsets.
Summary of components
| Image Memory | | 8 Mpixels |
| ADC resolution | | CMOS: 10 bits (10/8 bit transfer) / CCD: 12 bits (10 bit transfer) |
| Inputs | | 2 | 4 | 1 | 2 | 3 | 1 |
| Type | opto-isolated
5 V (TTL) / 24 V (PLC) switchable via software | LVTTL | opto-isolated | TTL | LVTTL | opto-isolated |
| Outputs | | 2 | 4 | 1 | 2 | - | 2 |
| Type | opto-isolated | LVTTL | opto-isolated | TTL | - | opto-isolated |
| USB 2.0 | | USB-B | 4-pin Wire-to-Board header | Mini-B USB (-xxW-) / 12-pin Wire-to-Board header (-xxB-) / Mini-B USB (-xxA-) | Mini-B USB |
| Optics | | |
| Lens Mount (Focal Distance) | C-mount (17.526 mm in air), CS-mount (12.5 mm in air) | C-mount (17.526 mm in air), CS-mount (12.5 mm in air), optional S-mount | C-mount (17.526 mm in air), CS-mount (12.5 mm in air), optional S-mount | C-mount (17.526 mm in air), CS-mount (12.5 mm in air) |
| Environment | | |
| Ambient Temperature | |
| Operation | 0..45 deg C / 30 to 80% RH |
| Storage | -20..60 deg C / 20 to 90% RH |
| | Protection class 1 | IP40 | | IP40 |
| Weight without lens | | approx. 120 g | approx. 17 g | approx. 10 g | approx. 80 g |
| Power supply (PWR_IN) | | |
| DC | 4.75 to 5.25 V via USB |
| Pmax | 1.5 W |
| Peak current draw | 0.5 A |
1 not evaluated by UL
Summary of available digital I/O's