|
Balluff - BVS CA-MLC / BVS CA-IGC / mvBlueFOX Technical Documentation
|
| We cannot and do not take any responsibility for the damage caused to you or to any other equipment connected to the device. Similarly, warranty will be void, if a damage is caused by not following the manual. |
| Handle the device with care. Do not misuse the device. Avoid shaking, striking, etc. The device could be damaged by faulty handling or shortage. |
| Use a soft cloth lightly moistened with a mild detergent solution when cleaning the camera. |
| Never face the camera towards the sun. Whether the camera is in use or not, never aim at the sun or other extremely bright objects. Otherwise, blooming or smear may be caused. |
| Please keep the camera closed or mount a lens on it to avoid the CCD or the CMOS from getting dusty. |
| Clean the CCD/CMOS faceplate with care. Do not clean the CCD or the CMOS with strong or abrasive detergents. Use lens tissue or a cotton tipped applicator and ethanol. |
| Never connect two USB cables to the device even if one is only connected to a PC. |
| The camera is bus powered < 2.5 W. |
| The device meets IP40 standards. |
| Using the single-board or board-level versions:
|
If you want to make own High-Speed (HS) USB cables, please pay attention to following design guidelines:
| The device complies with the provision of the following European Directives:
|
| Balluff corresponds to the EU guideline WEEE 2002/96/EG on waste electrical and electronic equipment and is registered under WEEE-Reg.-No. DE 25244305. |
| Class B |
This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when the equipment is operated in a residential environment. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. However there is no guarantee that interferences will not occur in a particular installation. If the equipment does cause harmful interference to radio or television reception, the user is encouraged to try to correct the interference by one or more of the following measures:
You are cautioned that any changes or modifications not expressly approved in this manual could void your authority to operate this equipment. The shielded interface cable recommended in this manual must be used with this equipment in order to comply with the limits for a computing device pursuant to Subpart B of Part 15 of FCC Rules.
This apparatus complies with the Class B limits for radio noise emissions set out in the Radio Interference Regulations.
Cet appareil est conforme aux normes classe B pour bruits radioélectriques, spécifiées dans le Règlement sur le brouillage radioélectrique.