|
Impact Acquire SDK GUI Applications
|
As described earlier, each device currently recognized will be listed in the drop down menu in the upper left corner of the "Upper Tool Bar". When this is the first time you start the application after the system has been booted this might take some seconds when working with devices that are not connected to the host system via PCI or PCIe.
Once you have selected the device of your choice from the drop down menu click on the "Use" button to open it.
When the device has been opened successfully, the remaining buttons of the dialog will become enabled!
Now, you can capture an image ("Acquisition Mode": "SingleFrame") or display live images ("Continuous"). Just
Three different acquisition modes are available:
The frame rate depends on
If you want to have a fixed frame rate using the "Continuous" mode, for some "GenICam" compliant devices the property "Setting → Base → Camera → GenICam → Acquisition Control → Acquisition Frame Rate" will be supported
Alternatively, if you need frame rates below 5 fps, you can use Timers.
To save an image directly from the live display directly, just
With "Save Current Image" a dialog will appear, where you can specify the destination folder and the file format.
With "Copy Current Image To Clipboard" you can open your preferred image-editing tool and paste the clipboard into it. For this functionality you can also use the shortcuts CTRL-C and CTRL-V.