Impact Acquire SDK Java
Loading...
Searching...
No Matches
Supported Operating Systems

The tables within this section list all operating systems that are/were supported by Impact Acquire

Windows®

Windows® VersionRelease DateFirst compatible Impact Acquire releaseLast compatible Impact Acquire release
Windows® 11Oct 05 20212.18.0 (Dec 13 2016)
Windows® 10Aug 02 2016 (>= 1607)64-bit2.18.0 (Dec 13 2016)
32-bit2.18.0 (Dec 13 2016)3.5.1 (May 23 2025)
Jul 29 2015 (< 1607)64-bit2.17.0 (Aug 4 2016)
32-bit2.17.0 (Aug 4 2016)3.5.1 (May 23 2025)
Windows® 8.1Oct 17 20131.10.64*, a (Mar 2 2009)3.4.0b (Nov 14 2024)
Windows® 8Oct 26 20121.10.64*, a (Mar 2 2009)3.4.0b (Nov 14 2024)
Windows® 7Oct 22 20091.10.64*, a (Mar 2 20093.4.0b (Nov 14 2024)
Windows® VistaJan 30 200764-bit1.9.3* (May 23 2007)3.4.0b (Nov 14 2024)
32-bit1.8.6* (Mar 14 2007)3.4.0b (Nov 14 2024)
Windows® XPOct 25 200164-bit1.9.3 (May 23 2007)2.26.0 (Apr 12 2018)
32-bit1.0.0 (Somewhere in 2005)2.26.0 (Apr 12 2018)

Linux

In contrast to Windows®, on Linux the compiler used to build the SDK is more important than the actual operating system on which the code is intended to run on later. In addition to that the device driver code usually shipped as part of the installation needs to be compatible with the kernel running on the target system. Therefore the Building And Running Applications Using Impact Acquire (especially for the C/C++ API) as well as the table from the previous chapter are more relevant here.

The following table lists which version of Impact Acquire was built with which version of gcc.

Impact Acquire versiongcc version[glibc version] (Linux x86_64)gcc version[glibc version] (Linux ARMhf)gcc version[glibc version] (Linux ARM64)
< 2.33.04.2.4[2.8]4.6.3[2.14]4.8.3[2.14]
since 2.33.04.8.5[2.14]4.9.4[2.14]
since 2.50.05.5.0[2.21]
Note
x86 and ARMsf were only supported up to and including Impact Acquire 2.37.0 and so used gcc 4.8.5 for x86 and gcc 4.9.4 for ARMsf.

Using compilers older than that or Linux systems with a glibc smaller than that mentioned in the table above or a libstdc++/libgcc older than bundled with the gcc versions mentioned above will most certainly not work and these systems will not be supported anymore. So in case you are bound to an older Linux system you might want to stick with an appropriate Impact Acquire version as indicated in the table above.

Apart from that the amount of Linux Distributions out there makes it practically impossible to test all these systems and assemble a complete list out of these results. Therefore this section will only present a condensed version of the supported target platforms.

Target PlatformFirst compatible Impact Acquire releaseLast compatible Impact Acquire release
ARM642.17.2 (Sep 21 2016)
ARMhf2.11.5 (Nov 24 2014)
ARMsf2.11.5 (Nov 24 2014)2.37.0 (Mar 03 2020)
x86_641.9.9 (Sep 04 2007)
x861.0.0 (Somewhere in 2005)2.37.0 (Mar 03 2020)