Balluff - BVS CA-GX0 / BVS CA-GX2 Technical Documentation
Loading...
Searching...
No Matches
I can see the camera in IPConfigure, but I cannot access the camera

In some cases, it can be possible that you can see the camera in IPConfigure, however,

There could be two reasons for this problem:

  1. The communication is blocked by a firewall.
  2. There are network configuration problems, which means that either the network is incorrectly configured or with regards to the network settings the camera itself.

To solve this issue, please check the firewall settings of your system. In the latter case, please have a look at the following chapters of the manual: