Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
Multi-AOI Wizard

This wizard will allow to set up a device for transferring multiple AOIs from one larger image combined into a single, then smaller frame.

Since
Version 2.19.0 of this application
Note
This wizard addresses Balluff specific features only thus will only be available for certain GenICam™ compliant Balluff devices! Whether or not a device supports all the features required by this wizard determines if it will be available or not. Whether or not a device supports the "mvMultiAreaMode" and other features required is described in the corresponding product manual.

If the currently selected device supports all the required features, the wizard can be selected from the "Wizards" menu or by selecting a feature required by the wizard within the The Property Grid and then pressing the Wizard button in the left toolbar or as described in the very beginning of the Wizards chapter:

ImpactControlCenter - Wizard menu

Once started the wizard will display one page for each AOI currently configured:

ImpactControlCenter - Multi AOI wizard

Either the controls on each page can be used to modify each AOI or the green AOIs can be configure like the Analysis AOIs used for the image analysis plots

The live image in the background shows the created AOIs in green and all the AOIs that must be transmitted as well in red. The red AOIs are needed as a result of how the sensors implement this feature. More information about this can be found in the product manual. The resulting image however always contains ALL areas in either red or green boxes. All the other areas will not be read out of the sensor thus can result in a dramatic reduction in both used bandwidth and sensor read-out time.

ImpactControlCenter - Multi AOI wizard - Live image
See also