|
Impact Acquire SDK Python
|
Triggering images can be realized by using the required device properties. Depending on the device type there might be different settings available which can be configured using an instance of a mvIMPACT.acquire.GenICam.AcquisitionControl object.
As trigger capabilities have a strong relationship to specific hardware it would be a good idea to check the corresponding translation dictionaries of the corresponding properties e.g.:
A sample on how to query a property's translation dictionary can be found here:
All trigger modes are defined by the enumeration
However, not every device will offer all these trigger modes but a subset of them. Valid trigger modes therefore can be found by reading the properties translation dictionary.
A sample on how to query a property's translation dictionary can be found here:
All trigger modes are defined by the enumeration
For more specified information about triggered images with CCD sensors, refer to the "More specific data" link in the sensor tables.