General
The Impact Acquire framework uses a property based concept to access parameters of internal structures or to configure the framework's behaviour. Features offered by the device will simply be added to other properties already present in the drivers feature tree. The following list displays the general layout of features in the GenICam™ interface layout (see GenICam™ vs. DeviceSpecific Interface Layout for details on different interface layouts):
|
|- ImagingSubsystem
| |
| |- Setting
| |
| |- Setting Base
| | |
| | |- Camera
| | |
| | |- GenICam
| | | |
| | | |- ImageFormatControl (see SFNC)
| | | |- AcquisitionAndTriggerControl (see SFNC)
| | | |- etc.
| | |
| | |- GenTL
| | |
| | |- Device
| | |- DataStream
| | |- etc.
|
|- System
| |
| |- CodeGeneration
| |- etc.
|
|- Info
|
|
other features
Runtime Feature Extraction
If an application shall be capable of dealing with every feature of every device and not all these devices are known at compile time, a code generator can not be used as it can only create code for devices which are accessible when creating the code. In this case, features must be extracted dynamically from the drivers feature tree. To do this SDK offers a set of functions that can be used to search and use features or to iterate over a tree of features. These objects and functions will be explained in the following sections.
- Note
- The GUI tool ImpactControlCenter can be of great help when writing code that shall extract certain features from the driver for using them inside an application. To find out how refer to the chapter "Changing the view of the property grid to assist writing code that shall locate driver features" in the technical manual of the device.
-
Most of the code presented in this section is also part of the SDK even though it is not part of the actual Impact Acquire driver framework. It has been added as a set of helper functions in a separate source file to the example applications. The source code can be found in the installation folder under apps/Common/exampleHelper_C*. An application can either add the full source file to its Makefile or extract and re-use source code as needed from here. All the example applications written in C do this as well.