To bind an object handle (::HOBJ) to a certain feature offered by the device at runtime the C interface offers several functions that can be used to do that. Let's assume an application wants to access a 64 bit integer property that is called Width and is located somewhere in the devices feature tree. In this case, we want to bind the property of the base setting. The code to bind the device feature to a C interface object would look more or less like this:
HOBJ getDriverProperty( HDRV hDrv,
const char* pName,
const char* pAddListName,
TDMR_ListType type )
{
{
{
printf( "OBJ_GetHandleEx for '%s' failed: %d Handle: %d. This property might not be supported by this device\n", pName, objResult, hObj );
}
}
else
{
printf( "DMR_FindList failed: %d. Lists of type %d are not available for this device\n", dmrResult, type );
}
return hObj;
}
HOBJ getSettingProp( HDRV hDrv, const char* pSettingName, const char* pPropName )
{
return getDriverProperty( hDrv, pPropName, pSettingName,
dmltSetting );
}
void myFun()
{
HDRV hDrv = getTheDriverHandleFromSomewhere();
HOBJ hProp = getSettingProp( hDrv, "Base", "Width" );
int64_t maxVal = 0;
{
}
else
{
}
}
TDMR_ERROR
Errors reported by the device manager.
Definition mvDriverBaseEnums.h:2779
TDMR_ListType
Defines valid interface list types, which can be located using the function DMR_FindList().
Definition mvDeviceManager.h:586
@ DMR_NO_ERROR
The function call was executed successfully.
Definition mvDriverBaseEnums.h:2781
@ dmltSetting
Specifies a certain setting.
Definition mvDeviceManager.h:593
MVDMR_API TDMR_ERROR DMR_CALL DMR_FindList(HDRV hDrv, const char *pName, TDMR_ListType type, unsigned int flags, HLIST *phDevList)
Locates a specified list within the device drivers interface.
Definition mvDeviceManager.cpp:2578
const unsigned int smIgnoreLists
When set lists are not taken into account during a search.
Definition mvPropHandlingDatatypes.h:94
const int INVALID_ID
A constant to check for an invalid ID returned from the property handling module.
Definition mvPropHandlingDatatypes.h:63
MVDMR_API TPROPHANDLING_ERROR DMR_CALL OBJ_SetI64(HOBJ hProp, int64_t val, int index)
Sets a property's value as a 64 bit integer value.
Definition ObjectHandling.cpp:2746
MVDMR_API TPROPHANDLING_ERROR DMR_CALL OBJ_GetHandleEx(HLIST hList, const char *pObjName, HOBJ *phObj, unsigned int searchMode, int maxSearchDepth)
Retrieves an objects handle.
Definition ObjectHandling.cpp:354
TPROPHANDLING_ERROR
Error codes of the module handling everything related to properties.
Definition mvPropHandlingDatatypes.h:383
MVDMR_API TPROPHANDLING_ERROR DMR_CALL OBJ_GetI64(HOBJ hProp, int64_t *pVal, int index)
Receives a property's value as an integer value.
Definition ObjectHandling.cpp:2821
const unsigned int smIgnoreMethods
When set method objects are not taken into account during a search.
Definition mvPropHandlingDatatypes.h:100
@ PROPHANDLING_NO_ERROR
The operation has been executed successfully.
Definition mvPropHandlingDatatypes.h:385