It's also possible to iterate over all the features offered by a device or a subtree of this. To see how this is done, refer to the description of the function OBJ_GetFirstSibling().
HOBJ getDriverList( HDRV hDrv,
const char* pName,
const char* pAddListName,
TDMR_ListType type )
{
HLIST baseList;
{
{
printf( "OBJ_GetHandle for %s failed: %d Handle: %d. This list might not be supported by this device\n", pName, objResult, hObj );
}
}
else
{
printf( "DMR_FindList failed: %d. Lists of type %d are not available for this device\n", dmrResult, type );
}
return hObj;
}
HOBJ getInfoProp( HDRV hDrv, const char* pSettingName, const char* pPropName )
{
return getDriverProperty( hDrv, pPropName, pSettingName,
dmltInfo );
}
void myFun()
{
HDRV hDrv = getTheDriverHandleFromSomewhere();
HOBJ hProp = getInfoProp( hDrv, "DeviceInformation", "DeviceVersion" );
{
}
else
{
}
}
TDMR_ERROR
Errors reported by the device manager.
Definition mvDriverBaseEnums.h:2779
TDMR_ListType
Defines valid interface list types, which can be located using the function DMR_FindList().
Definition mvDeviceManager.h:586
@ DMR_NO_ERROR
The function call was executed successfully.
Definition mvDriverBaseEnums.h:2781
@ dmltInfo
Specifies the driver interfaces list containing general information.
Definition mvDeviceManager.h:606
MVDMR_API TDMR_ERROR DMR_CALL DMR_FindList(HDRV hDrv, const char *pName, TDMR_ListType type, unsigned int flags, HLIST *phDevList)
Locates a specified list within the device drivers interface.
Definition mvDeviceManager.cpp:2578
const int INVALID_ID
A constant to check for an invalid ID returned from the property handling module.
Definition mvPropHandlingDatatypes.h:63
MVDMR_API TPROPHANDLING_ERROR DMR_CALL OBJ_GetHandleEx(HLIST hList, const char *pObjName, HOBJ *phObj, unsigned int searchMode, int maxSearchDepth)
Retrieves an objects handle.
Definition ObjectHandling.cpp:354
TPROPHANDLING_ERROR
Error codes of the module handling everything related to properties.
Definition mvPropHandlingDatatypes.h:383
const unsigned int smIgnoreProperties
When set property objects are not taken into account during a search.
Definition mvPropHandlingDatatypes.h:106
const unsigned int smIgnoreMethods
When set method objects are not taken into account during a search.
Definition mvPropHandlingDatatypes.h:100
@ PROPHANDLING_NO_ERROR
The operation has been executed successfully.
Definition mvPropHandlingDatatypes.h:385