Balluff - BVS CA-GX0 / BVS CA-GX2 Technical Documentation
Loading...
Searching...
No Matches
Introduction
Figure 1: BVS CA-GX0 / BVS CA-GX2

BVS CA-GX devices belong to an extreme compact and flexible industrial Gigabit Ethernet camera family compliant to GigE Vision and GenICam. The BVS CA-GX devices offer

  • a wide range of sensors,
  • high frame rates over long distances using inexpensive standard network parts,
  • I/Os suitable for industrial applications, and
  • wide range of resolutions.

The image memory of the camera enables a high-speed-buffer mode (a.k.a. burst mode) which writes images faster in the camera's memory as they are transferred. With this mode, image losses are a thing of the past.

BVS CA-GX devices are ideally suited for all classical areas of machine vision and allows an easy integration in the environment and support the application with helpful features to deliver faster and better results. The hardware capabilities can be teamed with machine vision libraries which are compliant to GigE Vision.

A Dual-GigE version named BVS CA-GX2 is also available.

Software concept

The BVS CA-GX devices are a GigE Vision compliant device, using a GenICam XML-file describing the device capabilities. Within this XML-file it uses the names, units, data types etc. recommended by the SFNC to describe the devices features. Whenever custom features have been added to the BVS CA-GX firmware these can clearly be spotted by the leading 'mv' in the features name. The device can communicate with every third party compliant GigE Vision capture driver that can interpret GenICam XML-files.

The following figure shows the software concept of GenICam™ GenTL compliant devices built by Balluff/MATRIX VISION:

Figure 2: Software concept

As shown in figure 2, for the BVS CA-GX devices the Impact Acquire interface is stacked on the GigE Vision and Genicam layers. The Impact Acquire interface internally uses the GenICam runtime libraries, so that it can be considered as a user application written with the GenICam interface.

Order code nomenclature

BVS CA-GX0 / BVS CA-GX1

The BVS CA-GX0 / BVS CA-GX1 nomenclature scheme is as follows.

Note
The BVS CA-GX1 differs from the BVS CA-GX0 in that it has an increased image memory of 128 MB and a larger FPGA.
SensorModel nameMATRIX VISION model name
0.3 Mpix, 656 x 520, 1/4'', IMX991, CMOS BVS CA-GX0-0003SG mvBlueCOUGAR-X100sG
0.4 Mpix, 728 x 544, 1/2.9'', IMX287, CMOS BVS CA-GX0-0004FG/C mvBlueCOUGAR-X100fG/C
0.4 Mpix, 752 x 480, 1/3'', MT9V034, CMOS BVS CA-GX0-0004ZG/C mvBlueCOUGAR-X100wG/C
1.2 Mpix, 1280 x 960, 1/3'', MT9M021, CMOS BVS CA-GX0-0012BG/C mvBlueCOUGAR-X102bG/C
1.2 Mpix, 1280 x 960, 1/3'', MT9M034, CMOS BVS CA-GX0-0012DG/C mvBlueCOUGAR-X102dG/C
1.3 Mpix, 1296 x 1032, 1/2'', IMX990, CMOS BVS CA-GX0-0013SG mvBlueCOUGAR-X101sG
1.3 Mpix, 1280 x 1024, 1/1.8'', EV76C560, CMOS BVS CA-GX0-0013ZG/C mvBlueCOUGAR-X102eG/C
1.6 Mpix, 1456 x 1088, 1/2.9'', IMX273, CMOS BVS CA-GX0-0016ZG/C mvBlueCOUGAR-X102fG/C
1.7 Mpix, 1600 x 1104, 1.1'', IMX425, CMOS BVS CA-GX0-0017ZG/C mvBlueCOUGAR-X102mG/C
1.7 Mpix, 1600 x 1104, 1.1'', IMX432, CMOS BVS CA-GX0-0017BG/C mvBlueCOUGAR-X102kG/C
2.0 Mpix, 1632 x 1248, 1/1.2'', IMX430, CMOS BVS CA-GX0-0020DG/C mvBlueCOUGAR-X102nG/C
1.9 Mpix, 1600 x 1200, 1/1.8'', EV76C570, CMOS BVS CA-GX0-0020ZG/C mvBlueCOUGAR-X104eG/C
2.4 Mpix, 1936 x 1216, 1/1.2'', IMX249, CMOS BVS CA-GX0-0024AG/C mvBlueCOUGAR-X104fG/C
2.4 Mpix, 1936 x 1216, 1/2.3'', IMX392, CMOS BVS CA-GX0-0024BG/C mvBlueCOUGAR-X103G/C
3.2 Mpix, 2064 x 1544, 1/1.8'', IMX265, CMOS BVS CA-GX0-0032AG/C mvBlueCOUGAR-X104iG/C
3.2 Mpix, 2064 x 1552, 1/3.1'', IMX900, CMOS BVS CA-GX0-0032BG/C mvBlueCOUGAR-X104kG/C
3.2 Mpix, 2080 x 1544, 1/1.8'', IMX993, CMOS BVS CA-GX1-0032SG mvBlueCOUGAR-X103sG
4.2 Mpix, 2048 x 2048, 1'', CMV4000, CMOS BVS CA-GX0-0042ZG/C mvBlueCOUGAR-X104bG/C
5.0 Mpix, 2592 x 1944, 1/2.5'', MT9P031, CMOS BVS CA-GX0-0050ZG/C mvBlueCOUGAR-X105G/C
5.1 Mpix, 2464 x 2056, 2/3'', IMX264, CMOS BVS CA-GX0-0051AG/C mvBlueCOUGAR-X105bG/C
5.1 Mpix, 2472 x 2064, 1/1.8'', IMX547, CMOS BVS CA-GX0-0051DG/C mvBlueCOUGAR-X105dG/C
5.1 Mpix, 2464 x 2056, 2/3'', IMX250_POL, CMOS BVS CA-GX0-0051PG/C mvBlueCOUGAR-X105pG/C
5.3 Mpix, 2592 x 2056, 1/1.4'', IMX992, CMOS BVS CA-GX1-0053SG mvBlueCOUGAR-X105sG
6.4 Mpix, 3096 x 2080, 1/1.8'', IMX178, CMOS BVS CA-GX0-0064ZG/C mvBlueCOUGAR-X106G/C
7.1 Mpix, 3216 x 2208, 1.1'', IMX428, CMOS BVS CA-GX0-0071AG/C mvBlueCOUGAR-X107bG/C
8.1 Mpix, 2856 x 2848, 2/3'', IMX546, CMOS BVS CA-GX0-0081AG/C mvBlueCOUGAR-X108aG/C
8.1 Mpix, 2848 x 2848, 2/3'', IMX487, CMOS BVS CA-GX0-0081UG/C mvBlueCOUGAR-X108uG/C
8.9 Mpix, 4112 x 2176, 1'', IMX267, CMOS BVS CA-GX0-0089AG/C mvBlueCOUGAR-X109bG/C
10.7 Mpix, 3856 x 2764, 1/2.35'', MT9J003, CMOS BVS CA-GX0-0107ZG/C mvBlueCOUGAR-X1010G/C
12.4 Mpix, 4112 x 3008, 1.1'', IMX304, CMOS BVS CA-GX0-0124AG/C mvBlueCOUGAR-X1012bG/C
12.4 Mpix, 4128 x 3008, 1/1.1'', IMX545, CMOS BVS CA-GX0-0124DG/C mvBlueCOUGAR-X1012dG/C
12.4 Mpix, 4072 x 3044, 1/1.7'', IMX226, CMOS BVS CA-GX0-0124RG/C mvBlueCOUGAR-X1012rG/C
16.2 Mpix, 5328 x 3040, 1.1'', IMX542, CMOS BVS CA-GX1-0162AG/C
20.5 Mpix, 5544 x 3692, 1.1'', IMX183, CMOS BVS CA-GX0-0205ZG/C mvBlueCOUGAR-X1020G/C
SeriesSensorColorOptionsHW VariantCUP/STD
TypecodeBVS CA-GX0-xxxxxG/C -see legend below-see legend below
MATRIX VISION typecodemvBlueCOUGAR-XxxxG/C/GE-see legend below-see legend below-see legend below
LegendModel nameMATRIX VISION model name
Options POE: Power over Ethernet, PoE class 2
PLC: Inputs for PLC levels only
POE-I: Power over Ethernet, PoE class 2 with a modular M12 industrial connector concept
POE-IP67: Power over Ethernet, PoE class 2 with a modular M12 industrial connector concept and IP67 protection class
POE-IP67C: Compact IP67 version
HW Variant(1)(2)(3)(4)(5)(6)

(1): Handling
1: Standard handling
2: Extended temperature range test

(2): Lensholder
0: None
1: C-mount Type 2 with high durability and factory-set backfocus
2: C-mount Type 1 with adjustable backfocus (standard)
4: CS-mount Type 1 with adjustable backfocus
5: C-Mount Type3, low cost, factory-set backfocus, D23.2mm Filter
A: C-Mount Type 2 + center position adjustable

(3): Filter
0: None
1: IR-CUT (standard)
2: Glass
3: Daylight cut (only without backfocus adjustment)

More filters on request

(4): Housing
0: None
1: Color black (standard)
4: IP67 enclosure for POE-I + lens, black anodized aluminium
6: IP67 enclosure for POE-I + lens, stainless steel
C: IP67 grade housing, black (available for POE-I)

(5): I/O
2: Default I/Os (standard)
3: Power over Ethernet and isolated inputs / outputs
4: Power over Ethernet with M12 industrial grade I/O connectors
6: PLC logic level digital inputs

(6): Software Adjustments
0: None
(1)(2)(3)(4)

(1): Lensholder
9: None
6: C-mount Type 2 with high durability and factory-set backfocus
1: C-mount Type 1 with adjustable backfocus (standard)
2: CS-mount Type 1 with adjustable backfocus
5: C-Mount Type3, low cost, factory-set backfocus, D23.2mm Filter
A: C-Mount Type 2 + center position adjustable

(2): Filter
1: IR-CUT (standard)
2: Glass
3: Daylight cut (only without backfocus adjustment)
9: None

More filters on request

(3): Housing
1: Color black (standard)
4: IP67 enclosure for POE-I + lens, black anodized aluminium
6: IP67 enclosure for POE-I + lens, stainless steel
9: None
C: IP67 grade housing, black (available for POE-I)

(4): I/O
1: Default I/Os (standard)
CUP/STD001 ET: With extended temperature behavior

BVS CA-GX2

The BVS CA-GX2 nomenclature scheme is as follows:

SensorModel nameMATRIX VISION model name
1.6 Mpix, 1456 x 1088, 1/2.9'', IMX273, CMOS BVS CA-GX2-0016ZG/C mvBlueCOUGAR-XD102fG/C
2.2 Mpix, 2048 x 1088, 2/3'', CMV2000, CMOS BVS CA-GX2-0022ZG/C mvBlueCOUGAR-XD204G/C
2.4 Mpix, 1936 x 1214, 1/1.2'', IMX174, CMOS BVS CA-GX2-0024ZG/C mvBlueCOUGAR-XD104dG/C
3.2 Mpix, 2064 x 1544, 1/1.8'', IMX252, CMOS BVS CA-GX2-0032ZG/C mvBlueCOUGAR-XD104hG/C
4.2 Mpix, 2048 x 2048, 1'', CMV4000, CMOS BVS CA-GX2-0042ZG/C mvBlueCOUGAR-XD204bG/C
5.1 Mpix, 2472 x 2064, 1/1.8'', IMX547, CMOS BVS CA-GX2-0051DG/C mvBlueCOUGAR-XD105dG/C
5.1 Mpix, 2464 x 2056, 2/3'', IMX250, CMOS BVS CA-GX2-0051ZG/C mvBlueCOUGAR-XD105aG/C
7.1 Mpix, 3216 x 2208, 1.1'', IMX420, CMOS BVS CA-GX2-0071ZG/C mvBlueCOUGAR-XD107G/C
7.1 Mpix, 3216 x 2208, 1.1'', IMX428, CMOS BVS CA-GX2-0071AG/C mvBlueCOUGAR-XD107bG/C
8.1 Mpix, 2856 x 2848, 2/3'', IMX546, CMOS BVS CA-GX2-0081AG/C mvBlueCOUGAR-XD108aG/C
8.9 Mpix, 4112 x 2176, 1'', IMX267, CMOS BVS CA-GX2-0089AG/C mvBlueCOUGAR-XD109bG/C
12.4 Mpix, 4112 x 3008, 1.1'', IMX304, CMOS BVS CA-GX2-0124AG/C mvBlueCOUGAR-XD1012bG/C
12.4 Mpix, 4128 x 3008, 1/1.1'', IMX545, CMOS BVS CA-GX2-0124DG/C mvBlueCOUGAR-XD1012dG/C
16.2 Mpix, 5328 x 3040, 1.1'', IMX542, CMOS BVS CA-GX2-0162AG/C mvBlueCOUGAR-XD1016G/C
20.4 Mpix, 4512 x 4512, 1.1'', IMX541, CMOS BVS CA-GX2-0204AG/C mvBlueCOUGAR-XD1020aG/C
24.6 Mpix, 5328 x 4608, 1.2'', IMX540, CMOS BVS CA-GX2-0246AG/C mvBlueCOUGAR-XD1025G/C
31.5 Mpix, 6480 x 4856, APS-C'', IMX342 CMOS BVS CA-GX2-0315ZG/C mvBlueCOUGAR-XD1031G/C
SeriesSensorColorOptionsHW VariantCUP/STD
TypecodeBVS CA-GX2-xxxxxG/C -see legend below-see legend below
MATRIX VISION typecodemvBlueCOUGAR-XDxxxG/C -see legend below-see legend below-see legend below
LegendModel nameMATRIX VISION model name
HW Variant(1)(2)(3)(4)(5)(6)

(1): Handling
1: Standard handling

(2): Lensholder
0: None
1: C-Mount, Type2, with high durability and factory-set backfocus, fixed square filter
2: C-Mount, Type1, with adjustable backfocus, round filter with screw ring, Ø23.2 mm
4: CS-mount Type1, with adjustable backfocus, round filter glued, Ø20 mm
A: C-mount Type 2 + center position adjustable
B: C-Mount Type 2 + D23.2mm Filter with screwring
N: M42x1 10mm no filter
P: M42x1 12mm focal distance with filter
Q: M42 to F-Mount adapter 46mm focal distance with filter
T: Lensholder with TFL-Mount or Adapter for M42 to TFL-Mount

(3): Filter
0: None
1: IR-CUT (standard)
2: Glass
3: Daylight cut (only without backfocus adjustment)

More filters on request

(4): Housing
0: None
1: Color black (standard)

(5): I/O
1: Default I/Os (standard)

(6): Software Adjustments
0: None
(1)(2)(3)(4)

(1): Lensholder
9: None
6: C-Mount, Type2, with high durability and factory-set backfocus, fixed square filter
1: C-Mount, Type1, with adjustable backfocus, round filter with screw ring, Ø23.2 mm
2: CS-mount Type1, with adjustable backfocus, round filter glued, Ø20 mm
A: C-mount Type 2 + center position adjustable
B: C-Mount Type 2 + D23.2mm Filter with screwring
N: M42x1 10mm no filter
P: M42x1 12mm focal distance with filter
Q: M42 to F-Mount adapter 46mm focal distance with filter
T: Lensholder with TFL-Mount or Adapter for M42 to TFL-Mount

(2): Filter
1: IR-CUT (standard)
2: Glass
3: Daylight cut (only without backfocus adjustment)
9: None

More filters on request

(3): Case
1: Color black (standard)
9: None

(4): Misc
1: Default I/Os (standard)
CUP/STD001 ET: With extended temperature behavior

Ordering code samples

Model nameMATRIX VISION model nameDescription
BVS CA-GX0-0020DC-111120mvBlueCOUGAR-X102nC11632 x 1248, CMOS 1/1.7", color, Gigabit Ethernet, IR-CUT filter, C-mount, etc.
BVS CA-GX0-0032AG-112130mvBlueCOUGAR-X104iG-POE-12112064 x 1544, CMOS 1/1.8", gray scale, Gigabit Ethernet with Power over Ethernet, C-mount, glass filter, etc.
BVS CA-GX2-0081AC-143120mvBlueCOUGAR-XD108aC-21112856 x 2848, CMOS 2/3", color, Dual-Gigabit Ethernet, CS-mount, IR-CUT filter, etc.

1: -1111 is the standard delivery variant and for this reason it is not mentioned.

What's inside and accessories

Due to the varying fields of application the BVS CA-GX devices are shipped without accessories. The package contents:

  • BVS CA-GX

For the first use of BVS CA-GX devices we recommend the following accessories to get the camera up and running:

  • network cable and
  • power supply via
    • MV-DC1201 BCX.
Note
To be able use the BVS CA-GX2 device it is required that the GigE ports (the two GigE interfaces at the host; either PC or a switch) support the LAG (Link Aggregation Group) functionality. Windows® 7 and newer and Linux support this functionality by default. Although the BVS CA-GX2 is connected via two cables it will act like a single device.

Accessories for the BVS CA-GX devices

Recommended accessories for the BVS CA-GX can be found on the product pages: