|
Balluff - mvVirtualDevice Technical Documentation
|
The mvVirtualDevice device package can be used to evaluate Impact Acquire functions and even implement the hardware specific part without having the Balluff imaging hardware installed yet.
For this reason the following components are recommended:
| Component | Recommendation |
| Processor | Preferably multi core Intel or ARM CPUs |
| RAM | 4 GB in 32-bit OS; 8 GB in 64-bit OS |
| Mainboard | USB connectors |
The following versions of Windows® are supported officially:
Other Windows® versions might work as well but will not be tested on a regular basis. A complete list of supported Windows® versions can be found here.
The latest version for the required target platform of the Impact Acquire framework can always be found here.
Currently supported Kernel versions are:
The latest version for the required target platform of the Impact Acquire framework can always be found here.
Currently, macOS version 12 (Monterey) is supported.