Balluff - BVS CA-UB Technical Documentation
Toggle main menu visibility
Loading...
Searching...
No Matches
Saving data on the device
Note
As described in
"Storing, Restoring And Managing Settings"
in the
"Impact Acquire SDK GUI Applications"
manual, it is also possible to save the settings as an XML file on the host system. Further information about this can be found in the Impact Acquire SDK manuals and the according setting classes:
https://assets.balluff.com/documents/DRF_957352_AA_000/classmvIMPACT_1_1acquire_1_1FunctionInterface.html
(C++)
There are several use cases concerning device memory:
Creating user data entries
Use Cases
Generated on
3.8.0