Balluff - BVS CA-UB Technical Documentation
Using BVS CA-MLC with motorized lenses (MotorFocusControl)

Introduction

It is possible to use the BVS CA-MLC with a motorized lens mount without optical filter. To control this lens mount you use either ImpactControlCenter or the class MotorFocusControl from Impact Acquire for your own applications.

This camera option consists of a single-board camera module plus additional interface board. The camera is equipped with a board-to-wire connector on the interface board for opto-coupled I/O connection and a Mini USB. Other versions with TTL coupled inputs and outputs and without Mini USB connector are available on demand. There is no optical filter in the light path. For color applications Balluff supplies S-mount lenses with IR absorbing coating.

Important technical data of the motorized lens mount: (Consult Balluff for more detailed data, application notes and the full lens command reference manual)

Lens Type (Lens not included), accepts M12x0.5mm, smaller lenses to M8x0.35 with adapter from your lens supplier
Lens Weight* < 5 grams
Travel Range Up to 1.5 mm
Housing Dimension 20 x 22 x 16 mm
Max Image Sensor Area (image sensor not included) 17 x 17 x 1.25 mm (including 1/2" and 1/1.8" formats)
Speed > 5 mm/s
Resolution 0.5 um
Hysteresis None
Repeatability Uni-directional +/- 5 um
Bi-directional +/- 20 um
Linear Accuracy +/- 30 um
Angular alignment (Static tip/tilt) > +/- 1 degree
Angular movement (Dynamic tip/tilt) > +/- 0.15 degree
Static Concentricity > +/- 0.25 mm
Dynamic Concentricity > +/- 0.02 mm
Input Voltage 3.1 to 3.6 Volts
Input Power** < 0.5 Watts (5mm/s with 5g mass)
< 0.13 Watts quiescent
Temperature / RH*** 5 ° to 70 °C (lower possible) < 95% RH non-condensing
Mean Time Before Failure > 2M Cycles (fixed orientation)
500K Cycles (random orientation)
Weight of module (without lens) 5.8 grams
Compliance CE / RoHS

* Fixed orientation will allow for heavier lens operation. Consult Balluff if your lens does not fit or cannot be focused. ** Power depends on input voltage, speed & load. *** Consult Balluff if you have lower temperature requirements.

Note
By default, the motorized lens mount is shipped in "closed loop mode". This means that the motor will move to and keep its absolute position in a permanent loop. Therefore you will hear a high frequent sound if you touch the lens or if you adjust the focus manually while the module is operating. For this reason, we recommend to use the "open loop mode" while adjusting the lens.
In fixed focus applications you might also consider switching to open loop mode. This will also extend the life time of the motor and reduce operation noise. Please note that the lens will remain at its position also in open loop mode due to mechanical friction.
The open loop mode can be set via MotorFocusSendBuffer (value: "<20 0>") and then call MotorFocusSend either in ImpactControlCenter or by programming.

Controlling motorized lens mount with ImpactControlCenter

Figure 1 shows a live snap of a scene with different focus planes.

Figure 1: ImpactControlCenter - Preview with blurred background and focused label

To control the motorized lens mount via ImpactControlCenter you have to change the "UserExperience" either to "Expert" or "Guru". Afterwards, there is a special section in "Digital I/O" called "MotorFocusControl" in the "Device Properties" tab:

Figure 2: ImpactControlCenter - MotorFocusControl in section Digital I/O

This is a wrapper of the MotorFocusControl class which makes the following methods and properties available in the GUI:

  • Properties:
    • MotorFocusAbsolutePositionCurrent: An integer property (read-only) storing the current absolute position (in encoder counts).
    • MotorFocusAbsolutePositionDesired: An integer property storing an absolute position (in encoder counts) that will be used by subsequent calls to the MotorFocusMoveToAbsolutePositionDesired command.
    • MotorFocusIncrement: An integer property storing an increment (in encoder counts) that will be used by subsequent calls to MotorFocusNear and MotorFocusFar commands.
    • MotorFocusReceiveBuffer: A string property (read-only) that will contain answers sent by the motor focus controller.
    • MotorFocusSendBuffer: A string property storing a command to be sent to the motor focus.
  • Methods:
    • MotorFocusFar: Calling this function will cause the motor focus to move backward by MotorFocusIncrement encoder units.
    • MotorFocusMoveToAbsolutePositionDesired: Calling this function will cause the motor focus to move to the position defined by the value of MotorFocusAbsolutePositionDesired.
    • MotorFocusNear: Calling this function will cause the motor focus to move forward by MotorFocusIncrement encoder units.
    • MotorFocusSend: Calling this function will send the value of MotorFocusSendBuffer to the hardware.

By clicking on the icon with the three dots (e.g. "MotorFocusNear()" in Figure 2), this method will be called using the set properties (e.g. "100" as "MotorFocusIncrement" value as shown in Figure 2).

The following explains the typical adjustment procedure:

  1. Move the lens mount to the farthest position by applying MotorFocusFar command as often as needed.
  2. Switch off closed loop mode by using the command described above.
  3. Screw in lens and focus at infinity.
  4. Move to the nearest position and check MOD.
  5. Move to your working distance.

If your application does not require focusing at infinity you might set the lens mount to the middle position (1500 steps) and focus the lens for your working distance. This gives you equal focusing headroom in both directions. In this case please check that for MotorFocusNear the lens does not block the movement until Zero is reached.

Programming the motorized lens mount

If you want to program own application using the motorized lens mount, the Impact Acquire API offers the class MotorFocusControl which is described in MotorFocusControl class reference in the manual for the corresponding programming language at the manuals section.

Note
The following code snippets are C# pseudo code.

To use the MotorFocusControl class, you have to create an instance of the class:

// Initializing the device DeviceManager deviceManager = new DeviceManager(); Device device = deviceManager.getDeviceByFamily("mvBlueFOX"); MotorFocusControl motorFocusControl = new MotorFocusControl(ref device);
Note
You can check, if the camera has a motorized lens mount at all via "motorFocusControl.motorFocusIncrement.valid == false".

Afterwards, you can

  • "write()" (integer) / "writeS()" (string) and
  • "read()" (integer) / "readS()" (string) the properties or
  • "call()" the methods like
// setting the increment value to 100 motorFocusControl.motorFocusIncrement.write(100);

or

// moving the motor focus backwards by motorFocusIncrement int status = motorFocusControl.motorFocusFar.call(); //getting the current position of the motor int position = motorFocusControl.motorFocusAbsolutePositionCurrent.read();
Note
The call functions can be back while the motor is still moving. For this reason, it is necessary to create a method which will check if the motor still moves.

To get information from the motor you can use "motorFocusSend". The following example shows how you can get status and position of the motor. Furthermore, it shows how you can check, if the motor is still running:

... int motorRunning = 0x4; motorFocusControl.motorFocusSendBuffer.writeS("<10>"); motorFocusControl.motorFocusSend.call(); String s = motorFocusControl.motorFocusReceiveBuffer.readS(); if(s.Length != 29) return false; // string is in hex int status = Convert.ToInt32(s.Substring(4, 6), 16); String positionStr = s.Substring(11, 8); // the position as integer int pos = Convert.ToInt32(positionStr, 16); return (status & motorRunning) == motorRunning; ...

Sending the command "<10>" will return the status and position with following format:

<10 SSSSSS PPPPPPPP EEEEEEEE>
  • SSSSSS is the motor status (6-digit hex format, 24 bit unsigned integer),
  • PPPPPPPP is the absolute position in encoder counts (8-digit hex format, 32-bit signed integer) and
  • EEEEEEEE is the position error in encoder counts (8-digit hex format, 32-bit signed integer)

"Motor status values"

Bit Description Values
0 Reserved N/A
1 Motor direction 0 = Reverse
1 = Forward
2 Running 1 = Motor is running
3 Motor interlock 1 = Motor is disconnected
4 Numbered burst mode 1 = Fixed number of bursts in progress
5 Timed run 1 = Timed free run in progress
6 Multiplexed axis 1 = Multiplexed axis (e.g., SQ-2306, 2206)
7 Controller status 1 = Under computer control (analog servo control, if supported, is not available)
8 Reserved
9 Forward limit 1 = Forward travel limit reached
10 Reverse limit 1 = Reverse travel limit reached
11 Motor burst or amplitude mode 1 = Amplitude mode (always used in closed-loop mode).
1 = Burst mode (200 Hz)
12 - 15 Reserved N/A
16 Encoder count error 1 = An error was detected in the encoder quadrature signal. Cleared by sending command <07>.
17 Zero reference enabled 1 = Encoder zero reference mark detection is enabled
18 Motor on target 1 = Encoder position error is zero
19 Motor moving toward target 1 = Motor is moving toward a target position; appears after command <08> or move step command <06>. Once the target is reached, bit 19 is set to zero.
20 Maintenance mode enabled 1 = Controller will actively hold the last target position
Note
If bits 20 and 21 are set 1 and bit 18 is set to 0, the controller is in the process of moving back toward the last targeted position.
21 Closed loop enabled 1 = Motion commands use the encoder for feedback
22 Motor accelerating 1 = The motor is accelerating to the desired velocity (set at the start of closed-loop motion)
0 = Required motor speed is reached, motor is decelerating, or motor is stopped
23 Stalled 1 = The position error exceeds the stall detection threshold

Following two examples will show, how the motor status value will look like (using the code snippet before):

Example 1: Motor doesn't move (return = false)

Status: Hex: 340080 Dec: 3408000 Binary: 0011 0100 0000 0000 1000 0000 23-20 19-16 15-12 11-08 07-04 03-00 => bit 2 is 0 motorRunning would be 4 = 0000 0000 0000 0000 0000 0100 (status & motorRunning) = 0 => return false

Example 2: Motor does move (return = true)

Status: Hex: 380086 Dec: 3670150 Binary: 0011 1000 0000 0000 1000 0110 23-20 19-16 15-12 11-08 07-04 03-00 => bit 2 is 1 (status & motorRunning) = 4 => return true

Example 3: Something a little more complex

This shows a more complex piece of code of how the motor focus can be used.

#ifdef _MSC_VER
# include <windows.h>
#else
# include <time.h>
#endif
#include <apps/Common/exampleHelper.h>
#include <iostream>
#include <iomanip>
#include <mvIMPACT_CPP/mvIMPACT_acquire.h>
#include <typeinfo>
using namespace std;
// This whole sample shows the low level access to the focus motor. For some
// of the functions presented here, there are also convenience functions in
// 'mvIMPACT::acquire::MotorFocusControl'
//-----------------------------------------------------------------------------
static void millisleep( long millisec )
//-----------------------------------------------------------------------------
{
#ifdef _MSC_VER
Sleep( millisec );
#else
timespec requested;
requested.tv_sec = millisec / 1000;
requested.tv_nsec = ( millisec % 1000 ) * 1000000L;
nanosleep( &requested, NULL );
#endif
}
//-----------------------------------------------------------------------------
class MotorControl
//-----------------------------------------------------------------------------
{
private:
const MotorFocusControl mfc;
const string version;
// private, so as to hide the command strings from the outside world
TDMR_ERROR write( const string& command ) const
{
mfc.motorFocusSendBuffer.writeS( command );
const TDMR_ERROR retval = static_cast<TDMR_ERROR>( mfc.motorFocusSend.call() );
#if _DEBUG
if( retval != DMR_NO_ERROR )
{
cerr << "Call to command '" << command << "' failed with error '" << DMR_ErrorCodeToString( retval ) << "'" << endl;
}
#endif
return retval;
}
void waitForCommandReceipt( const string& expectedReply ) const
{
const size_t length = expectedReply.length();
string reply;
while( ( ( reply = getReply() ).length() < length ) ||
( reply.length() == length && reply != expectedReply ) ||
( reply.length() > length && reply.substr( 0, length ) != expectedReply ) )
{
cout << "Waiting for confirmation of command " << expectedReply.substr( 1, length - 1 ) << " (" << reply << ")" << endl;
}
}
TDMR_ERROR writeConfirmed( const string& command ) const
{
const TDMR_ERROR retval = write( command );
if( retval == DMR_NO_ERROR )
{
waitForCommandReceipt( command.substr( 0, 3 ) );
}
return retval;
}
string initializeAndGetVersion( void ) const
{
write( "<01>" ); // must be the first command written
millisleep( 1500 ); // initialization takes time
return getReply();
}
unsigned int replyToInt( const string& reply, int bitNr /* < 32, or it won't fit in an unsigned int */ ) const
{
unsigned int nrOfCharactersNeeded = ( bitNr >> 2 ) + 1; // four bits in one character
if( reply.length() < nrOfCharactersNeeded + 4 ) // first four characters contain no status bits
{
throw runtime_error( "Reply string too short" );
}
unsigned int uistatus;
istringstream iss( reply.substr( 4, nrOfCharactersNeeded ) ); // skip the first four characters, that contain no status bits
iss >> hex >> uistatus; // string returned is in hex
return uistatus;
}
bool bitIsSet( unsigned int uistatus, int bitNr ) const
{
return ( uistatus & ( 0x1 << bitNr ) ) != 0;
}
bool bitIsNotSet( unsigned int uistatus, int bitNr ) const
{
return ( uistatus & ( 0x1 << bitNr ) ) == 0;
}
bool bitIsSet( const string& reply, int bitNr ) const
{
return bitIsSet( replyToInt( reply, bitNr ), bitNr );
}
bool bitIsNotSet( const string& reply, int bitNr ) const
{
return bitIsNotSet( replyToInt( reply, bitNr ), bitNr );
}
public:
explicit MotorControl( Device* device ) : mfc( MotorFocusControl( device ) ), version( initializeAndGetVersion() )
{
if( bitIsNotSet( getStatus(), 21 ) )
{
writeConfirmed( "<20 1>" ); // only in closed-loop drive mode will command moveToPosition work
}
}
~MotorControl()
{
write( "<03>" ); // halt the motor (do not wait for confirmation, as the dtor will also be called when the USB plug is pulled, and then one would obviously wait forever)
write( "<02>" ); // release computer control
}
string getVersion( void ) const
{
return version.length() > 8 ? version.substr( 6, version.length() - 7 ) : version;
}
string getReply( void ) const
{
millisleep( 40 );
return mfc.motorFocusReceiveBuffer.read(); // mfc is private
}
string getStatus( void ) const
{
write( "<10>" ); // request status
return getReply();
}
// only first 16 status bits of "<10>"
string getShortStatus( void ) const
{
write( "<19>" ); // request motor status
return getReply();
}
bool isRunning( void ) const
{
return bitIsSet( getShortStatus(), 2 ); // would also work with getStatus()
}
string getPositionStr( void ) const
{
string status = getStatus();
if( status.empty() )
{
throw runtime_error( string( "Could not retrieve status" ) );
}
return status.substr( 11, 8 );
}
int getPosition( void ) const
{
int ipos;
istringstream iss( getPositionStr() );
iss >> std::hex >> ipos; // string returned is in hex
return ipos;
}
void moveToPosition( int pos ) const
{
ostringstream oss;
oss << string( "<08 " );
oss << std::hex << setw( 8 ) << setfill( '0' ) << pos;
oss << string( ">" ) << ends;
writeConfirmed( oss.str() );
}
void waitForEndOfMove( void ) const
{
while( isRunning() )
{
millisleep( 40 ); // wait until the position has been reached
}
}
// required after plugging FOX out and back in again
void reestablishMotorControl( void ) const
{
while( initializeAndGetVersion().empty() ) {};
}
};
//-----------------------------------------------------------------------------
bool isDeviceSupportedBySample( const Device* const pDev )
//-----------------------------------------------------------------------------
{
if( pDev->family.read() != "mvBlueFOX" )
{
return false;
}
return true;
}
//-----------------------------------------------------------------------------
int main( void )
//-----------------------------------------------------------------------------
{
DeviceManager devMgr;
Device* pDev = getDeviceFromUserInput( devMgr, isDeviceSupportedBySample );
if( !pDev )
{
cout << "Unable to continue! Press [ENTER] to end the application" << endl;
cin.get();
return -1;
}
try
{
pDev->open();
}
catch( const EDeviceManager& e )
{
cerr << "Could not open device " << pDev->serial.read() << " (" << e.what() << ", " << e.getErrorCodeAsString() << ")" << endl;
return -1;
}
try
{
MotorControl mc( pDev );
cout << "Found " << mc.getVersion() << endl;
try
{
int i = 4;
while( i-- )
{
mc.moveToPosition( 1500 );
mc.waitForEndOfMove();
cout << mc.getPosition() << endl;
mc.moveToPosition( 2500 );
mc.waitForEndOfMove();
cout << mc.getPosition() << endl;
}
}
catch( const exception& e )
{
cerr << "Exception of " << typeid( e ).name() << " '" << e.what() << "'" << std::endl;
return -1;
}
}
catch( const exception& e )
{
cerr << "No M3-F found on this device (" << e.what() << ")" << endl;
return -1;
}
pDev->close();
return 0;
}