Impact Acquire SDK GUI Applications
|
The mvBlueCOUGAR-S cameras feature a built-in defective pixel compensation. For that purpose, you will need the current firmware.
To compensate the defective pixels, please do following steps (you can use the tab "Pixel Histogram" to show the gray scale values):
Over "int PixelCompensationDetect()", click on the right mouse button and confirm with "Execute".
Now, activate the PixelCompensation by setting "PixelCompensationMode" to "On."
This setting can be saved in the camera via "int PixelCompensationSave()" so that the pixel compensation is system independent.