Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
AOI Wizard
ImpactControlCenter - AOI Wizard

The AOI wizard allows the set up all sorts of AOIs in a fairly easy way. Supported AOIs can either be configured as described within the image analysis chapter (Analysis AOIs) or by using the controls offed by the dialog. To select a certain AOI when starting the wizard first the device will be configured to full AOI mode again. Pressing "Ok" will then close the dialog and will apply all AOI settings to the device, pressing "Cancel" will revert all changes made with this dialog.