Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
Using Multiple Displays

ImpactControlCenter is also capable of working with multiple display windows! This becomes particularly useful when either working with one device and multiple settings as described here or when working with a GenICam™ device that offers a sequencer. See Sequencer Control Wizard to find out more about that!

The amount of parallel image displays can be configured via the Command-line Interface by the parameters "dcx" and "dcy":

ImpactControlCenter dcx=1 dcy=2

This will result in 1 display in horizontal direction and 2 in vertical direction.

Since
Version 2.18.1 of this application

It is also possible to change the amount of display at runtime via "Settings → Image Displays → Configure Image Display Count":

ImpactControlCenter - Configure Image Display Count

Afterwards 2 smaller dialogs will pop up allowing to select the amount of display windows in X/horizontal direction:

ImpactControlCenter - Selection of display windows in horizontal direction

And in Y/vertical direction:

ImpactControlCenter - Selection of display windows in vertical direction

As a result then the application will look like this:

ImpactControlCenter - 2 by 3 display windows

Each display window can be configured individually via it's context menu. For example it is possible to assign different scaling factors and interpolation algorithms to each window. The perform an analysis like calculating a histogram the corresponding display must be selected by left-clicking on it.