Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
Horizontal/Vertical Line Profile

The horizontal and vertical line profile plots provide a way to visualize course of the intensity either in a horizontal or in a vertical direction:

ImpactControlCenter - Line Profile

In this example (horizontal line profile) each test image bar within the AOI results in a flat line of a certain intensity within the middle of the intensity range. Whenever a new intensity bar starts there is a sudden jump in intensity found as well in the profile.

Typically the AOI dimension in the other direction will be 1 but also any other value is possible. In that case the average value of the included range will be calculated.

Note
The profile lines can also be used to conveniently adjust the focus by looking at an edge and then try to adjust the lens in a way this edge has its maximum gradient.
See also
Other Drawing/Display Options