Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
Record To Hard Disk

This mode can be used to save a sequence of images from the current acquisition to the hard disk directly.

You can save acquired images to the hard disk the following way:

  • Select "Capture → Setup Hard Disk Recording" from the menu.
  • Enable the Hard Disk Recording.
  • Enable saving of meta data if needed.
  • Afterwards select the target folder for the images.
  • Finally, choose the file format of the acquired images.
  • Click "Apply" or "Ok" to finish the setup
  • Current status information will be visible in the Output tab of the Image Analysis (The Big Picture)
ImpactControlCenter - Hard Disk Recording.