Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
Viewing The Current Network Topology
Since
3.5.0

IPConfigure does allow to display the current network topology showing which device has been discovered on which network interface. This can be helpful for

  • Fixing incorrect network configurations. E.g. in scenarios where devices are detected on multiple interfaces or on an unexpected interface
  • Checking bandwidth related issues. E.g. when trying to equally distribute network load
IPConfigure - Network Topology

A network adapter that hasn't jumbo frames set up, or a transmission line, that doesn't support large network packets, immediately becomes apparent. See Optimizing Network Performance chapter how to configure network adapters correctly.

IPConfigure - Network Topology good and bad MTU setting