Impact Acquire SDK GUI Applications
Loading...
Searching...
No Matches
Remove The GigE Vision™ Capture Filter Driver

To remove the GigE Vision™ capture filter driver, please follow these instructions:

  1. Start the GigEConfigure by clicking the program in the start menu.
  2. When started click on the "Remove driver" button.
    The tool will then automatically remove the GigE Vision™ capture filter driver from ALL NICs it is currently installed on.
Note
Afterwards the list of NICs will be empty, since only those where the GigE Vision™ capture filter driver is installed on (either enabled or disabled) will be listed.