Impact Acquire SDK Python
Loading...
Searching...
No Matches
Java Support

In case an application makes use of the Java to Impact Acquire native interface the libmvIMPACT_Acquire.java.so library must be deployed on the target system as well. The same restrictions, path information, etc. as in the Common Files Needed For Every Device Family section apply.

Note
More information about locations of libraries within the standard installation is summarized at Locating Runtime Libraries.